USB-C Power Delivery Data Lines Demand Enhanced Protection
Abstract
USB Type-C and USB-C power delivery raise voltage and power levels. A new reversible connector with a tighter pin pitch than that of the USB Micro-B increases the risk of short circuits. In conjunction with the ever-increasing complexity of portable devices, this leads to enhanced electrostatic discharge (ESD), surge, and overvoltage (OV) protection requirements. This article presents a design solution that has a compact, full-featured protection IC. This lowers the BOM and takes up less space on the PCB.
Introduction
The USB Type-C® (USB-C) cable and connector specification makes it easy to link and power electronic gadgets, such as digital cameras and ultrathin tablets (Figure 1). The specification supports USB-C charging applications up to 15 W. The USB-C power delivery (PD) extends charging up to 100 W and includes interchangeable charging across a wide variety of devices.
With USB Type-C connectivity, there are new design challenges in protecting the system. The new connector has a smaller pitch than that of the USB Micro-B, which leads to increased risk of mechanical shorts to VBUS. Additionally, due to the high voltages associated with USB PD, more robust protections are needed. And finally, the ever-increasing complexity of the electronic loads demand enhanced protection from ESD and voltage surges. This article reviews the USB Type-C PD architecture and the challenges associated with D+/D– data signal protection. It then proposes a highly integrated 2× SPDT switch that can address these challenges with minimum BOM and PCB occupancy.


USB-C PD System
Figure 2 illustrates a typical portable power management device front end equipped to connect to a USB-C cable and powered by a lithium-ion (Li+) battery.
When the VBUS is present, it powers the charger, the system, and the rest of the blocks. In this phase, the battery is charged. When the VBUS is disconnected, the battery powers the system. With the USB-C cable, the CC1 and CC2 pins determine port connection, cable orientation, role detection, and port control. The D+/D– lines are the standard USB-C communication lines handling data with a speed of 480 Mbps and are protected by the D+/D– protection device. The PD controller implements the power delivery protocol.
The Protection Challenge
Electric surges and ESDs in a power supply are common and can interfere with or cause damage to electronic loads and equipment. The transfer of static electrical charge from a body to an electronic circuit causes ESD. ESD is a big concern for handheld electronics. Electrical surges can be caused by lightning or induced by long cables laying in proximity of a lightning strike. Switches or relays can cause surges during on and off operation. A load dump is a surge generated by cutting the battery connection off on an automobile. A good data line protection IC should offer adequate protection without significant data degradation.
Integrated Solution
As an example, the MAX20334 is a 2× SPDT switch with overvoltage protection intended for use with portable devices (Figure 3). The IC protects the downstream data line from a high voltage short, ESD, or surge event. It combines low on-capacitance and low on-resistance necessary for high performance switching applications in portable electronics. The IC features internal positive overvoltage and surge protection. The device handles USB low/full/high speed signaling and operates from a 2.7 V to 5.5 V supply. It is available in a 12-ball (1.23 mm × 1.63 mm) wafer-level package (WLP) and operates over the –40°C to +85°C extended temperature range.
Extended Protection
ESD protection structures are incorporated on all pins to protect against electrostatic discharges up to ±2 kV (human body model) encountered during handling and assembly. COMA and COMB (Figures 2 and 3) are further protected against ESD up to ±15 kV (human body model), ±15 kV (air gap discharge method described in IEC 61000-4-2), and ±8 kV (contact discharge method described in IEC 61000-4-2) without damage. The ESD structures withstand high ESD, both in normal operation and when the device is powered down. After an ESD event, the IC continues to function without latch-up. The IC is surge-protected from –30 V to +45 V (IEC 61000-4-5) and overvoltage protected up to +20.5 V.
Figure 4 compares the PCB layout of this highly integrated, extended protection solution with a typical competitor device offering positive-only surge protection and lower OV and ESD protections. The latter will require additional circuitry to meet ESD/surge/OV specifications, leading to a more costly BOM and a 5× bigger PCB active area occupancy.
Data Integrity
The eye diagram in Figure 5 shows at a glance the good level of integrity of the data signal. The curved blue lines maintain a close-to-maximum distance from the forbidden red zone. The high bandwidth of the protection IC causes a minimum slowdown of the signal rise and fall times and jitter, resulting in a good margin for error. This is important to pass USB compliance tests.
Conclusion
With USB Type-C come new challenges in interconnecting, powering, and protecting our electronics. The new connector has a smaller pitch than that of the USB Micro-B, leading to an increased risk of mechanical shorts to VBUS. Additionally, due to the high voltages associated with USB PD, more robust protections are needed. And finally, the ever-increasing complexity of the electronic loads demands enhanced protection from ESD and voltage surge. An enhanced protection device with up to ±15 kV ESD, –30 V to +45 V surge, and +20.5 V overvoltage protection can protect data lines and meet ESD/surge/OV specifications while lowering BOM costs.
About the Authors