The MAX1463EVKIT Setup and Functional Verification

Feb 18 2003
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Abstract

The MAX1463 is a highly integrated, low power, two-channel sensor signal processor optimized for industrial and process control applications such as pressure sensing, RTD and thermal-couple linearization, weight sensing, and remote process monitoring with limit indication.

The MAX1463 accommodates sensors with outputs ranging from 1mV/V to 1V/V. It includes two 16-bit output DACs, two 12-bit PWM outputs, and supports 4mA–20mA output. It incorporates a 16-bit CPU, 4Kb of program and 128 bytes of user flash memory.

The following procedure will guide you to set up the MAX1463 hardware/software and verify that it is functioning correctly.

Hardware Requirements

  • Microsoft® Windows 98 or higher.
  • 32MB of RAM.
  • 20MB of hard disk.
  • One parallel port.

EV board Configuration

  • See the MAX1463 evaluation board diagram in Figure 1.
  • Configure the EV board jumpers per Table 1

Figure 1. The MAX1463 evaluation board.

Figure 1. The MAX1463 evaluation board.

Table 1. EV Board Jumpers Configuration
JU1 SHORT Power Supply Selection Unregulated external +8VDC to +40VDC.
JU2 SHORT
Pin 1-2
VREF Selection Internal VREF.
Pin-1 is at the bottom.
JU3 OPEN Clock Selection Internal Oscillator
JU4 SHORT
(shorted)
Communication Interface 3-Wire Communication Interface.
Cut wire to open.
JU5 OPEN ISRC pin Configuration ISRC pin floating.
JU6 OPEN GPIO1 Mode Logic level = 0
JU7 OPEN GPIO2 Mode Logic level = 0
JU8 SHORT LED1 Configuration LED1 driven by GPIO1.
JU9 SHORT LED2 Configuration LED2 driven by GPIO2.
JU10 OPEN Bridge Voltage Drive Selection Bridge Voltage connected to +5VDUT.
Pin 1 is at the bottom.
JU11 OPEN INP1 Configuration INP1 floats.
JU12 OPEN INM1 Configuration INM1 floats.

Hardware Connection

  • Set up the system per Figure 2.
  • Connect the DMM. The terminals are connected between the VSS (pin 14) and any pin you wish to measure. For example: small op-amp; large op-amp; Channel-1... etc.
  • Connect one end of the 16-pin ribbon cable between the 16-pin headers on the EV board and the communication KEY. Please make sure the pin-1 of the ribbon cable is connected to the pin-1 of the boards.
  • Apply 9V supply to the TB1 terminal block.
  • Connect the 25-pin connector of the KEY to the computer parallel port. Any available parallel port is acceptable.

Figure 2. Hardware connection.

Figure 2. Hardware connection.

Software Installation

  • Insert the MAX1463 CD in the CD drive.

  • Install ASM1463 in your computer. The default destination directory is "C:\MAX1463". The destination directory can be changed as desired.
  • The MAX1463 control software and supporting files will be stored in the specified directory.

System Verification

  • Run the "Hardware Debugger":
    "Start/Programs/Maxim MAX1463 Evaluation Kit/Hardware Debugger"

  • Press function-key F9 or select the "Flash Memory" tab.

  • From "Flash Position 0" block of the window, press the "Load buffer from file" button. An open file window will appear that will include the following files. Select the "Ccmtr1.hex" and press Open.

  • From "Flash Position 0" block of the window, press the "Write to device" button. At completion, "Programming complete" statement will be displayed.

  • From "Flash Position 0" of the window, press the "Verify device against buffer". The program will read the content of the flash memory (what you just wrote) and compare that with the buffer (what you intended to write). At completion, "Verify complete" will be displayed. In case of failure, a "mismatch..." message will be displayed along with the address of the memory location where the mismatch was found.
  • Press "Reset CPU"
  • Press "Run CPU".
    The red LEDs on the EV board will start flashing.
    The blinking LEDs confirm that the software installation was successful, you have proper hardware setup, and the EVKIT is working.
  • Press "Halt CPU".
    The LEDs will stop blinking.

View Program Listing

  • Select the "Program Listing" tab

  • From the directory you installed the MAX1463 programs, Open the "Cctmr1.lst" listing with File | Open...

  • You may roll the side bar up and down in order to view the entire program listing.


Related to this Article

Product Categories

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project