Simulating Power Planes with LTspice

Apr 8 2013

Figure 1

   

When designing Power Distribution Networks (PDN) it is common to use SPICE models to represent the planes. High-end designs use 2D/3D electronic magnetic modeling tools to extract SPICE models. However, there are times when a simple spice model will suffice, or you may not always have access to very expensive 2D/3D modeling tools. With a few simple tricks, PDN designs can be modeled with LTspice up to about 3GHz.

Many times a PDN can be considered as a two-plane rectangle in the PCB, either because the actual layout is small and rectangular, or can be approximated with a small rectangle. When this is the case, one can first model the plane with an analytical tool, build an LTspice model, and then with some trial and error tune the LTspice model to match the analytical model. The results will come reasonably close to PDN measurements. In this post, I will demonstrate how to build the LTspice model from an analytical model. Then I will show measurement data from a proto board demonstrating the limitations of the technique.

There is a good analytical model spreadsheet from Istvan Novak that can be downloaded at http://www.electrical-integrity.com. On the tools page, look for the model that says, “It calculates the self impedance of a bare rectangular parallel plates at arbitrary locations.” Let’s proceed with an example using this model.

Suppose we have a 2 inch square plane with 0.003 mils separation built with FR4. Also assume that the load is in the center of the plane, and that the best impedance model is at the center of the square. Putting these parameters into the model we get the following results.

 

Simulating Power Planes with LTspice IV

 

Simulating Power Planes with LTspice IV

The planes look like a capacitor out to 600MHz, then they look like an inductor out to about 3GHz, and finally things get weird because we are dealing with a resonant cavity. A good LTspice model should account for the capacitance, the inductance,
and the first resonance peak. A useful SPICE model can be found in the DesignCon 2013 paper titled “Innovative PDN Design Guidelines for Practical High Layer‐Count PCBs” by Shringarpure, Pan, and Kim. Here is the figure from the paper with the basic model, which includes the ecoupling capacitors and feedthrough inductances:

 

Simulating Power Planes with LTspice IV

The plane portion of the model is the middle piece, so we begin with that.

 

Simulating Power Planes with LTspice IV

The next step is to estimate the capacitance and inductance of the planes by using points on the graph from the analytical model.

 

Simulating Power Planes with LTspice IV

 

Simulating Power Planes with LTspice IV

We make an educated guess at LIC, which models the resonance peak, by choosing 100pH. Now we divide the C and L by 1/2 and we have our first model.

 

Simulating Power Planes with LTspice IV

 

Simulating Power Planes with LTspice IV

Clearly the plane resonance peak is not near 3GHz, so the next step is to iteratively modify LIC until the peak moves near 3GHz and matches the analytical model, and then fine tune the other elements until we match the analytical model. When LIC is 8pF, and LP1 and LP2 are 42pF, the SPICE model matches the analytical model.

 

Simulating Power Planes with LTspice IV

However, the cavity resonances are missing, because the SPICE model does not have elements to represent them. This plane model is usable to about 4GHz, assuming the rectangular plane adequately represents the actual PCB shapes. With the plane model in place, we can continue modeling the rest of the PDN by adding capacitors modeling feedthroughs, following the model in the DesignCon paper. For example, here is a model of a Point of Load (POL) proto board:

 

Simulating Power Planes with LTspice IV

 

Simulating Power Planes with LTspice IV

The target impedance of this PDN was 10mΩ out to 10MHz.

 

Simulating Power Planes with LTspice IV

The measured results are close, but we can see some discrepancies. To get close to the measured results I measured each capacitor with a Bode 100 VNA and modeled them as an RLC. The feedthrough inductances where approximated from past experience. Analytical models of feedthroughs could be used, but by empirically modifying the inductances, some of the spreading inductance was accounted for in the model. Like any model, you have to decide how much effort you are willing to make, and how accurate the model needs to be. 

In summary, you can build reasonable LTspice PDN models out to 1‐3GHz. The models are limited by the assumption of rectangular planes, approximating spreading inductance and feedthrough inductance. Be sure to validate models by measuring PDN impedance with a VNA. Low frequency measurements out to 40Mhz can be made with a Bode 100 or similar instrument. Agilent and other companies make VNA that are good out to Ghz. Once you have valididated models, you can reuse them in future designs.

If you need a highly accurate model that does not depend on prototyping and past experience, you should use 2D/3D modelers. But even with these great modeling tools, you should validate your results with a VNA to ensure your model is accurate.

 

Simulating Power Planes with LTspice IV

This Shows The Actual Layout

About the Authors

Michael Jones

Related to this Article

Resources

Latest Media 21

Subtitle
Learn More