Multi-Rail DC/DC Converter in a 3mm × 3mm QFN Takes Inputs as Low as 0.7V
Multi-Rail DC/DC Converter in a 3mm × 3mm QFN Takes Inputs as Low as 0.7V
Jun 1 2008
Introduction
Modern handheld instrumentation, portable medical devices and consumer electronics demand a multitude of power rails for internal processors, memory, audio and color displays. Popular battery technologies for these devices include single or multiple cell alkaline, NiMH or Li-Poly/Li-Ion batteries. Operation from a USB port or a wall adapter is another common trait. Replaceable alkaline batteries are particularly attractive for remote locations and portable medical devices where power or time is not available to recharge batteries. The challenge is to create a compact and efficient power solution for these wide VIN range, multi-output applications. The LTC3100 multichannel DC/DC converter makes it easier to meet this challenge.
The LTC3100 is a high efficiency, 1.5MHz multichannel DC/DC converter in a compact 3mm × 3mm × 0.75mm QFN package. It features a synchronous step-up (boost) DC/DC converter, a synchronous step-down (buck) DC/DC converter and a 100mA low dropout linear regulator (LDO).
The boost and buck converters can operate independently from different sources, from the same source, or cascaded to create a buck-boost converter. Internal loop compensation simplifies the design and minimizes external component count and solution size. Each converter has a Power Good indicator that is useful for voltage sequencing. The boost converter offers up to 95% efficiency and features true output disconnect, a 700mA minimum current limit and can start with input voltages as low as 700mV, making it ideal for single alkaline or NiMH cell applications. The buck converter offers up to 94% efficiency and can deliver 250mA or more from input voltages between 1.8V and 5.25V. Both converters feature automatic Burst Mode® operation for high efficiency at light loads. For low noise applications, Burst Mode operation can be disabled by grounding the MODE pin. The 100mA LDO, whose input is internally connected to the boost output, can be used to produce a third, low noise output. It can also be used for voltage sequencing of the boost output voltage.
The circuit shown in Figure 1 takes advantage of the LTC3100’s ability to operate from independent input sources to generate multiple outputs regardless of which power source is available. In this example, the boost converter produces a regulated 3.3V output from a single- or dual-cell input voltage. The buck converter runs from a 5V USB or wall adapter input and produces 3.3V as well, with its output externally tied to that of the boost.

Figure 1. Multiple-input source 3.3V and 1.8V converter.
By leaving the MODE pin open, the automatic Burst Mode operation feature of the LTC3100 is enabled, maximizing battery life at light load. When USB or wall adapter power is available, the buck converter is automatically enabled and generates a 3.3V output that is set 3.8% higher than that of the boost converter. This puts the boost converter in sleep mode, reducing the load on the batteries to just a few micro-amps. The result is a 3.3V output that seamlessly transitions from battery power to USB power while maximizing battery life. The diode on the USB input prevents any reverse current from the 3.3V output (while operating on batteries) back to the USB input when it is open or grounded. Figure 2 shows the converter efficiency versus load with various input sources, illustrating the high efficiency over a wide load range. The LDO in the LTC3100 (with its input internally tied to the Boost output) provides a second regulated output, in this case programmed to 1.8V.

Figure 2. Converter efficiency for the circuit of Figure 1.
Because the buck converter input can come from the boost output, the LTC3100 can function as an ultra-low voltage buck-boost converter, providing a regulated 1.2V output from a single alkaline or NiMH cell. This is shown in Figure 3, where the LTC3100 generates two regulated outputs from a single cell input (whose voltage may be above or below 1.2V) by boosting VIN up to 3.5V and then regulating down to 1.2V and 3.3V using the buck and the LDO. In this example, the Power Good outputs and the LDO are used to provide voltage sequencing, so that the 1.2V core supply comes up before the 3.3V I/O supply, as shown in the scope photo of Figure 4. The LDO also provides additional noise filtering and ripple rejection for the 3.3V output, guaranteeing a low noise output for sensitive analog circuitry, even when the converters are in Burst Mode operation.

Figure 3. Single-cell dual output converter with voltage sequencing.

Figure 4. Voltage sequencing of the output voltages for the circuit of Figure 3.
Conclusion
The LTC3100 is a high efficiency, multichannel converter that can operate from a wide range of voltage sources. Independent input voltages for each converter, Power Good outputs and an LDO make the LTC3100 a small, highly integrated and flexible solution for many demanding applications.
About The Authors
David Salerno was a Design Section Leader for the Power by Linear group of Analog Device (former Linear Technology) for nearly 20 years. His main focus was the DC/DC Converter design on boost applications. David hold an B...
Related to this Article