MAX3991: Accurate Loss-of-Signal Detection in 10Gbps Optical Receivers using the MAX3991

Dec 10 2004
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Abstract

This design note outlines the characteristics of the MAX3991 LOS detector, and describes how to set the optical assert power in a 10Gbps receiver for a specified BER. A method for increasing LOS hysteresis for operation at low power levels is also described.

About The Authors

Sharon Wang

Latest Media 20

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project