Make Your Small Asset Tracker Last Longer

Abstract

This design solution reviews a typical asset tracking solution and shows how the MAX3864x nanopower buck converter family, with its high efficiency and small size, enables longer battery life in small portables. New, low power data connections are sparking a proliferation of asset tracking solutions thanks to their low cost of deployment. The effects can be seen in multiple applications, particularly transportation and supply chain management.

Introduction

In a typical application, a sensor provides updates from a given location, transmitting data about temperature, humidity, pressure, and motion. The sensor only needs to transmit small amounts of data, which results in higher coverage and ultra low power consumption, enabling far greater device longevity. The sensor’s battery must last from several weeks to a few years. Asset tracking, depending on the application, may require the deployment of several tracker devices. Accordingly, these asset tracker devices must also be small, portable, and cost-effective.

In this design solution, we discuss the power management challenges encountered by a typical battery-operated asset tracker device and show an example using a small, high efficiency buck converter.

Edge-to-Enterprise Communication

Figure 1 illustrates a typical tracking communication chain. The asset being tracked transmits the data via a beacon, which reaches a server through a dedicated cellular network. From here, the data reach the enterprise portal for asset management and analytics.

Figure 1. Real-time GPS tracking.
Figure 1. Real-time GPS tracking.

In the factory environment, asset tracking brings the management of facilities, vehicle fleet equipment, and maintenance into a single platform, resulting in improved safety, productivity, and extended asset life.

Asset Tracking Networks

A new generation of beacons connects directly to dedicated cellular networks (LTE-M, NB-IoT), eliminating the use of Bluetooth® to communicate with a gateway. These technologies can be very different but are all characterized by low power consumption, enabling several years of battery life (Table 1).

Table 1. Networks Characteristics
NB-IoT LTE-M Units
Bandwidth 180 1400 kHz
Peak Data Rate 100 384 kbps
U/D Link Speed 62.5 1000 Mbps
Latency 10 100 ms
Battery Life >10 10 Years
Voice No Yes

Typical Asset Tracker System

Figure 2 shows a typical asset tracker block diagram. The three-series alkaline battery supplies a charge of 2000 mAh. A step-down regulator powers the onboard controller, sensors, and radio.

Figure 2. An asset tracker block diagram.
Figure 2. An asset tracker block diagram.

For demanding asset tracking applications, the system must last for a year on three alkaline batteries, drawing only 100 µA in deep sleep, and transmitting 100 mA once per day for about 2 minutes (Figure 3). While it is true that, depending on power level and other options supported in the LTE-M or NB-IoT asset trackers, currents can be higher, for our discussion, we will stick to the 100 µA to 100 mA range.

Figure 3. Asset tracker current profile.
Figure 3. Asset tracker current profile.

High use performance requires careful selection of each block for minimum power consumption. The buck regulator must be efficient over a wide range from 100 µA to 100 mA. For instance, a 4% average loss of efficiency by the buck converter translates into a field deployment reduction of about two weeks.

Ultralow Quiescent Current

The buck converter’s quiescent current is especially important since the device is in deep sleep or quiet mode most of the time, consuming only 100 µA or less. With VOUT = 1.8 V, the output power during deep sleep is POUT = 1.8 V × 100 µA = 180 µW. With η = 90%, the input power is:

Equation 1

If the buck converter is not carefully chosen and has a typical quiescent current of 3 µA and a 3.6 V input voltage, there is an additional power dissipation of:

Equation 2

The final buck converter efficiency is:

Equation 3

A quiescent current of 3 µA robs the buck converter of 4 efficiency points, draining the battery significantly faster!

On the other hand, a buck converter with 300 nA quiescent current will barely reduce the efficiency, lowering it by only half a percentage point. For asset tracking applications, it is critical to select a buck converter with ultralow quiescent current as the system spends the majority of the time in quiet mode and relies on a battery.

Nanopower Buck Converter

As an example of high efficiency, the nanopower ultralow 330 nA quiescent current buck (step-down) DC-to-DC converter shown in Figure 4 operates from a 1.8 V to 5.5 V input voltage and supports load currents of up to 175 mA with peak efficiencies of 96%. While in sleep mode, it consumes only 5 nA of shutdown current. The device is housed in a space-saving 1.42 mm × 0.89 mm, 6-ball wafer-level package (2 × 3 ball WLP, 0.4 mm pitch). If higher currents are desired based on the power level in the NB-IoT or LTE-M networks, sister parts can deliver higher currents.

Figure 4. An integrated buck converter.
Figure 4. An integrated buck converter.

Small Size

The nanopower buck converter’s application footprint is shown in Figure 5. Thanks to its WLP package, high switching frequency operation, and small external passives, the net PCB area of the buck converter is a meager 7.1 mm2.

Figure 5. Asset tracker buck converter application (7.1 mm2 net area).
Figure 5. Asset tracker buck converter application (7.1 mm2 net area).

Efficiency Advantage

Figure 6 shows the efficiency curve of the buck converter with a 3.6 V input and a 1.8 V output. Synchronous rectification at high load and pulsed operation at light load and ultralight load assure high efficiency across a wide operating range.

An 87.5% high efficiency operation at 100 µA and 92% efficiency at 100 mA make the IC ideal for asset tracking applications. This buck converter has the advantage of several efficiency points compared to alternative solutions.

Figure 6. MAX38640 efficiency curve.
Figure 6. MAX38640 efficiency curve.

The benefits of high efficiency and smaller footprint go hand in hand, resulting in less heat generation. This helps in designing a smaller, cooler asset tracker, easing concerns of device overheating.

Conclusion

Asset trackers, depending on their specific application, must operate in the field for several weeks to a few years powered only by small batteries. This type of operation requires careful selection of each block for minimum power consumption. The buck regulator must operate efficiently over a wide input current range, from tens of microamps to hundreds of milliamps. The MAX3864x nanopower buck converter family, with its high efficiency and small size, provides an ideal power solution for asset tracking applications.;

About the Authors

Anil Telikepalli
Anil Telikepalli was the managing director of the Core Products Business Unit at Analog Devices with responsibility for power and data converter products. Anil joined Analog Devices in 2010 and managed definition, product ...
Nazzareno Rossetti
Nazzareno (Reno) Rossetti was an analog and power management expert at Analog Devices. He is a published author who holds several patents in the field. Reno has a doctorate in electrical engineering from Politecnico di Tor...
Simo Radovic
Simo Radovic is a power product applications director in the Advanced Consumer Power Group at Analog Devices. He has more than 16 years of DC-to-DC switching converter experience. Simo holds a master’s degree in electrical...

Latest Media 21

Subtitle
Learn More