LED Driver for Automotive Display Applications
Abstract
In today's entertainment and information-centered world, display plays a bigger role in customer mind when selecting a vehicle. Thus, automotive displays have been integrated in applications such as Instrument Clusters, Central Information Displays, Heads Up Display, Mirror Replacements, Rear-Seat Entertainment Displays, and many more, with a total of up to 12 displays per car. People also want home entertainment or phone or tablet display quality experience inside the car. Thus, bigger, wider, higher resolution and crisper displays are needed. In this solution guide, we will be showing various display needs in automotive applications, and how Maxim LED driver products can meet these criteria.
About the Authors
Related to this Article
Products
Automotive I2C-Controlled 4-Channel 150mA Backlight Driver and 4-Output TFT-LCD Bias
Automotive 6-Channel Backlight Driver with Boost/SEPIC Controller and I2C Interface
16-Channel Automotive Local-Dimming Backlight Driver with SPI Interface
Automotive 6-Channel Backlight Driver with Boost/SEPIC Controller and I2C Interface
Automotive 4-Channel TFT-LCD Power Supply with VCOM Buffer and ASIL B Features
Automotive Low Input Voltage I2C 4-Channel 150mA Backlight Driver
4-Channel, Low-Voltage, 120mA LED Backlight Drivers with Integrated Boost Converter
Automotive 4-Channel 130mA Backlight Driver with Boost/SEPIC Controller and I2C Interface
I2C-Controlled 4-Channel Low-Voltage 120mA LED Backlight Driver with Integrated Boost Converter
Automotive 6-Channel Backlight Driver with Boost/SEPIC Controller and Hybrid Dimming
Automotive Low Input Voltage I2C 4-Channel 150mA Backlight Driver Supporting ASIL B
4-Channel, Low-Voltage, 120mA LED Backlight Drivers with Integrated Boost Converter
Automotive 4-Channel 130mA Backlight Driver with Boost/SEPIC Controller and I2C Interface
Automotive I2C-Controlled 4-Channel 150mA Backlight Driver and 4-Output TFT-LCD Bias