Integration of Isolation for Grid-Tied Photovoltaic Inverters
Integration of Isolation for Grid-Tied Photovoltaic Inverters
by
Baoxing Chen
Jul 1 2012
The photovoltaic (PV) industry has been enjoying great growth over the past few years, mostly driven by high oil prices and environmental concerns. However, PV cost remains to be the greatest barrier for further expansion, and it needs to come down further to compete with traditional coal based grid electricity. Besides solar panels, the electronic components, such as PV inverters, are the major cost components. For safety and operational concerns, grid-tied PV converters need to have harvested dc be isolated from the ac grid. Isolation is usually required to satisfy safety regulation to prevent dc injection into the ac grid that may impact distribution transformers and traditional watt-hour meters. Traditional isolation solutions such as optocouplers can’t satisfy the 25 year warranty typical for PV panels. Microinverters also become the trend where the system availability is improved and performance under shading condition is also dramatically improved. In those cases, the PV inverter is installed at the back of the PV panel where the high temperature there can accelerate the degradation of the optocouplers. This paper discusses the signal and power isolation needs in PV inverters and how integration of isolation functions using microtransformers can improve the system performance and reliability and reduce the system size and cost.
There are two major types of PV inverters, transformer-less and transformer isolated ones. Transformer-less inverters can suffer from large ground leakage current and injected dc current because of large panel capacitance and lack of isolation between the PV panel and ac grid, as shown in Figure 1(a). A dc component in the injected ac currents into the grid is less than desirable as it can potentially saturate distribution transformers. There are strict grid requirements for the amount of dc injection in many safety standards and, in some cases, transformer isolation is mandatory. Transformer isolation between the panel and grid would eliminate such a dc injection path arising from the voltage variation of the panel relative to the grid, as shown in Figure 1(b). Besides dc injection,

Figure 1. (a) DC Injection into Grid for Nonisolated Inverter (b) Interruption of DC Injection by Isolation
Besides isolated current and voltage measurements, there are also needs for some interface functions such as
Traditionally the isolation is provided by optocouplers. However, its current transfer function degrades over time, and it may become inoperable in a few years, much shorter than the 20 year lifetime warranty offered for many of these solar panels. Here we propose microtransformer based signal and power isolation that can address a variety of integration needs in PV inverters. Not only can it eliminate the lifetime degradation limitation for the optocouplers, it also allows integration of sensing functions such as ADCs or interface functions such as gate drivers and
Signal and Power Isolation Using Microtransformers
Microtransformers can be used to provide integrated signal and power isolation for up to 5 kV rms [1]. For signal transfer, the input data is usually encoded before being transmitted to the primary of a data transformer. A decode is used at the secondary side to recover the signal. Isolation between the input and output is provided by the insulation layers between the primary coil and the secondary coil. For efficient power transfer across isolation, a self oscillating high frequency oscillator is used to drive the primary for the power transformer, and high frequency Schottky diodes are used to provide rectified dc voltage. The regulation is done by a PWM generated by a secondary controller to pass through a feedback transformer to turn on and off the oscillator in a frequency much lower than the oscillation frequency as shown in Figure 2(a). The feedback signal transmitted through the feedback transformer works the same way as that for other data channel signals through the data transformers. With separate control paths for energy conversion and feedback, energy conversion efficiency is optimized while stable regulation is maintained. An example 500 mW isolated

Figure 2. (a) Schematic Diagram for an Isolated DC-to-DC Converter (b) Package Implementation for a 4-Channel Isolator with 500 mW Isolated Power
In this example, the transformers are built on separate chips from those of the encoder or the primary chip and the decoder or the secondary chip. However, this is primarily driven for cost reasons, and the transformers can in principle be built on top of one of the IC chips. Additional circuit functions such as gate drivers, transceivers, and ADCs can all be integrated.
Integration of Isolation in PV Inverters
Figure 3 shows a typical

Figure 3. Isolation Implementation in a 3-Stage PV Inverter
The microtransformer based isolation can also be integrated with high current output gate drivers to provide fully isolated

Figure 4. Gate Driver Implementation in a 3-Stage PV Inverter
Usually 2.5 kV or 5 kV isolated gate drivers would be needed for the microcontroller at the dc side to communicate directly to the ac side inverters. The low side gate driver can be powered by the integrated
Each

Figure 5. Transformer Structure (a) 1 kV Gate Driver (b) 2.5 kV Gate Driver
Two 1 kV transformers, as shown in Figure 5(a), were implemented on the input chip, one for each gate driver output. The inputs are connected to the bottom coils that are isolated by 2.64 µm thick oxide from top coils, and each top coil is isolated from each other through lateral oxide isolation. The two gate driver chips sit on their own split paddles and are connected to the top coils at the input chip through
For a
Conclusion
Microtransformer based isolation integration is the ideal solution for the isolation needs for
About the Authors
Baoxing Chen is an ADI fellow. He has a Ph.D. in physics and an M.S. in electrical engineering from the University of Michigan. He is chief technologist for the Isolation Group and has been leading core iCoupler and...
Related to this Article
Industry Solutions
Product Categories
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}