Important Characteristics of Insulated Gate Drivers

May 1 2019

Figure 1

   

In power electronics, as found, for example, in drive technology, IGBTs are frequently used for high voltage and high current switching. These power transistors are voltage controlled and produce their main losses during switching. To minimize the switching losses, it is desirable to have short switching times. However, fast switching simultaneously conceals the danger of high voltage transients, which could possibly affect or even damage the processor logic. Hence, gate drivers that supply the IGBTs with the appropriate gate signals perform the function of providing short-circuit protection and influence the switching speed. However, in the selection of the gate driver, certain characteristics are critical.

Figure 1. Simple schematic of the isolated gate driver ADuM4135.

Current-Driving Capability

During switching, the transistor is briefly in a state in which both a high voltage and a high current are applied. According to Ohm’s law, this results in certain losses that depend on the durations of these states (see Figure 2). The goal is to minimize these time periods. A major impact here is the gate capacitance of the transistor, which must be charged/discharged for switching. Higher transient currents accelerate this process.

Figure 2. Simplified representation of the individual loss components of a transistor.

Drivers that can supply higher gate currents for a longer time accordingly have a favorable effect on the switching losses. The ADuM4135 from Analog Devices, Inc. (ADI), for example, can provide a current up to 4 A. Depending on the IGBT, this may allow switching times in a very low ns range.

Timing

Decisive factors for minimizing switching times are output rise time (tR), fall time (tF), and the propagation delay (tD). The propagation delay is defined as the time needed for an input edge to reach the output and is dependent on the driver output current and the output load. The propagation delay usually behaves with minimal differences between the rising and falling edges, whereby a certain pulse width distortion (PWD) arises:

238329-eq-01

Because drivers often have multiple output channels, which have different response times despite being driven by the same input, a small, additional offset, the propagation delay skew (tSKEW), is yielded.

Figure 3. Timing behavior of a gate driver with multiple outputs.

Figure 4. Simple schematic of a gate driver with multiple outputs.

Insulation Withstand Voltage

In power electronics, insulation is needed for both functional and safety reasons. Because gate drivers are used, for example, in the form of a half-bridge topology in drive technology and thereby come in contact with high bus voltages and currents, insulation is unavoidable. The functional reason is that actuation of the power stage usually occurs from the low voltage circuit and hence actuation of the high-side switch of the half bridge would not be possible due to the higher potential with a simultaneously open low-side switch. At the same time, the insulation represents reliable isolation of the high voltage section from the control circuit in the event of a fault, so that contact by humans is possible. Insulated gate drivers typically exhibit dielectric strengths of 5 kV (rms)/min or higher.

Immunity

Harsh industrial environments require the best possible immunity or interference resistance of the applications to sources of interference. For example, RF noise, common-mode transients, and magnetic interference fields are critical because they can couple into the gate driver, and can excite the power stage so that it switches at undesirable times. With insulated gate drivers, the common-mode transient immunity (CMTI) defines the ability for common mode transients between the input and the output to be rejected. For example, the ADuM4121 exhibits an excellent value of >150 kV/µs.

The addressed parameters solely represent one part of the specifications for a gate driver and do not represent a complete list. Other decisive factors can include the operating voltage, the supply voltage, the temperature range, and additionally integrated functions such as a Miller clamp and desaturation protection. Thus, a large number of different gate drivers can be selected based on the requirements of the application.

About the Authors

Thomas Brand
Thomas Brand began his career at Analog Devices in Munich in October 2015 as part of his master’s thesis. From May 2016 to January 2017, he was part of a trainee program for field application engineers at Analog Devices. A...
Latest Media 21
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project