HFAN-04.5.1: Measuring Random Jitter on a Digital Sampling Oscilloscope

Sep 2 2002

Abstract

Random jitter is playing an increasingly important role in today's high-speed digital communications systems. For example, SONET specifies that an optical transceiver has no more than 10mUIRMS of random jitter (1 UI = 1 Unit Interval = 1 bit period). This would mean for a 10Gbps system, the random jitter must be less than or equal to 1psRMS. This application note describes an improved technique for measuring sub-picosecond random jitter. Read full article.

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Product Categories

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project