HFAN-02.3.2: Maintaining Average Power and Extinction Ratio, Part 2, MAX3863 Laser Driver and DS1847 Digital Resistor

Jun 5 2002
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Read other articles in this series.

Abstract

The purpose of this application note series (Part 1 and Part 2) is to demonstrate by practical example how the laser properties can change over temperature, and how to compensate for these changes in order to maintain constant extinction ratio and average power in fiber optic transceivers. Read full article.



Related to this Article

Product Categories

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project