Abstract
This document will cover a methodology for extending the 1-Wire range to a limit of near infinity using proxies. The best analogy to describe the basic proxy is to imagine the proxy server in most companies (sometimes referred to as the company firewall). In this setup, only one computer (the proxy) has an actual connection to the Internet and the rest of the user machines only have access to the proxy. All network packets on the LAN that are intended for computers outside the LAN are repeated on the WAN and vice-versa. This idea is transferable to 1-Wire networks. Connecting to a 1-Wire network through a proxy requires a couple of software modules: the client module and the host module. The host module is the code that runs on the 1-Wire Proxy Server (a PC, MxTNI™, or microcontroller) that has hardware access to the 1-Wire network. The client module is the code that runs on the distant machines that have only network access to reach the host module. It is possible that the host module, rather than having hardware access to the 1-Wire network, could have access to a client module, which would refer to yet another host module. In this way it is possible to chain together the proxy for reaching the 1-Wire network.
Introduction
The original design of the 1-Wire protocol arose from the desire to communicate with nearby devices on a short connection. Although through careful considerations, it is possible to extend the length of this connection further than originally anticipated, the limits are still very real. For more information about the limitations, worst-case considerations, and possible solutions, see application note 148, "Guidelines for Reliable Long Line 1-Wire® Networks" and application note 159, "Software Methods to Achieve Robust 1-Wire® Communication in iButton® Applications."
This document will cover a methodology for extending the 1-Wire range to a limit of near infinity using proxies. The best analogy to describe the basic proxy is to imagine the proxy server in most companies (sometimes referred to as the company firewall). Generally, a company provides their employees with a LAN (Local Area Network), for connecting to each other's computers and sharing files. It is usually necessary for the company to provide a means of accessing the Internet (a very Wide Area Network). In this setup, only one computer (the proxy) has an actual connection to the Internet and the rest of the machines only have access to the proxy. The proxy makes all requests for Internet data on the behalf of all computers on the LAN. In this example, the proxy acts as an interface between the WAN and the LAN. All network packets on the LAN that are intended for computers outside the LAN are "repeated" on the WAN and vice-versa.
Figure 1. Proxy server example.
Figure 1 illustrates the fundamental service provided by the proxy server and that is to give access to a network that is not normally accessible by the internal computers. More specifically, the internal computers, which can reach the proxy via the LAN, have no other means of reaching the WAN without the help of the proxy. By routing information requests through the proxy server, the previously unreachable external servers can now be reached. Although a lot of the specifics change, this same fundamental idea can be applied to 1-Wire Networks. Figure 2 illustrates the basics of this application.
Figure 2. 1-Wire proxy example.
The applications in Figure 2 represent any applications that want access to the 1-Wire Network, but (for whatever reason) cannot access it directly. The reasons could be that they are too far from the network or they are operating in an environment that does not allow for hardware access (i.e., a Java™ application running on a Java-powered cell phone). Due to electrical limitations, an application using a 1-Wire network would typically be running on hardware that is located less than 200 meters from the 1-Wire slave devices. In the scenario depicted in Figure 2, all an application needs is access to the network medium and a suitable 1-Wire Proxy Server. The network medium could be anything such as a RF wireless network, an IR point-to-point link, or a TCP/IP Ethernet network. Thanks to the immensely large Wide Area Network known as the Internet, the distance between the external computers and the actual 1-Wire Network is not an issue anymore.
Overview
Connecting to a 1-Wire network through a proxy requires a couple of modules: the client module and the host module. The host module is the code that runs on the 1-Wire Proxy Server (a PC, MxTNI, or microcontroller) that has hardware access to the 1-Wire Network. The client module is the code that runs on the distant machines that have only network access to reach the host module. It is possible that the host module, rather than having hardware access to the 1-Wire Network, could have access to a client module, which would refer to yet another host module. In this way it is possible to chain together the proxy for reaching the 1-Wire Network. Figure 3 illustrates the interactivity between the 1-Wire application, the client module, the host module, and the 1-Wire Network.
Figure 3. Client/host configurations.
The way a PC normally communicates on the 1-Wire Network is through the use of an adapter, usually with a suitable 1-Wire Master for producing correct timings. The DS9097U adapter, for example, uses a DS2480B Serial 1-Wire line driver chip. The PC is connected to the DS9097U using the serial port. Commands sent through the serial port reach the DS2480B and are then translated into 1-Wire Network commands. The DS2480B returns the output of any 1-Wire Network commands through the PC's serial port. However, when communicating with the 1-Wire Network through a 1-Wire Proxy, the PC will instead call on the client module to send commands to the host module. These commands will be transmitted through the network medium (e.g., the Internet) to the host module. The host module will then communicate through a 1-Wire Master with the physical 1-Wire Network. The results of the 1-Wire communication will be returned in a buffer to the client module back through the network medium.
Implementation
The software application layer at which the repeating occurs could be any of a number of places. A 1-Wire application essentially consists of the following layers:
- Application—maintains knowledge about how the 1-Wire data is used (i.e., how to convert a block of 1-Wire communication into a temperature result in degrees Fahrenheit).
- Presentation—maintains knowledge about the different data formats and wraps this into a potentially useful API.
- Transport—maintains knowledge of how to transfer blocks of data to and from the 1-Wire Network.
- Link—maintains knowledge of how to reset the 1-Wire network and transmit ones or zeroes.
Installing a proxy at the link layer would entail transmitting serial or parallel port commands over the network. For example, if you had a host with a DS9097U adapter on one of the serial ports, the client module would send commands intended directly for the DS2480B Master chip. The serial-to-Ethernet example available on the iButton website (see Links section at end of this document) demonstrates this principle exactly. This example allows a PC to have a virtual COM port. All commands sent to this virtual COM port are transmitted over the network to another device (a PC or a MxTNI). If there is a DS9097U on the host device's serial port, it is possible for the client to treat the DS9097U as if it were directly connected.
The idea of installing a proxy at the transport layer is dealt with by a protocol specification for IEEE® 1451.4. The client module, at this layer, would not be concerned with the actual hardware used for interfacing to the 1-Wire Network, but would instead take the link layer for granted as something the host handles. The client would transmit mostly reset commands and blocks of data to (and from) the host.
The highest layer, and probably the most efficient, would be the presentation layer. A proxy of this sort is included with the 1-Wire API for Java Kit. In the 1-Wire API for Java, every suitable adapter for 1-Wire connectivity is represented by a subclass of DSPortAdapter. In object-oriented language, that means that all instances of the various kinds of adapters (serial, parallel, or USB) can all be treated as if they are instances of their parent class, DSPortAdapter. This is a case of hiding the implementation from the presentation that object-oriented programmers should be very familiar with. Because of this design choice in the 1-Wire API, it's simple to add a new subclass of DSPortAdapter that merely implements the client module discussed above. This client module, and its relationship to the host module, is depicted in the class diagram of Figure 4.
Figure 4. Class interaction diagram.
The largest problem with the use of a 1-Wire Proxy is packet latency. If the network medium has a packet turnaround time of one second, most real-time applications simply won't be possible. Ideally, the network packet latency (sometimes referred to as the PING time) should be less than the latency the PC incurs when interfacing external hardware. For example, if the packet turnaround time for any data sent to and read from the serial port is 20ms, a network packet latency of 5ms would hardly be noticeable. If the network packet latency is significantly higher, an even higher-layer implementation may be necessary to increase the real-time responsiveness of the application. To illustrate the point, here's what an example packet exchange might look like for a link-layer proxy:
Client Module transmits a serial write command to reset the DS2480B Packet = {XMIT_SERIAL, DS2480B_COMMAND_MODE, DS2480B_CMD_RESET} Server Module writes bytes to serial port. Client Module transmits a serial read command with a number of bytes to read Packet = {RECV_SERIAL, NUM_BYTES_TO_RECV} Server Module transmits bytes read from serial port, representing return value of reset command Packet = {NUM_BYTES_TO_RECV, however many bytes...} Client Module interprets return value
For each packet sent, add a multiplier for the packet latency. If multiple successive calls were made to the DS9097U in this manner, it's obvious that it can add up to a lot of network traffic rather quickly. At the presentation-layer, that exact same 1-Wire activity could be reproduced as follows:
Client Module transmits reset command Packet = {ADAPTER _CMD_RESET} Server Module transmits reset command to serial port. Then reads bytes back from serial port, and interprets the return value of reset command. Server Module transmits return value Packet = {RET_SUCCESS}
Moving the 1-Wire Proxy implementation to the application-layer could significantly reduce the packet latency problem. But since an implementation at this layer would be highly non-portable (i.e., an implementation at the application-layer would inherently be tied to a specific application), there is no reference implementation currently available. Just for the purposes of illustration, let's examine the difference with one specific application: temperature polling. A possible network packet exchange for a temperature conversion would generate numerous packets at both the link layer and the presentation layer. It would be necessary to transmit a '1-Wire Reset' command, a 'Match ROM' command, and a 'Do Temperature Convert' command. The client module would be responsible for interpreting the return value of each command as it is received in the form of a network packet from the host module. If implementing a 1-Wire Proxy at the application layer, it would only be necessary for the client module to transmit a 'Perform Complete Temperature Conversion' command. The return value from the server, in a single packet, could be just the result of the temperature conversion.
Software Interface Example
Using the client module in the 1-Wire API for Java Kit is as simple as creating an instance of the NetAdapter and passing a connection string to an initialization method. The format of the connection string is:
<hostname>:<port>:<shared secret>
Hostname is either the hostname of the PC (or MxTNI) that is running the host module or the IP address of that computer. The port is the TCP/IP port that the host is listening on. The shared secret is used for a simple form of authentication. When the client module connects to the host module, the host issues a random challenge to the client. The client then finds the CRC-16 of the random challenge bytes and the shared secret. This CRC-16 is then transmitted back to the host for verification. If the CRC-16 matches what the host calculated, the user is considered authenticated. Note that there is an additional initialization method available in NetAdapter that allows further steps for securing your connection by accepting an already established TCP/IP socket, which could be an encrypted connection.
In the 1-Wire API for Java Kit, there is a sample program that facilitates the use of the host module. This application takes all the parameters for the host module as arguments on the command-line, and uses these parameters to create an instance of NetAdapterHost. A pre-built binary is included for both the desktop and the MxTNI. Figure 5 illustrates the command line for starting the host module on the desktop using a DS9097U adapter on the COM1 serial port. The current working directory is the application folder for StartNetAdapterHost in the 1-Wire API for Java Kit.
java -cp ".;<path to onewireapi.jar>" StartNetAdapterHost -adapterName DS9097U -adapterPort COM1 -listenPort 6161 -secret "this is my secret"
Figure 5. Starting the host module on a PC.
Executing the line shown in Figure 5 on the PC will start the NetAdapterHost, which will create a listening TCP/IP socket on port 6161. The shared secret used for the simple authentication is "this is my secret". Starting the host module on a MxTNI is nearly identical. Simply ftp the StartNetAdapterHost.tini file to the MxTNI machine. Then log on and use the command-line shown in Figure 6.
java StartNetAdapterHost.tini -adapterName TINIExternalAdapter -adapterPort serial1 -listenPort 6161 -secret "this is my secret"
Figure 6. Starting the host module on a MxTNI.
Once the host module has started, incoming connections will be accepted from the client module. Figure 8 shows a remote temperature demo that demonstrates how to connect to the host and interact with a 1-Wire device. This application will connect to the specified host and look for any temperature devices. It then polls each device and displays the current temperature in both degrees Celsius and Fahrenheit. To use the sample app, simply copy-and-paste the code into a file called RemoteTemperatureDemo.java. Change the constants at the top of the class to reflect the actual setup (i.e., make sure the hostname variable has the hostname of the computer that NetAdapterHost was started on). Then execute the commands shown in Figure 7 to compile and execute this class.
javac -classpath ".;<path to onewireapi.jar>" RemoteTemperatureDemo.java java -classpath ".;<path to onewireapi.jar>" RemoteTemperatureDemo
Figure 7. Compile and run remote temperature demo.
The output of this program should be the 64-bit 1-Wire address of each temperature device that was found followed by the current temperature. If no device was found, an error message will be displayed indicating just that.
For more information about the use of NetAdapter and NetAdapterHost, see the JavaDocs for these classes. The JavaDocs for all 1-Wire classes are included with the 1-Wire API for Java Kit.
import com.dalsemi.onewire.adapter.*; import com.dalsemi.onewire.container.*; import com.dalsemi.onewire.utils.*; import java.util.Enumeration; public class RemoteTemperatureDemo { // update these variables to reflect your setup public static final String hostname = "shughes.dalsemi.com"; public static final int port = 6161; public static final String secret = "this is my secret"; public static void main (String[] args) { OneWireContainer owc = null; TemperatureContainer tc = null; // create the NetAdapter object NetAdapter adapter = new NetAdapter(); try { // connect to the NetAdapterHost adapter.selectPort(hostname + ":" + port + ":" + secret); adapter.beginExclusive(true); // find the first temperature device Enumeration e = adapter.getAllDeviceContainers(); while (tc==null && e.hasMoreElements()) { // get the next container owc = (OneWireContainer)e.nextElement(); // check if it is a temperature device if(owc instanceof TemperatureContainer) { tc = (TemperatureContainer)owc; System.out.println("Device: " + owc.getAddressAsString()); // poll the temperature device byte[] state = tc.readDevice(); tc.doTemperatureConvert(state); double temp = tc.getTemperature(state); // display temeprature result System.out.print(" " + temp + " C ("); System.out.println(Convert.toFahrenheit(temp) + " F)"); } } // if no temperature devices were found if(tc==null) System.out.println("No temperature devices found!"); } catch (Exception e) { System.out.println(e.getMessage()); } finally { adapter.endExclusive(); try { adapter.freePort(); } catch(Exception e) {;} } } }
Figure 8. Remote temperature demo.
Related to this Article
Products
Universal 1-Wire COM Port Adapter
Serial to 1-Wire Line Driver
USB to 1-Wire Bridge Chip
Product Categories
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}