Designing a Functionally Safe SIL 3 Analog Output Module with SIL 2 Components
Designing a Functionally Safe SIL 3 Analog Output Module with SIL 2 Components
Sep 8 2023
Abstract
Manufacturers requiring a safety integrity level (SIL) 3 solution face several challenges when using SIL 2 components. As Revision 3 of the industrial functional safety standard IEC 61508 is released, new methods must be employed. This article outlines a solution to overcome the challenges of successful SIL 3 implementation and reduce time to market.
Introduction
There has been a marked uptake in industrial functional safety systems over the last number of years, which has been driven by several factors such as:
- Manufacturers’ desire to use new complex technology to lower costs (for example, use of safe torque off instead of adding a second contactor)
- The use of robots, specifically collaborative robots, which has been shown to bring productivity improvements across many factory floors
- Recognizing that using safety certified equipment improves overall reliability
- Acknowledging that the use of diagnostics improves throughput in many factories and plants
- The introduction of new safety requirements
An additional driver has been the introduction of stringent requirements for the energy, oil, and gas sectors combined with regulatory obligations.
Before getting into too much detail, let’s take a look at some basic definitions to help readers of all levels better appreciate this article.
What Is Safety?
Safety is considered to be freedom from unacceptable risk. For example, an unprotected rotating machine on a factory floor would be considered unsafe.
What Is a Safety Function?
This defines an operation that must be carried out to achieve or maintain safety. The purpose of a safety function is to reduce risk in the system. For example, if that same rotating machine had a light curtain installed in front of it, the safety function would be to detect the broken light beam when a hand passes through it and stop the rotating machine before the hand has time to touch it.
Typically, a safety function has three subsystems. Figure 1 shows a safety system that is used to detect the level of a hazardous liquid and turn off the flow when it is full.
- An input subsystem used to detect a value or state (sensor, like a level sensor)
- A logic subsystem that decides if the state is hazardous (programmable logic controller (PLC))
- An output subsystem that can take an action to maintain safety (actuator)
What Is Functional Safety?
This deals with confidence that a system will carry out its intended safety function when required to do so. It is effectively a measure of how confident a functional safety engineer is that the light curtain and stopping safety function of the motor will operate when the light beam is broken.
A system is considered functionally safe if the hardware metrics (random errors), systematic capability (SC), and common cause failures (CCF) do not lead to malfunctioning of the safety system, injury or death in humans, damage to the environment, nor loss of production.
Now with some of the basic safety definitions explained, let’s consider some functional safety standards that must be adhered to when designing a functional safety system and what benefits they bring.
When following a functional safety development process like IEC 61508 or ISO 26262 for example, there are many benefits to manufacturers like:
- Improved up front requirements clarity
- Fewer bugs during testing
- Greater consistency within the software written
- Fewer defects found during integration
- More thorough testing
- Fewer defects in the field
- Improved differentiation compared to the competition
There are many safety standards (see Figure 2), most of which have been derived from the industrial IEC 61508 standard. It is worth noting that 90% to 95% of the IEC 61508 requirements are similar across all standards.
This article will focus on IEC 61508 for industrial applications and specifically how to design a SIL 3 solution with SIL 2 components using identical redundancy.
Redundancy, High Availability, and Hardware Fault Tolerance
No matter how reliable a system is, systems will eventually fail! Two common failure types are systematic and random. See Figure 3.
Redundancy is effectively having a spare or redundant path that is able to carry out the intended safety function in case a fault occurs within the safety system. It is worth noting that if a system has a level of redundancy, it does not automatically mean it has high availability. It only has high availability if the redundant path can be turned on or activated automatically. Another term commonly used within the IEC 61508 is called hardware fault tolerance (HFT). An HFT of N means the N + 1 is the minimum number of faults that could cause a loss of the safety function. It is worth pointing out that no account shall be taken of other measures that may control the effects of faults such as diagnostics. HFT is effectively a means to ensure the hardware is robust against failures while allowing you to trade off HFT vs. SFF. See Table 1.
Safe Failure Fraction of an Element | Hardware Fault Tolerance | ||
0 | 1 | 2 | |
<60% | Not allowed | SIL 1 | SIL 2 |
60% to <90% | SIL 1 | SIL 2 | SIL 3 |
90% to <99% | SIL 2 | SIL 3 | SIL 4 |
≥99% | SIL 3 | SIL 4 | SIL 4 |
Safety Integrity Level
SIL describes the integrity of a safety function and the relative level of risk-reduction provided. IEC 61508 specifies four SILs, SIL 1 having the lowest level of safety integrity and SIL 4 the highest level of safety integrity. Table 2 compares industrial IEC 61508 safety levels (SIL) to the automative (ISO 26262) safety levels (ASIL) and the avionics safety levels. Note these are only approximate comparisons.
IEC 61508 | ISO 26262 | Avionics |
SIL 1 | ASIL A | D |
SIL 2 | ASIL B | C |
SIL 3 | ASIL C/D | B |
SIL 4 | A |
As the SIL level increases in number (from SIL 1 to SIL 4), the allowed failures in time (FIT) decreases. One FIT equates to one failure per billion (1e9) hours of operation. 1e9 hours ~ 100,000 years! It is worth pointing out that no device will last one billion hours of operation, but if you operate 100,000 devices for one year you can expect one random hardware failure in that time. Safe failure fraction (SFF) is a calculation of the total safe plus dangerous detected faults compared to the total faults in a safety function.
Table 3 shows the link between safe failure fraction (SFF) and SIL for a hardware fault tolerance of zero (HFT = 0).
SIL | SFF | High Demand Rate Dangerous Failures Per Hour | Theoretically Allowed Dangerous Failures |
1 | 60% | 1e–5 (10,000 FIT) | 1 dangerous failure every 10 years |
2 | 90% | 1e–6 (1,000 FIT) | 1 dangerous failure every 100 years |
3 | 99% | 1e–7 (100 FIT) | 1 dangerous failure every 1,000 years |
Problem/Existing Solution
The problem for many designers employing functional safety, specifically those designing with ICs, is that it can be difficult and expensive to achieve certification along with the very real risk of noncompliance. A system-level FMEDA must be created, and they must treat ASICs as black boxes as they don’t know the:
- Transistor count
- Internal failure mechanisms
- Layout block sizes
- Reliability for an IC
As a result, designers must be overly conservative in their FIT calculations and overly safe in other parts of their safety system in order to achieve their overall SIL target. This generally means the use of external diagnostics like an external ADC. The problems with this are:
- More expensive (BOM)
- Larger footprint
- More complexity
- Additional overhead in system software
- Longer development time
To compound these problems, there is a new version of IEC 61508 standard coming out (Revision 3).
IEC 61508 Revision 3
Currently planned changes in IEC 61508 Revision 3 include explicit warnings about the use of on-chip diagnostics to detect failures on the same chip unless the IC was developed in compliance to IEC 61508. It is also planned to include requirements similar to automotive ISO 26262 latent fault metric. In addition to a kind of SFF for diagnostic functions, the diagnostic circuiting will also have an SC requirement.
ADFS5758: World’s First Certified Data Converter
The ADFS5758 is a single-channel, 16-bit current out DAC with integrated dynamic power control (DPC), and internal reference along with numerous on-chip diagnostics. Figure 4 shows the block diagram.
Diagnostics/Safety Measures on the ADFS5758
- Main on-chip diagnostic is an ADC; as stated previously, IEC 61508 Revision 3 plans to clarify that the use of on-chip diagnostics to detect on-chip failures is not generally allowed unless the IC was developed in compliance to IEC 61508
- Checks for valid read/write address
- ECC correction
- Watchdog timer
- The ability to lock configuration registers
- Internal bias voltage monitors
- Temperature monitor
Designed to meet the requirements of:
- Industrial factory automation
- Process control applications
- High density small form factor PLC analog I/O cards
Safety Function:
Takes a digital input code and produces an output current to within ±2.5% full-scale range (FSR).
Developed to IEC 61508:
- SIL 2 in terms of hardware metrics
- SIL 3 in terms of systematic requirements
See Figure 5 for a copy of the TUV Rheinland functional safety certificate for the ADFS5758.
Figure 6 shows the ADFS5758 being used in a typical safety application.
For a system to meet SIL requirements, then both the hardware metrics (also known as architectural constraints) and the SC must meet the SIL target.
Architectural Constraints
Placing two SIL 2 elements (identical or diverse) in parallel allows a customer to achieve a higher SIL 3 level from a hardware metrics perspective. See Figure 7.
Systematic Capability
Redundancy can be achieved by using either diverse (different) elements or identical elements.
Identical Elements
Using identical elements with the same SC does not improve the overall SC as they are both prone to the same CCF-like temperature spikes or voltage drops and the same fault could bring down both elements. See Figure 8.
Diverse Elements
Using diverse elements in a redundant configuration increases the overall system capability. See Figure 9.
The reason for this is that since the two elements are diverse or different, the same fault is unlikely to take both elements down at the same time.
The problem with this method is that it can be costly to use diverse elements in a safety system as the workload to design in and test increases significantly.
Ideally what is required here is a way to use two identical elements to meet both the SC and random or hardware metrics for the functional safety requirements.
Importance of Developing SC One Level Higher than SIL: Identical Redundancy
If an element could be employed in the system that was developed to a system capability one level higher than the SIL of the element, then two identical elements can be used in a safety system to provide redundancy along with increasing the overall system capability. See Figure 10 for an example.
Conclusion
When using the certified ADFS5758 within a safety system, there are numerous advantages:
- Less risk: What will TÜV say
- Can use on-chip diagnostics (ADC and distributed diagnostics)
- Smaller solution size/more channels in a given space (due to using integrated ADC)
- Minimizing external component count (higher reliability)
- Targeted diagnostics (lower detection time and higher coverage)
- Key numbers available for the system-level engineer (FMEDA)
- Less overhead on system software (fewer diagnostics in software)
- Reliability analysis for an assumed environment is available
- Shorter development times for customers
- Relevant documentation available (safety manual and TÜV assessment report)
- IEC 61508 Revision 3 future proof
Along with the above advantages, the ADFS5758 allows for the use of SIL 2 components to design a SIL 3 solution using identical redundancy.
If you wish to explore functional safety and the ADFS5758 further:
- Please visit the ADFS5758 product webpage to learn more.
- Order the ADFS5758 evaluation kit to gain familiarity with the part.
- View the Analog Devices Industrial Functional Safety webpage.
- Read the Analog Devices Safety Matters Blog.
About the Authors
Brian Condell is a digital marketing engineer at Analog Devices based in Limerick, Ireland. He graduated with honors from the University of Limerick with a bachelor’s degree in electrical engineering. Brian has over 25 yea...