Current-Limit Circuit for the Buck Regulator

Mar 28 2023
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

A current limit can be added to a step-down converter by using a MAX4173H current-sense amplifier to inject current into the feedback network. D1 sharpens the threshold of current limit by converting the current sense feedback signal from linear to exponential. This current-limit circuit can be scaled for any output current by adjusting R3. In this case, the MAX1692 provides up to 600mA output and the MAX4173H limits the output current by decreasing the output voltage for output current above 300mA.

Figure 1.

IL (mA) VOUT (V)
0 3.827
100 3.729
200 3.701
258 3.637 (-5%)
258 3.637 (-5%)
300 3.503
312 3.444 (-10%)
347 3.254 (-15%)
380 3.062 (-20%)
400 2.951
414 2.862 (-25%)
450 2.630
500 2.305
550 1.977
600 1.732

Additional Information:

Related to this Article

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project