ADuCM350 + AD8233 Analysis

Nov 21 2016
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Introduction

This report explains how to obtain the ECG signal using the ADuCM350 and the AD8233. The ADuCM350 and the AD8233’s evaluation board have been used in this test.

AD8233 evaluation board is supplied to 3.3V_BOARD. Therefore, ADuCM350 and AD8233 are supplied to the same voltage. The AD8233_REFIN is connected to VBIAS. The AD8233’s output is connected to AN_B. An ECG simulator has been connected to: +IN, -IN and RLD in the AD8233. The picture below shows the block diagram, it also includes the required lines to control the AD8233. Some of these control lines are optional and they can be tied to VCC or GND.

The ADuCM350’s firmware used in this analysis can be found in the ADuCM350’s examples folder. This example code is called AuxChanMeasurement. The value of the constant DUR has been modified to 5000000, the rest of the code has not been modified.

Measurements

Input Noise


The first test has been to short-circuit the +IN and -IN pins and connect them to VBIAS.

The obtained signal is shown below.

As the reader can observe, the difference between the maximum value and the minimum value is 117 LSBs. This means the noise is: 117 · 54.9 µV/LSB = 6.423 mVpp. The AD8233 gain is 1100, thus, the noise in the AD8233’s input is: 6.423mVpp/ 1100 = 5.84µVpp.

The picture below shows the AD8233 noise at 0V is 9.8µVpp typically. It means the system is not degrading the AD8233 performance, we are getting the best performance we can get with the AD8233.

Specification AD8232 New Design (AD8233)
Supply Current Typ @ 27C 180µA 60µA
.5 to 40 Hz Noise Typ, 0V differential, 27C 18.5µV pk-pk 9.8µV pk-pk
.5 to 40 Hz Noise Typ, +/ 300mV differential, 27C 22µV pk-pk 16.82µV pk-pk
.05 to 150Hz Noise Typ, 0V differential, 27C 25.6µV pk-pk 15.1µV pk-pk
.05 to 150Hz Noise Typ, +/-300mV differential, 27C 30.6µV pk-pk 25µV pk-pk
DC/60Hz CMRR Min, +/-300mV differential, 0-70C 105/74.6dB 109/78.2dB

Two electrodes measurement ECG simulator 60 BPM


After checking the ADuMC350’s performance we have tested the system using an ECG simulator. The ECG bandwidth applied in this study has been the sport bandwidth, the sport bandwidth is: 7-24Hz. This bandwidth is the recommended bandwidth if the system must obtain the Heart rate. This bandwidth makes the system more robust in front of motion artifacts, although the ECG waveform is altered.

The circuit under test and the results are shown in the pictures below.


Two electrodes measurement ECG simulator 130 BPM


Same experiment has been carried out with 130bpm. The obtained signal is shown below.


Three electrodes measurement ECG simulator 60 BPM


The experiments were being repeated with 3 electrodes. In this case, the RLD is also used. The results with the emulator are shown below.

Conclusions

The ADuCM350 and the AD8233 are 100% compatible and the ADuCM350’s ADC provides plenty resolution. Besides, the AD8233’s reference can be generated by the ADuCM350. The rest of functionalities can be perfectly carried out by this system.


Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project