Adding Three Power MOSFETs Lets a Single Step-Down Converter Drive RGB LEDs in Projectors

Mar 17 2023

Description

Introduction

This application note presents an RGB LED driver reference design for a low-power projector. This high-current LED driver is based on a single MAX16821 device that drives 10A to a set of RGB LEDs in step-down mode with less than 1µs turn-on/turn-off times. Only one color LED is driven at a time, with RGB colors sharing the PWM period in required proportions.

LED Driver Specifications:

  • Input supply voltage: 10V to 15V
  • LED drive current: 10A
  • LED forward voltage: 4.5V to 6V
  • LED current rise/fall times: < 1µs
  • LED current ripple: 10% peak to peak, max

Inputs:

  • VIN (J4): supply voltage input
  • PWMR, PWMB, PWMG (J8 pins 1, 3, and 4): RGB PWM input signals. Amplitude should be 3.3V to 5V. As output can rise/fall within 1µs, any PWM period higher than 2µs can be used. Only one of the above three signals should be high at a time.
  • PWMN (J8 pin 4): digital NOR of PWMR, PWMG, and PWMB. PWMN will be high only when all three PWM signals are low.
  • ON/OFF (J1): leave open or drive +5V to enable the driver. Connect to GND for disabling the board.

Outputs:

  • LEDR, LEDG, LEDB (J5, J6, and J7): 10A RGB LED outputs. Connect LED+ to pins 3, 4, and 5; connect LED- to pins 6, 7, and 8.
  • OUTV (J2): provides a signal proportional to the LED current. The voltage at OUTV will be 135 times the voltage across R12||R16.
  • VIN_OUT (J3): input supply-voltage output for connecting to other boards. Pins 1 and 2 are VIN+; pins 3 and 4 are GND.
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project