The MAX17599 low IQ active-clamp current-mode PWM controller contains all the control circuitry required for designing wide-input isolated forward converter industrial power supplies.
The device includes an AUX driver that drives an auxiliary MOSFET (clamp switch) that helps implement the active-clamp transformer reset topology for forward converters. This reset topology has several advantages, including reduced voltage stress on the switches, transformer-size reduction due to larger allowable flux swing, and improved efficiency due to elimination of dissipative snubber circuitry. Programmable dead time between the AUX and main driver allows for zero voltage switching.
Primary Power Stage
The active-clamp transformer primary side is driven by an n-channel MOSFET (N3) and a p-channel MOSFET (P1). While N3 is on, power is delivered to the secondary side, and magnetizing energy is being stored in the transformer. During this time, P1 is off, and the clamp capacitor (C10) is charged at a constant voltage level.
When N3 turns off, the leakage and magnetizing currents charge up the drain-to-source capacitance of N3. Once the drain-to-source voltage of N3 exceeds the voltage across the clamp capacitor, the body diode of P1 begins to conduct. With the body diode of P1 conducting, the magnetizing current begins to charge the clamp capacitor.
After the body diode of P1 conducts, P1 turns on. This provides zero current switching for the p-channel MOSFET. The clamp capacitor continues to charge until the magnetizing current is reduced to 0A. At this point, the magnetizing current reverses, and the clamp capacitor begins to discharge until the p-channel MOSFET turns off.
After P1 turns off, the clamp capacitor remains at a fixed voltage. There is a fixed delay before N3 turns on. During this delay, the energy in the parasitic components discharges the VDS of N3 towards VIN. This allows softer turn-on and lower switching losses for N3.
The MAX17599 NDRV pin drives the n-channel MOSFET while the AUXDRV pin is level shifted through C11, R9, R14, and D4, and then drives the p-channel MOSFET.
Secondary Power Stage
The secondary power stage consists of the synchronous rectifiers (N1, N2), the output filter (L1, C4, C5, and C6), and the gate driving circuit for N1 (R3) and N2 (R2).
When N3 is on, the voltage on the gate wiring of T1 ensures N2 is on, while N1 is off. During this time, a voltage equal to the input voltage multiplied by the NS:NP turns ratio of the transformer is applied across N3; the inductor and the load capacitor are charged and being stored with energy.
When N3 is off, the voltage on the gate wiring of T1 reverses and ensures N2 is off, while N1 is on. During this time, the inductor current flows through N1 and continues transferring energy to the load capacitor.
The voltage on the input end of the filter inductor is a typical buck-converter square wave. The inductor and output capacitors filter the square wave to produce DC voltage on the output.
Feedback Control Loop
A feedback network is typical of most isolated forward converters. It is constructed using a TL431V programmable shunt regulator, a 3000V isolation optocoupler, and other RC components.
Startup Voltage and Input Overvoltage Protection Setting (EN/UVLO and OVI pins)
The EN/UVLO pin in the MAX17599 serves as an enable/disable input, as well as an accurate programmable undervoltage lockout (UVLO) pin. The MAX17599 does not begin startup operations unless the EN/UVLO-pin voltage exceeds 1.21V (typ). The MAX17599 turns off if the EN/UVLO pin voltage falls below 1.15V (typ). A resistor divider from the input DC bus to ground can be used to divide down and apply a fraction of the input DC voltage to the EN/ UVLO pin. The values of the resistor-divider can be selected so that the EN/UVLO-pin voltage exceeds the 1.21V (typ) turn-on threshold at the desired input DC bus voltage. The same resistor-divider can be modified with an additional resistor, ROVI, to implement overvoltage input protection in addition to the EN/UVLO functionality. When the voltage at the OVI pin exceeds 1.21V (typ), the MAX17599 stops switching. Switching resumes with soft-start operation, only if the voltage at the OVI pin falls below 1.15V (typ). For the expected values of the startup DC input voltage (VSTART) and overvoltage input protection voltage (VOVI), the resistor values for the divider can be calculated as follows:
VSTART = (R4 + R7 + R5)/(R4 + R7) × 1.21 (V)
VOVI = (R4 + R7 + R5)/R4 × 1.21 (V)
If R4 = 24.9kΩ, R5 = 698kΩ, and R7 = 24.9kΩ, then:
VSTART = 18.2V, VOVI = 36.3V.