Overview

Design Resources

Design & Integration File

  • Schematic
  • Bill of Materials
  • Gerber Files
  • PADS Files
  • Assembly Drawing
Download Design Files 3.34 K

Evaluation Hardware

Part Numbers with "Z" indicate RoHS Compliance. Boards checked are needed to evaluate this circuit.

  • CFTL-LED-BAR ($58.85) 3-Channel RGB LED Board
  • EVAL-ADICUP3029 ($52.97) ADuCM3029 Arduino Form Factor Compatible Development System
  • EVAL-CN0397-ARDZ ($76.51) 3-Channel RGB Light Spectrum and Intensity Board
  • EVAL-CN0398-ARDZ ($82.39) Soil Moisture, pH, and Temperature Sensing Board
  • EVAL-CN0410-ARDZ ($88.28) 3-Channel LED Driver Board
Check Inventory & Purchase

Circuit Function & Benefits

The IoT smart greenhouse is an application for monitoring and controlling several important parameters that help maximize the growth of plants. The data is processed locally and sent via Wi-Fi to a local gateway, before arriving at the cloud connected platform.

Simplified System Block Diagram
Figure 1. Simplified System Block Diagram

 

Light is the single most important factor in plant growth and photosynthesis. Most plants typically absorb light in the red and orange wavelength and the blue and purple wavelength. Light in the green and yellow wavelength is typically reflected, and does not contribute much to growth or flowering.

Plants even require different spectrum of light at different intensities during their life cycle. For example, plants tend to want more blue light during sprouting and seedling, whereas red light appears to be more important during later growth stages and flowering or fruiting.

By controlling the spectrum and intensity of light the plant is exposed to during the various stages of life, the growth of the plant can be more effectively and efficiently maximized and the yield from these crops can ultimately increase.

Soil moisture, soil pH, and temperature measurements ensure that the plant has the correct amount of water and nutrients available for optimal growth conditions.

The solution is Wi-Fi enabled so that the data being collected can be displayed and viewed in a web browser on a computer or smartphone, and commands can be sent back to the system to change the light settings.

Circuit Description

The smart greenhouse application focuses on increasing the growth efficiency and maximizing the yield cycles of various types of plants. The theory and details apply to many agriculture sectors such as indoor greenhouses, vertical farming, and container farming. The smart greenhouse application addresses other general concerns for users in the agriculture market, such as keeping operating costs down and decreasing overhead (preventing over watering or wasted soil enrichment).

Smart Greenhouse Demo Photo
Figure 2. Smart Greenhouse Demo Photo

 

The smart greenhouse application hardware is made up of three different Circuits from the Lab reference designs.

The CN-0397 is designed to measure the intensity of the visible light spectrum, particularly at the wavelengths that correspond to the colors red, green, and blue (RGB). Red and blue light are absorbed by the plant and used during photosynthesis, whereas green light is reflected by the plant. Each sensor measures the intensity of light at its targeted wavelength and outputs a proportional current. The CN-0397 converts that small current into a voltage, and transforms the voltage into the standard unit of measurement for light intensity (Lux). See the CN-0397 for more information on how the circuit operates.

The CN-0410 is a programmable, 3-channel, current drive LED circuit. Each channel of RGB is independently controlled, allowing for unique LED color combinations. The board allows connection to the CFTL-LED-BAR by connecting the terminal block on each board together with a twisted pair wire. Light intensity commands are sent via Wi-Fi to the smart greenhouse, and a proportional integral (PI) software control loop between the CN-0410 and the CN-0397 is used to create the RGB color combination.

The CN-0410 also has an isolated repeater function on the board, so that the user can set multiple banks or bays of CN0410 and LED bar combinations to a single value with only a single controller board, which minimizes the cost over a large LED network. See the CN-0410 documentation (available from the circuit note webpage) for complete details on the repeater function, LED settings, and power consumption.

The CN-0398 measures three other critical parameters including soil moisture, pH, and temperature. Soil moisture measurements are important to ensure that the vegetation has the proper amount of water to promote growth, and also to ensure that water is not being unnecessarily wasted. pH monitoring is also important. pH affects nutrient availability and absorption of potentially harmful materials. Some plants germinate or flower within certain temperature requirements or profiles, and therefore the temperature measurements are used to help regulate the HVAC system. See the CN-0398 for more information on how the circuit operates.

The ADICUP3029 Arduino form factor-compatible development platform controls the Arduino shield hardware modules described previously. This platform contains the ADuCM3029 ultra low power Cortex-M3 microprocessor. The development platform also has onboard Bluetooth and Wi-Fi connectivity for connection to the internet and development of IoT connected applications.

For the smart greenhouse application, data is sent wirelessly from the node (ADICUP3029 and shield modules) to an existing wireless gateway through Wi-Fi. The Wi-Fi uses a message queuing telemetry transport (MQTT) standard protocol, which is typically used in low power, IoT sensor nodes that need to send small amounts of data to the gateway.

The IBM® Watson cloud service is used to collect and display the smart greenhouse data. Bidirectional communication receives the data and transmits it from the cloud service back down to the remote node. There are other connectivity options available. For complete details on the IBM Watson option and other cloud connection options, see the Smart Greenhouse Wiki User Guide.

IBM Watson Data Using Node Red
Figure 3. IBM Watson Data Using Node Red

Common Variations

In the current application, there is no closed loop feedback for the temperature, watering system, or adding soil nutrients. All these actions can be included in the control hardware and software as needed for the user’s system requirements. For example, the temperature reading can be tied into the HVAC system to turn on the air conditioning or heat, or the moisture reading can be used to control a valve on the irrigation system to ensure that the moisture of the soil stays within a required range.

The LED being driven may require a certain wavelength for the vegetation, and therefore may need to be customized in the user specific application. The CN-0397 can be customized to accommodate different LED sources by adjusting the peak wavelength at which the photodiodes sense the light. See the CN-0397 for information on how to change the photodiodes and gain values for full-scale usage.

Circuit Evaluation & Test

To set up the smart greenhouse system, stack the boards on stop of each other. The sensors plug directly into the designated connectors. The following sections provide the basics of how to connect the system. For complete details, see the Smart Greenhouse Wiki User Guide.


Equipment Needed

The following equipment is needed:

  • EVAL-CN0397-ARDZ
  • EVAL-CN0398-ARDZ
  • EVAL-CN0410-ARDZ
  • CFTL-LED-BAR
  • EVAL-ADICUP3029
  • Smart Greenhouse Embedded Software
  • PC with a USB port and Windows® XP or Windows Vista® (32-bit), or Windows 7 (32-bit)
  • Micro USB cable
  • Power supply: 6 V to 19 V wall wart


Getting Started

See the Smart Greenhouse Wiki User Guide for complete step by step instructions on setting up the smart greenhouse. The following are the basic steps for setup:

  1. First, configure the hardware. Ensure that the jumpers are set on each board correctly.
  2. Make sure that all the sensors are connected to the boards.
  3. Stack the shield boards on top of each other in the following order: CN-0397, CN-0410, and then CN-0398.
  4. Set up the ADICUP3029 so that the Wi-Fi module is plugged in to P1. Set the S2 switch to the Wi-Fi position (if using cloud connectivity). Otherwise, set the S2 switch to the USB position for serial terminal run mode.
  5. Plug the USB cable from the ADICUP3029 to the PC and flash the smart greenhouse firmware onto the board.
  6. Press the 3029_Reset button or power cycle the system, and follow the instructions in the Smart Greenhouse Wiki User Guide.


Functional Block Diagram

Smart Greenhouse System Functional Block Diagram
Figure 4. Smart Greenhouse System Functional Block Diagram