JFET

What is a JFET?

Definition

A JFET, or junction field-effect transistor, or JUGFET, is a FET in which the gate is created by reverse-biased junction (as opposed to the MOSFET which creates a junction via a field generated by conductive gate, separated from the gate region by a thin insulator).

For example: A p-channel JFET would consist of a bar of p-type silicon with the "drain" at one end and the "source" at the other. Between these two terminals is some n-type material connected to a "gate". A positive voltage applied to the gate creates a "depletion field" which restricts current flow between the source and drain.

Synonyms

Junction FET
Find a term alphabetically: