Overview

Product Details

The EVAL-AD7783EBZ is a fully featured evaluation board for the AD7783.The evaluation board can be connected to a PC via the parallel port. Software is provided enabling the user to perform detailed analysis of the ADC's performance.

Applicable Parts

Software

Evaluation Software

AD7783 Software
The software provided runs under Windows 2000 and will allow the user to control all the functions of the AD7783 via the printer port of a PC. The software should be installed by running the SETUP.EXE program.