Using a DDR3 Memory Module with the DS34S132
Abstract
This application note explains how to interface the DS34S132, a 32-point TDM-over-packet IC, with a DDR3 memory chip. The DS34S132 uses an external double data rate (DDR) synchronous DRAM (or DDR1) device to buffer data. The memory supplies sufficient buffer space to support a 256ms Packet-Delay Variation (PDV) for each of the 256 pseudowires (PWs)/bundles and to enable packet reordering.
Introduction
The DS34S132, a 32-port TDM-over-packet IC, uses an external double data rate (DDR) synchronous DRAM (also referred to as "DDR1") device to buffer data. The large memory supplies sufficient buffer space to support a 256ms Packet-Delay Variation (PDV) for each of the 256 individually configurable pseudowires (PWs)/bundles. The memory also enables packet reordering if the packet switch network (PSN) incorrectly arranges the packets. Since DDR3 is readily available, it is more convenient to use a DDR type 3 (DDR3) memory chip with the DS34S132. This application note explains how to interface the DS34S132 with a DDR3 memory chip.
Figure 1 shows the proposed block diagram to replace DDR1 with a FPGA and DDR3.
Figure 1. Replacing DDR1 with DDR3 and FPGA.
The DDR SDRAM interface has higher transfer rates than a typical SDRAM, due to its sophisticated timing control of electrical data and clock signals. For example, a DDR SDRAM with a 125MHz clock frequency can achieve almost twice the bandwidth (BW) of a SDRAM running at the same frequency. Thus, Maxim now uses DDR1 instead of SDRAM, which was used in the previous generation of Maxim's TDM over Packet (TDMoP) devices.
DDR3 SDRAM is a DRAM-interface specification. The actual DRAM arrays that store the data are similar to earlier types, with similar performance. DDR3 SDRAM can transfer data at four times the rate of DDR1, and thus enables higher bandwidth.
These days, DDR1 memory modules are not as widely available as DDR2 or DDR3. Unfortunately, DDR2 and DDR3 are neither backward- nor forward-compatible with DDR1. Thus, DDR2 or DDR3 memory modules will not work in DDR-equipped motherboards, and vice versa.
DDR Interface Configuration of the DS34S132
Inside the DS34S132 TDMoP device,
- The DDR1 interface must be programmed to a column-address-strobe (CAS) latency of 3.
- The "refresh rate" must be calculated and programmed to have a fast-enough interval for the DDR3 memory module.
- The clock rate for the DDR is 125MHz.
It is worth noting that DDR3 has 8 banks. The DS34S132 has only 2 bank select bits. Hence one half of the DDR3 memory module (upper banks) will be unused.
Configuration of the DDR3
DDR3 should run at a clock speed of 500MHz. This frequency is chosen since it is four times the DDR1 clock speed of 125MHz.
For the Verilog® RTL simulation, we used 8-bit data, which will have a BW of 500MHz × 2 × 8 bits. This BW is twice the BW of 125MHz × 2 × 16 bits on the DDR side. The extra BW will be used to pipeline and pass back the read data from DDR3 to the DS34S132 without use of FPGA FIFO memory. For the DDR3, we used:
- CAS latency: 8
- CAS write latency: 6
- DLL reset, then enabled.
The Micron DDR3 MT41J128M8 (16 Meg × 8 × 8 banks) specifications were used for simulation. The cycle time for the DDR3 was 1.87ns at CL = 8 (DDR3 - 1066) -187. Support for other DDR3 configurations/speed may require incremental or significant effort. The DDR3 that we used for simulation had the following specifications:
'elsif sg187 // sg187 is equivalent to the JEDEC DDR3-1066G (8-8-8) speed bin eter TCK_MIN 1875; // tCK ps Minimum Clock Cycle Time eter TJIT_PER 90; // tJIT(per) ps Period JItter eter TJIT_CC 180; // tJIT(cc) ps Cycle to Cycle jitter eter TERR_2PER 132; // tERR(2per) ps Accumulated Error (2-cycle) eter TERR_3PER 157; // tERR(3per) ps Accumulated Error (3-cycle) eter TERR_4PER 175; // tERR(4per) ps Accumulated Error (4-cycle) eter TERR_5PER 188; // tERR(5per) ps Accumulated Error (5-cycle) eter TERR_6PER 200; // tERR(6per) ps Accumulated Error (6-cycle) eter TERR_7PER 209; // tERR(7per) ps Accumulated Error (7-cycle) eter TERR_8PER 217; // tERR(8per) ps Accumulated Error (8-cycle) eter TERR_9PER 224; // tERR(9per) ps Accumulated Error (9-cycle) eter TERR_10PER 231; // tERR(10per)ps Accumulated Error (10-cycle) eter TERR_11PER 237; // tERR(11per)ps Accumulated Error (11-cycle) eter TERR_12PER 242; // tERR(12per)ps Accumulated Error (12-cycle) eter TDS 75; // tDS ps DQ and DM input setup time relative to DQS eter TDH 100; // tDH ps DQ and DM input hold time relative to DQS eter TDQSQ 150; // tDQSQ ps DQS-DQ skew, DQS to last DQ valid, per group, per access eter TDQSS 0.25; // tDQSS tCK Rising clock edge to DQS/DQS# latching transition eter TDSS 0.20; // tDSS tCK DQS falling edge to CLK rising (setup time) eter TDSH 0.20; // tDSH tCK DQS falling edge from CLK rising (hold time) eter TDQSCK 300; // tDQSCK ps DQS output access time from CK/CK# eter TQSH 0.38; // tQSH tCK DQS Output High Pulse Width eter TQSL 0.38; // tQSL tCK DQS Output Low Pulse Width eter TDIPW 490; // tDIPW ps DQ and DM input Pulse Width eter TIPW 780; // tIPW ps Control and Address input Pulse Width eter TIS 275; // tIS ps Input Setup Time eter TIH 200; // tIH ps Input Hold Time eter TRAS_MIN 37500; // tRAS ps Minimum Active to Precharge command time eter TRC 52500; // tRC ps Active to Active/Auto Refresh command time eter TRCD 15000; // tRCD ps Active to Read/Write command time eter TRP 15000; // tRP ps Precharge command period eter TXP 7500; // tXP ps Exit power down to a valid command eter TCKE 5625; // tCKE ps CKE minimum high or low pulse width eter TAON 300; // tAON ps RTT turn-on from ODTLon reference eter TWLS 245; // tWLS ps Setup time for tDQS flop eter TWLH 245; // tWLH ps Hold time of tDQS flop eter TWLO 9000; // tWLO ps Write levelization output delay eter TAA_MIN 15000; // TAA ps Internal READ command to first data eter CL_TIME 15000; // CL ps Minimum CAS Latency
FPGA Configuration
The FPGA has critical functions:
- At power-up, it initializes the DDR3 memory chip.
- Once initialization is complete, it services the following incoming DDR1 commands from the DS34S132 by converting to DDR3 commands/data.
- i. Read
- ii. Write
- iii. Precharge
- iv. Use a digital clock module (DCM) to multiply the incoming DDR1 clock (125MHz) from the DS34S132 by 4 to generate the DDR3 clock (500MHz).
- v. Use a second DCM to generate four phases of the DDR3 clock for edge timing to the DDR3. Additionally a feedback clock (out and back of an IO pad) will optimally adjust the phase relationship of these clocks to the DDR1 clock edge. This would help read data timing back to the DS34S132.
Next, the FPGA and the DDR3 memory combined will appear like a DDR1 memory for the DS34S132. The FPGA code includes DCMs and IO DDR primitives. Please download these codes and the specifications from this link here.
The FPGA used is Spartan for Verilog RTL simulation has a speed grade of -4, which should be capable of 500MHz. FPGA resources use approximately 300 flip flops with no FPGA RAM being used. We also used two DCMs to convert clock rates. To verify the operation of the DDR1-to-DDR3 conversion scheme, we ran the following tests in Verilog RTL simulations:
- Run test in DDR1 mode and log results.
- Run test in DDR3 mode via FPGA and log results.
- Monitor some DDR3 writes and read individually verified using monitor against DDR1 writes and read. Figure 2 and Figure 3 show the write and read simulation results of DDR1 and DDR3.
In this Verilog RTL simulation, we could successfully send the signal from DDR3 through FPGA to the device effectively. We also successfully read the signal from the device to DDR3. Thus, the simulation result proved that this conversion scheme from DDR1 to DDR3 test operates correctly.
Figure 2. The write simulation results of DDR1 (top) and DDR3 (bottom).
Figure 3. The read simulation results of DDR1 (top) and DDR3 (bottom).
Conclusion
We implemented a Verilog RTL simulation of FPGA with the Micron DDR3 MT41J128M8 parameter model and are confident that it will work with the DDR3 and the Spartan FPGA. However, this solution will not be successful for all DDR3s, and knowing which DDR3 to implement is the designer's responsibility. FPGA mapping was not implemented and bit file was not used.
For further information on TDMoP devices or other Maxim telecom products, please visit our contact the Tech support team.