Thermal Considerations for a UCSP Package
Abstract
The amount of power that an audio amplifier will dissipate is primarily limited by its package and external heat sink (whether a copper plane on the PCB or a metal heat sink). While more efficient amplifiers like Class D do not dissipate as much as conventional Class AB amplifiers, all amplifiers dissipate some power as heat. This application note discusses the power-dissipation capabilities of the UCSP™ package, and how that package can limit dissipated output power compared to other package options.
The UCSP Package
The UCSP is a packaging technology that eliminates the traditional plastic package used to encapsulate integrated circuits (ICs). Soldering the silicon directly to a PCB saves board space, but at the sacrifice of some of the advantages of a traditional package, especially heat dissipation.
Most packages used for audio amplifiers have some type of exposed pad that allows the substrate of the IC to be connected directly to either a heat sink or the PCB's ground plane. This design provides a low-thermal impedance path for the heat transferred from the IC to its surroundings, and thus keeps the device from overheating.
With a UCSP package, however, the IC is directly soldered to the PCB using bumps on the bottom surface of the device. While there are direct paths from the substrate to the PCB through the ground bumps and these bumps have a low thermal impedance, their area is much less than a typical exposed pad. Consequently, thermal dissipation is reduced. Nonground bumps also help dissipate heat, but at a reduced capacity compared to ground bumps. Top-side thermal dissipation through a heat sink is impractical due to the space constants of most systems using UCSP devices. The UCSP package is, moreover, not as mechanically robust as other packages typically used with heatsinks. A UCSP can actually become damaged while in contact with the heat sink. The thermal capabilities of a UCSP device are therefore determined by combining the heat dissipated by the grounded bumps with the rest of the bumps on the device.
Power Dissipation
Audio amplifiers are generally offered in multiple packages and characterized using the package option with the most power dissipation. In most cases these packages prevent the power dissipated by the package itself from limiting the possible output power.
Most ICs list the continuous power dissipation that is possible with each package option in the Absolute Maximum Ratings section of the data sheet, as shown in Figure 1. Packages with an exposed pad (TDFN in this case) generally dissipate the most power. Note that the UCSP dissipates significantly less power than the exposed package device.
Figure 1. Typical Absolute Maximum Ratings for continuous power dissipation in an audio amplifier.
Calculating Output Power Limits
When considering a package without an exposed pad, one must recognize the possibility of reduced output power caused by the package's reduced power dissipation. Alternatively, a higher load impedance can be used to maximize the efficiency and, thus, minimize the dissipation.
Class AB Amplifiers
Calculating the achievable output power depends on the type of amplifier used. Manufacturers of Class AB amplifiers typically provide a plot of power dissipation vs. output power similar to Figure 2. Depending on the amplifier, multiple graphs may be provided for different supply voltages and load impedances.
Figure 2. Power Dissipation vs. Output Power for a Class AB amplifier.
Compare the continuous power dissipation data from the Absolute Maximum Ratings (Figure 1) with the Power Dissipation vs. Output Power (Figure 2) to determine the output power possible in a given package. In this case the TDFN and µMAX® packages will not limit output power while the UCSP does. Even though this example amplifier is rated to 1.1W continuous power, only 100mW is possible in the UCSP package.
Class D Amplifiers
Class D amplifiers typically provide efficiency instead of power dissipation curves, as shown in Figure 3.
Figure 3. Efficiency vs. Output Power for a Class D amplifier.
The efficiency of Class D is much higher than for a Class AB amplifier, so the power dissipation for the same output power will be much lower. Power dissipation can be calculated using the following formula:
To achieve 1.1W of continuous output power this amplifier will dissipate 225mW. Since this power dissipation is lower than maximum output power of all the possible packages shown in Figure 1, the same output power is thus possible with each package option, including the UCSP.
Audio Source-Material Considerations
The output power of an audio amplifier is generally calculated using a 1kHz sine wave at 1% (< 6W) or 10%
Audio Source Material |
Ratio of RMS Level to Peak Level (dB) |
||
Sine Wave |
-3 |
||
Rock Music |
-10.8 |
||
Telephone Ringing |
-12.3 |
||
Classical Music |
-15.8 |
This data show that to achieve the same output power and, as a result, power dissipation, the output signal must have a significantly higher peak voltage for normal audio content when compared to sine waves.
Take, for example, the previously mentioned Class AB amplifier in a UCSP package. The continuous output voltage possible with sine waves is 2.5VP-P. With the rock music example in Table 1, the same package can withstand 6.2VP-P at the output without exceeding the package's power dissipation capabilities. A sine wave with the same peak voltage would result in 600mW delivered to an 8Ω load.
Conclusion
Clearly one must consider the power dissipation of the various package options when choosing an audio amplifier. In many cases only some, not all, package choices can achieve the same continuous output power. In fact, the UCSP often sustains less continuous power than packages with an exposed pad. One can overcome this power dissipation problem not by abandoning the benefits of UCSP, but by using more efficient Class D amplifiers instead of Class AB. That design modification will allow the UCSP package to be used in many more applications.
A translated, similar version of this article appeared in the February 2007 issue of EE Times Japan.