One IC for Multiple DC/DC Topologies: Dual Output Step-Down IC can also be used in SEPIC and Boost Applications

Introduction

Industrial systems designers and automotive manufacturers are significant consumers of power electronics, requiring the full array of available DC/DC converter topologies, including buck, boost and SEPIC in a variety of combinations. In an ideal world, each new project would be performance-optimized with its own specialized controller or monolithic converter IC, but this is unrealistic.

The reality is that each new chip used in an industrial or automotive setting must be qualified via extensive testing before it can be utilized in these demanding environments. Implementing a different IC for each application is time consuming and cost prohibitive. It is far better to have a tested and verified IC on the shelf that can be used in multiple topologies, allowing it to be reused across a variety of applications. As an example, this article will show how to use the LTC3892 step-down controller for SEPIC (step-up and down) and boost applications.

Circuit Description and Functionality

The LTC3892 is designed as a dual output synchronous buck controller with input-output voltage range 4.5V to 60V—covering the requirements for most automotive and industrial applications. In these environments, the voltage input to the converter can vary significantly, such as those resulting from cold cranking and load dumps in automotive applications, or brownouts and voltage spikes in industrial systems when plant machinery is turned off and on. The native step-down topology of the LTC3892 cannot regulate output voltages when the input drops below the output, but a SEPIC topology can.

Figure 1 shows a SEPIC solution that supports two outputs: VOUT1 is 3.3V at 10A and VOUT2 is 12V at 3A. The input voltage range is 6V to 40V. VOUT1 is implemented as a straightforward step-down converter with a power train including L1, Q1, Q2. To reduce number of components, the VPRG1 pin is connected to GND, internally programming VOUT1 to 3.3V.

Figure 1. Electrical schematic of LTC3892 in SEPIC and buck applications.

The second output of the LTC3892 is a SEPIC converter. The SEPIC power train includes L2, L3, Q3 and D1. A non-coupled SEPIC, with two discrete inductors, is employed here, expanding the range of the available inductors, an important consideration for cost-sensitive devices.

Figure 2 shows how the converter functions when faced with voltage drops, such as during cold cranking. The rail voltage VIN drops far below nominal 12V, but both VOUT1 and VOUT2 remain in regulation, providing a stable power supply to the critical loads. Figure 3 shows how the converter functions when experiencing voltage spikes, such as load dumps. VOUT1 and VOUT2 remain regulated, even as VIN flies far above the nominal 12V input.

Figure 2. Shows a cold cranking event. The rail voltage drops from 14 V to 7 V, but both VOUT1 and VOUT2 remain in regulation.

Figure 3. Load dump event. The rail voltage rises from 14 V to 24 V. However, both VOUT1 and VOUT2 stay in regulation.

Figure 4 is the demonstration circuit DC2727A, a dual output converter described herein. The SEPIC portion of the DC2727A can be easily rewired to a boost topology by removing one inductor L2 and replacing second L3 to an appropriate boost choke.

Figure 4. Demonstration circuit DC2727A. The LTC3892 controls two outputs: a noncoupled SEPIC and a step-down converter.

Conclusion

The LTC3892 is a flexible controller that can serve a variety of DC/DC converter needs in automotive and industrial environments. Although it is primarily designed for employment in synchronous buck converters, it can also be used in SEPIC and boost converter applications, simplifying the qualification testing process when these topologies are needed.

Author

Victor Khasiev

Victor Khasiev

Victor Khasiev was a senior applications engineer at ADI with extensive experience in power electronics both in ac-to-dc and dc-to-dc conversion. He holds two patents and has written multiple articles. These articles are related to using ADI semiconductors in automotive and industrial applications. Topics cover step-up, step-down, SEPIC, positive-to-negative, negative-to-negative, flyback, forward converters, and bidirectional backup supplies. His patents include efficient power factor correction solutions and advanced gate drivers. Victor enjoys supporting ADI customers by answering questions about ADI products, designing and verifying power supply schematics, laying out printed circuit boards, and troubleshooting and participating in testing final systems.