Design Note 274: 12-Bit ADC with Sequencer Simplifies Multiple-Input Applications

The LTC1851 is a new 12-bit, 1.25Msps ADC with an 8-channel input multiplexer, a programmable gain sample-and-hold and an internal reference. This Design Note describes a novel feature of the LTC1851: a programmable sequencer that can automatically control the input mux and sample-and-hold.

New ADC Automatically Converts Multiple Inputs with Different Spans at Different Rates

Let’s imagine a hypothetical application with the following inputs: input A has a range of 0V to 4.096V and needs to be sampled at 400ksps, input B needs 400ksps with a range of 0V to 2.048V, input C has a range of ±2.048V around 2.5V and needs 200ksps, input D needs 100ksps with a range of ±1.024V and is truly differential with a common mode of 2V and input E needs 100ksps with a range of 1V to 3.048V. There are both single-ended and differential, unipolar and bipolar inputs, two different spans and different required sampling rates.

The solution is the LTC1851 sequencer, which allows the user to program a repeating pattern of up to 16 independent mux addresses and configurations and allocates the bandwidth of the LTC1851 as needed. The LTC1851 can easily be programmed to read all five of these inputs continuously and automatically.

Table 1 shows a twelve-step sequence sampling input A every third conversion, input B every third conversion, input C every sixth conversion, and inputs D and E once every 12 conversions. This will result in effective sampling rates of 1.25Msps • 4/12 = 416.67ksps for inputs A and B, 208.33ksps for input C and 104.167ksps for inputs D and E. The LTC1851 handles the channel selection and input configuration and will cycle through these twelve steps automatically as conversions are performed.

Table1. Twelve Step Sequence Provides Effective Sampling Rate of 416ksps for Inputs A and B, 208ksps for Input C and 104ksps for Inputs D and E
STEP INPUT +INPUT PIN –INPUT PIN INPUT RANGE (V) MEMORY LOCATION DIFF A2 A1 A0 UNI/BIP PGA
1 A CH0 COM 0 TO 4.096 0000 0 0 0 0 0 1
2 B CH1 COM 0 TO 2.048 0001 0 0 0 1 0 1
3 C CH2 CH3 ±2.048 0010 1 0 1 0 1 1
4 A CH0 COM
0 TO 4.096  0011 0 0
0 0 0
1
5
B CH1 COM 0 TO 2.048 0100 0 0 0 1 0 0
6 D CH4 CH5 ±1.024 0101 1 1 0 0 1 0
7 A CH0 COM 0 TO 4.096 0110 0 0 0 0 0 1
8 B CH1 COM 0 TO 2.048 0111 0 0 0 1 0 0
9 C CH2 CH3 ±2.048 1000 1 0 1 0 1 1
10 A CH0 COM 0 TO 4.096 1001 0 0 0 0 0 1
11 B CH1 COM 0 TO 2.048 1010 0 0 0 1 0 0
12 E CH6 CH7 1 TO 3.048 1011 1 1 1 0 0 1

Figure 1. Simplified Block Diagram with Input Connection.

Writing and Reading the Sequencer

To write to the sequencer, RD must be high and M0 taken low (see Figure 2). The falling edge of WR enables the configuration control inputs (DIFF, A2, A1, A0, UNI/BIP and PGA) and the rising edge latches the data and advances to the next location. Subsequent WR low pulses will write up to 16 locations. After the last desired location is written, M0 should be taken high.

Figure 2. Writing the Sequencer.

To confirm the integrity of the programmed sequence, the user can read the contents of the Sequencer. WR must be high and M0 taken low (see Figure 3). An RD low pulse will output the first sequencer location on the 7 status word output pins (S6 to S0). The rising edge of RD will return the output pins to a high impedance state and advance to the next location. Subsequent RD low pulses will read through all 16 locations. The last location in the sequence will be indicated by a logic 1 on the S0 pin.

Figure 3. Reading the Sequencer.

Running the Sequencer

The M0 pin must be returned high, which will reset the pointer to location 0000 (see Figure 4). The LTC1851 will begin acquiring the input signal using the configuration stored in that location. The falling edge of CONVST will sample the inputs and begin a conversion. After the conversion, the LTC1851 will begin acquiring the next input using the configuration stored in location 0001 and the 12-bit data output word (D11 to D0), along with the 4-bit mux address (DIFFOUT, A2OUT, A1OUT, A0OUT), will be available on the data output pins. (The 12-bit output word will automatically switch format for unipolar and bipolar inputs.) When the last programmed location is reached, the sequencer will start over at location 0000. The program stored in the sequencer memory is retained as long as power is continuously applied to the part.

Figure 4. Running the Sequencer.

Conclusion

The LTC1851 greatly simplifies the task of continuously converting multiple inputs. It can be programmed to handle a wide variety of inputs and automate channel selection and input configuration. For more information see the November 2001 issue of Linear Technology magazine or the LTC1851 data sheet.

Author

Generic_Author_image

Jeff Huehn