AN-1602: Using the ADuM4135 Gate Driver with the Microsemi APTGT75A120T1G 1200 V IGBT Module

Introduction

Insulated gate bipolar transistors (IGBTs) are cost effective solutions for high voltage applications such as on-board chargers, off board chargers, dc-to-dc fast chargers, and switch mode power supplies (SMPS) applications. The switching frequency ranges from dc to 100 kHz. IGBTs can be single devices or even half bridge devices as selected for the design shown in Figure 1.

Figure 1. ADuM4135 Gate Driver Module
Figure 1. ADuM4135 gate driver module

The APTGT75A120 IGBT in the design described in this application note is a fast trench device with field stop IGBT technology that is proprietary to Microsemi Corporation®. This IGBT device also has low tail current, a switching frequency to 20 kHz, and soft recovery parallel diodes with low stray inductance due to the symmetrical design. The high level of integration with the selected IGBT gives optimal performance at high frequency, with a low junction to case thermal resistance.

Gate drive technology from Analog Devices, Inc., drives the IGBT. The ADuM4135 gate driver is a single-channel device with a typical drive capability of 7 A source and sink at >25 V operating voltage (VDD to VSS). The device has a minimum common-mode transient immunity (CMTI) of 100 kV/μs. The ADuM4135 provides supplies up to 35 V. Therefore, a ±15 V supply is adequate for this application. 

Test Setup

Electrical Setup

 
The electrical setup of the system test circuit is shown in Figure 2. A dc voltage is applied to the inputs across the full half bridge where decoupling capacitors of 900 μF (C1) are added to the input stage. The output stage is an inductor capacitor (LC) filter stage of 200 μH (L1) and 50 μF (C2), filtering the output into the load (R1) of 2 Ω to 30 Ω. Table 1 details the test setup power components. U1 is the DC supply for HV+ and HV− and T1 and T2 are a single IGBT module.

Figure 2. Electrical Setup of the System Test Circuit
Figure 2. Electrical setup of the system test circuit

A complete electrical setup is shown in Figure 3 and Table 2 gives the full list of equipment used in the test.

Table 1. Test Setup Power Components
Equipment Value
IGBT Module, T1, T2 APTGT75A120T1G1
U1 200 V to 900 V
Capacitor C1 900 μF
Inductor L1 200 μH
Capacitor C2 50 μF
Load Resistor R1 2 Ω to 30 Ω
Table 2. Complete Setup Equipment
Equipment Manufacturer Part Number
Oscilloscope Agilent DSO-X 3024A, 200 MHz
DC Supply Delta Elektronika SN660-AR-11 (two in serial)
Gate Driver Board WATT&WELL ADUM4135-WW-MS-02 SN001
Waveform Generator Agilent 33522A
Current Probe Hioki 3275
Current Probe Hioki 3276
Passive Voltage Probe Keysight N2873A, 500 MHz
Passive High Voltage Probe Elditest GE3421, 100 MHz
High Voltage Differential Probe Tektronix P5200
High Voltage Differential Probe Testec TT-SI 9110
Thermal Camera Optris PI 160
Figure 3. Connection Diagram for Gate Driver Power Board Testing
Figure 3. Connection diagram for gate driver power board testing

Test Results

No Load Testing

 
In a no load testing setup low output current is drawn at the output of the module. In this application, a 30 Ω resistor is used.

Table 3 shows important elements of the electrical test setup with no load along with the low current flowing within the load. Table 4 shows the temperature observed across the module. Table 3 and Table 4 contain summaries of the observed results. Figure 5 to Figure 10 show the test results of the switching waveforms across various voltages and switching frequencies.

As shown in Table 3, Test 1 and Test 2 are carried out at 600 V. Test 1 is carried out at a 10 kHz switching frequency, and Test 2 is carried out at a 20 kHz switching frequency. Test 3 is carried out at 900 V with a switching frequency of 10 kHz.

Figure 4 shows the electrical setup for no load testing.

Figure 4. Electrical Setup for No Load Testing
Figure 4. Electrical setup for no load testing
Table 3. No Load Testing, Figure Assignments
Test DC Voltage, VDC1, (V) Switching Frequency, fSW, (kHz) Duty Cycle (%) IIN2 (A) Reference Figures
1 600 10 50 0.007 Figure 5 and Figure 6
2 600 20 50 0.013 Figure 7 and Figure 8
3 900 10 50 0.009 Figure 9 and Figure 10

1 VDC is the HV+ and HV− voltage.
2 IIN is the input current through U1.

Table 4. No Load Testing, Temperature Summary1
Test VDC (V) fSW (kHz) Temperature DC-to-DC Power Supply Temperature Gate Driver Temperature
Ambient (°C) Heat Sink (°C) High-Side (°C)2 Low-Side (°C)2 High-Side (°C) Low-Side (°C)
1 600 10 26 30.8 34 34 38.2 37.6
2 600 20 26 31 35 35 39.5 39.4
3 900 10 26 31 34.2 34.2 38.6 37.7

1 All temperatures are recorded with a thermal camera.
2 Measured from transformers.

Performance Graphs for Turning IGBT On and Off

 
The test results in this section show the switching waveforms at various voltage of interest where fSW = 10 kHz and 20 kHz. VDS is the VDRAIN source and VGS is the VGATE source.

Figure 5. VDC = 600 V, fSW = 10 kHz, No Load
Figure 5. VDC = 600 V, fSW = 10 kHz, no load
Figure 6. VDC = 600 V, fSW = 10 kHz, No Load
Figure 6. VDC = 600 V, fSW = 10 kHz, no load
Figure 7. VDC = 600 V, fSW = 20 kHz, No Load
Figure 7. VDC = 600 V, fSW = 20 kHz, no load
Figure 8. VDC = 600 V, fSW = 20 kHz, No Load
Figure 8. VDC = 600 V, fSW = 20 kHz, no load
Figure 9. VDC = 900 V, fSW = 10 kHz, No Load
Figure 9. VDC = 900 V, fSW = 10 kHz, no load
Figure 10. VDC = 900 V, fSW = 10 kHz, No Load
Figure 10. VDC = 900 V, fSW = 10 kHz, no load

Load Testing

 
The test configuration is similar to the test setup (see Figure 4) of the no load tests in the No Load Testing section. Table 5 summarizes the observed results, and Figure 11 to Figure 16 show the test performance and results across various voltages, frequencies, and loads.

Test 4 is carried out at 200 V at a 10 kHz switching frequency with a 25% duty cycle. Test 5 is carried out at 600 V at a 10 kHz switching frequency with a 25% duty cycle. Test 6 is carried out at 900 V at a 10 kHz switching frequency with a 25% duty cycle.

Table 5. Load Testing
Test VDC (V) fSW (kHz) Duty Cycle (%) IOUT1 (A) VOUT2 (V) POUT3 (W) IIN (A) Reference Figures
4 200 10 25 1.8 49.3 90.2 0.55 Figure 11 and Figure 13
5 600 10 25 5.4 146.5 791.1 1.62 Figure 12 and Figure 14
6 900 10 25 7.8 214 1669.2 2.5 Figure 15 and Figure 16

1 IOUT is the output current in Load Resistor R1.
2 VOUT is the output voltage across R1.
3 POUT is the output power (IOUT × VOUT).

Performance Graphs for Turning IGBT On and Off and No Load Testing

 
The test results in this section show switching waveforms at various voltage of interest across fSW = 10 kHz and 20 kHz.

Figure 11. VDC = 200 V, fSW = 10 kHz, POUT = 90.2 W
Figure 11. VDC = 200 V, fSW = 10 kHz, POUT = 90.2 W
Figure 12. VDC = 600 V, fSW = 10 kHz, POUT = 791.1 W
Figure 12. VDC = 600 V, fSW = 10 kHz, POUT = 791.1 W
Figure 13. VDC = 200 V, fSW = 10 kHz, POUT = 90.2 W
Figure 13. VDC = 200 V, fSW = 10 kHz, POUT = 90.2 W
Figure 14. VDC = 600 V, fSW = 10 kHz, POUT = 791.1 W
Figure 14. VDC = 600 V, fSW = 10 kHz, POUT = 791.1 W
Figure 15. VDC = 900 V, fSW = 10 kHz, POUT 1669.2 W
Figure 15. VDC = 900 V, fSW = 10 kHz, POUT 1669.2 W
 Figure 16. VDC = 900 V, fSW = 10 kHz, POUT 1669.2 W
Figure 16. VDC = 900 V, fSW = 10 kHz, POUT 1669.2 W

High Current Testing

 
The test configuration is similar to the physical setup shown in Figure 3. Table 6 summarizes the observed results, and Figure 17 to Figure 20 show the test performance and results across various voltages, frequencies, and loads.

The output load resistor is varied for individual tests, as shown i n Table 1, where 2 Ω and 30 Ω loads are used to vary the current. VOUT is measured as the voltage across R1.

Test 7 is carried out at 300 V at a 10 kHz switching frequency with a 25% duty cycle. Test 8 is carried out at 400 V at 10 kHz switching frequency with 25% duty cycle.

Table 6. High Current Testing
Test VDC (V) fSW (kHz) Duty Cycle (%) IOUT (A) VOUT (V) PIN1 (W) IIN (A) Reference Figures
7 300 10 25 19.6 68.7 1346.3 5 Figure 17 and Figure 19
8 400 10 25 25.8 91.7 2365.9 6.6 Figure 18 and Figure 20

1PIN is the input power (IIN × VIN) where VIN is the dc source power supply.

Performance Graphs for Turning IGBT On and Off with Load Testing

 
The test results in this section show switching waveforms at various voltage of interest across fSW = 10 kHz and 20 kHz.

Figure 17. VDC = 300 V, fSW = 10 kHz, POUT = 1346.3 W
Figure 17. VDC = 300 V, fSW = 10 kHz, POUT = 1346.3 W
Figure 18. VDC = 400 V, fSW = 10 kHz, POUT = 2365.9 W
Figure 18. VDC = 400 V, fSW = 10 kHz, POUT = 2365.9 W
Figure 19. VDC = 300 V, fSW = 10 kHz, POUT = 1346.3 W
Figure 19. VDC = 300 V, fSW = 10 kHz, POUT = 1346.3 W
Figure 20. VDC = 400 V, fSW = 10 kHz, POUT = 2365.9 W
Figure 20. VDC = 400 V, fSW = 10 kHz, POUT = 2365.9 W

Desaturation Testing

 
The electrical setup of the system test circuit is shown in Figure 21. A dc voltage is applied to the inputs across the full half bridge, where decoupling capacitor of 900 μF are added to the input stage. This setup is used to test the desaturation detection. In this application, the maximum IC = 150 A, where IC is the current through T1 and T2.

Figure 21. Electrical Setup of the System Test Circuit
Figure 21. Electrical setup of the system test circuit

The high-side switch of the IGBT (T1) is bypassed by an inductor of 83 μH, and the T1 switch must be off.

The low-side switch of the IGBT (T2) is driven for 50 μs every 500 ms.

Table 7 details a list of the power components of the desaturation testing setup.

Figure 22 shows a switching event at 135 A in the inductor L1, and Figure 23 shows a desaturation detection at 139 A in the inductor L1.

Table 7. Test Setup of the Power Components for Desaturation Testing
Equipment Value
U1 0 V to 80 V
C1 900μF
L1 83 μH
Figure 22. VDC < 68 V, fSW = 2 Hz, Duty Cycle = 0.01%
Figure 22. VDC < 68 V, fSW = 2 Hz, Duty Cycle = 0.01%
Figure 23. VDC > 68 V, fSW = 2 Hz, Duty Cycle = 0.01%
Figure 23. VDC > 68 V, fSW = 2 Hz, Duty Cycle = 0.01%

Application Schematic

Figure 24. ADuM4135 Gate Driver Board Schematic
Figure 24. ADuM4135 gate driver board schematic

Conclusion

The ADuM4135 gate driver has the current drive capability, proper power supply range, and a strong CMTI capability of 100 kV/μs to deliver optimal performance when driving IGBTs.

The test results in this application note provide data that demonstrate that the ADuM4135 evaluation board is a solution for high voltage applications driving IGBTs.

Author

Martin Murnane

Martin Murnane

Martin Murnane is a member of the Solar PV Team at Analog Devices in Limerick, Ireland. He previously held roles in ADI’s Automotive Team. Prior to joining ADI, he worked in several roles involving application development in energy recycling systems (Schaffner Systems), Windows-based application software/database development (Dell Computers), and product development using strain gauge technology (BMS). He holds an electronic engineering degree and an M.B.A. from the University of Limerick.