AN-1352: Calibration Procedures for the ADA4571

Introduction

The ADA4571 is an analog anisotropic magnetoresistive (AMR) angle sensor consisting of a sensing element and a conditioning analog instrumentation amplifier. This application note discusses various simple calibration procedures to reduce the angle linearity error from the sensor. The AMR angle sensor element consists of two resistive Wheatstone bridges. Each Wheatstone bridge is completely independent within the sensor. Resistive mismatches occur due to minor process variations. These mismatches appear as electrical offsets and amplitude variations between the two bridges. To achieve the most accurate result from the AMR sensor, it is important to perform simple calibration routines.

Figure 1. Typical Measurement Configuration for an AMR Angle Sensor.
Figure 1. Typical Measurement Configuration for an AMR Angle Sensor.

Calibrating the ADA4571

Single Point, End Of Line (EOL) Calibration Procedure for the ADA4571


Figure 2 and Figure 3 show the typical accuracy over temperature that can be achieved with a room temperature calibration with gain control (GC) mode enabled and GC mode disabled.

Figure 2. Angular Error over Temperature After Calibration at Room Temperature, GC Enabled.
Figure 2. Angular Error over Temperature After Calibration at Room Temperature, GC Enabled.
Figure 3. Angular Error over Temperature After Calibration at Room Temperature, GC Disabled.
Figure 3. Angular Error over Temperature After Calibration at Room Temperature, GC Disabled.

The two angle relevant output voltages for the ADA4571 AMR magnetic field angle are VSIN and VCOS. The following equations represent these two outputs throughout an entire magnetic field rotation when referenced to VDD/2:

VSIN = AS × sin(2 × α + θS) + OS

where:

AS is the amplitude of VSIN.
α is the current magnetic field angle.
θS is the phase of VSIN.
OS is the offset of VSIN.

VCOS = AC × cos(2 × α + θC) + OC

where:

AC is the amplitude of VCOS.
α is the current magnetic field angle.
θC is the phase of VCOS.
OC is the offset of VCOS.

Typical output signals are shown in Figure 4.

Figure 4. Typical Output Signals over a Single Mechanical Revolution.
Figure 4. Typical Output Signals over a Single Mechanical Revolution.

The amplitude mismatch (k) between the VSIN and VCOS channels is production tested and specified as ±1% maximum. However, typically, this mismatch is much lower. Figure 5 shows the distribution of the amplitude mismatch over a sample of devices.

Figure 5. Sample Test Distribution of Sine/Cosine Amplitude Mismatch.
Figure 5. Sample Test Distribution of Sine/Cosine Amplitude Mismatch.

Figure 6 shows the theoretical error contribution from amplitude mismatch.

Figure 6. Theoretical Error Contribution due to Amplitude Mismatch of Sine/Cosine Outputs.
Figure 6. Theoretical Error Contribution due to Amplitude Mismatch of Sine/Cosine Outputs.

This error is typically much smaller than other errors in the system. In addition, any miscalculation in an attempt to correct for amplitude mismatch can result in extra error added to the system. Therefore, ignore amplitude mismatch correction.

The orthogonality error between the VSIN and VCOS channel is specified at 0.05° maximum though typically is much lower. Therefore, negligible error contribution is the result of orthogonality error; therefore, ignore this factor also.

Because of ignoring the amplitude mismatch and phase errors from the respective channels, the representative equations simplify to:

VSIN = A × sin(2 × α) + OS

where A is the amplitude of the sine and cosine channels.

VCOS = A × cos(2 × α) + OC

Offset only remains as the primary error contributor to the end angle.


Single-Temperature Calibration for the ADA4571


Complete the following steps to calibrate the device through an entire 360° rotation. Note, if possible, it is recommended to complete the following routine as close as possible to the final application temperature:

  1. Turn the magnetic stimulus through an entire 360° revolution in either direction while continuously monitoring the VSIN and VCOS outputs of the device.
  2. Calculate the offset of VSIN and VCOS independently. Calculate the offset either by the maximum and minimum or by the mean of the respective output as shown in the following equations:

Equation 01

Final Angle

To calculate the final electrical angle using the arctangent2 function.

Equation 02

The result repeats twice for each full 3600 magnetic rotation (see Figure 7). This is a function of the AMR technology.

Figure 7. Calculated Angle over an Entire Mechanical Revolution.
Figure 7. Calculated Angle over an Entire Mechanical Revolution.

Two-Temperature EOL Calibration for the ADA4571


To reduce further the error across the wide temperature span of the device, complete a two-temperature EOL calibration. Use the on-board temperature sensor to monitor the temperature at the device under test (DUT).

Because this calibration procedure uses the temperature sensor integrated into the ADA4571, the two-temperature calibration procedure does not require an accurate temperature forcing system to complete or any other temperature monitoring device during operation. As long as the system can go into a hot and cold temperature relative to the operating temperature range of the end application, this type of calibration performs well.

Figure 8 shows typical data of both the sine and cosine outputs for the remaining offset due to the offset drift of the ADA4571 after the single point calibration scheme at 25°C. For the two-temperature calibration procedure, this data set was examined.

Figure 8. Sine and Cosine Remaining Offset After a Single Point Calibration at 25°C.
Figure 8. Sine and Cosine Remaining Offset After a Single Point Calibration at 25°C.

With a single point calibration scheme at room temperature, the device achieves typical angular error results (see Figure 3). However, a two-temperature calibration increases accuracy over the entire operating temperature.

Figure 9, Figure 10, and Figure 11 show the remaining offset of the ADA4571 after a two-point calibration at a few different chosen temperature points. If these temperatures are altered, a different remaining offset profile is the result. To reduce the effect of the offset drift, it is best to choose two calibration temperatures that span nearly the entire operating temperature range in the final application. A lower magnitude of the remaining offset over the entire operating temperature range results in a more accurate angle calculation.

Figure 9. Sine and Cosine Remaining Offset After a Two-Point Calibration at 0°C and 110°C.
Figure 9. Sine and Cosine Remaining Offset After a Two-Point Calibration at 0°C and 110°C.
Figure 10. Sine and Cosine Remaining Offset After a Two-Point Calibration at 20°C and 80°C.
Figure 10. Sine and Cosine Remaining Offset After a Two-Point Calibration at 20°C and 80°C.
Figure 11. Sine and Cosine Remaining Offset After a Two-Point Calibration at 20°C and 50°C.
Figure 11. Sine and Cosine Remaining Offset After a Two-Point Calibration at 20°C and 50°C.

Using the same analysis to reduce the output terms as described in in the Single Point, End of Line (EOL) Calibration Procedure for the section, the two outputs terms reduce to:

VSIN = A × sin(2 × α) + OS

VCOS = A × cos(2 × α) + OC

However, a correction factor for the offset drift over temperature must be considered. Add this correction factor to the end of the VSIN and VCOS equations as follows:

VSIN = A × sin(2 × α) + OS1 + TCS × (VTEMP_CURVTEMP1)

where:

OS1 is the sine channel offset at Temperature 1 (T1).
VTEMP_CUR is the VTEMP output voltage at the current operating temperature.
VTEMP1 is the VTEMP output voltage at T1.
TCS is the temperature coefficient of the sine channel and equals:

Equation 03

where:

OS2 is the sine channel offset at Temperature 2 (T2).
VTEMP2 is the VTEMP output voltage at T2.

VCOS = A × cos(2 × α) + OC1 + TCC × (VTEMP_CURVTEMP1)

where:

OC1 is the sine channel offset at T1. TCC is the temperature coefficient of the cosine channel and equals:

Equation 04

where:

OC2 is the cosine channel offset at Temperature 2.

To achieve the following ideal equations, both the initial calibrated offset as well as the drift must be subtracted from the previous equations:

VSIN = A × sin(2 × α)

VCOS = A × cos(2 × α)

The routine for a two-temperature calibration requires monitoring one additional pin on the device, the VTEMP pin.

Procedure for Two-Temperature Calibration

Complete the following steps for proper two-temperature calibration for the ADA4571:

  1. Bring the system to T1 and hold the temperature steady during Step 2.
  2. Turn the magnetic stimulus through an entire 360° revolution in either direction while continuously monitoring the VSIN and VCOS outputs of the device. Monitor the VTEMP output to record temperature information for VTEMP1.
  3. Calculate the offset of VSIN (OS1) and VCOS (OC1) independently using the same scheme as described in the Single-Temperature Calibration for the ADA4571 section.
  4. Bring the system to T2 and hold the temperature steady during Step 5.
  5. Turn the magnetic stimulus through an entire 360° revolution in either direction while continuously monitoring the VSIN and VCOS outputs of the device. Monitor the VTEMP output to record temperature information for VTEMP2.
  6. Calculate the offset of VSIN (OS2) and VCOS (OC2) independently using the same scheme as described in the Single-Temperature Calibration for the ADA4571 section.
  7. Calculate the offset temperature coefficient for each channel by using the following equations:

Equation 05

Final Angle

To correct for offset drift during operation of the device, monitor the VTEMP pin channel. Calculate the final angle by:

Equation 06

Dynamic Calibration Procedure for the ADA4571


Dynamic calibration only performs in a free running application where the sensor goes through entire electrical rotations faster than the environment is changing. In general, this condition requires an electrical revolution faster than 1 Hz. For an end of shaft magnetic configuration, an electrical revolution of 1 Hz equates to a motor spinning at 30 rpm. Dynamic calibration in slower motors are possible; however, the accuracy of the dynamic calibration depends on the motor speed relative to the speed of temperature change in the system.

Dynamic calibration is similar to a single point calibration in that only offset correction is needed to achieve the desired accuracy. However, the offset correction factor constantly updatesto increase the accuracy. It is recommended to use the ADA4571 with its GC mode enabled when performing a dynamic calibration because it increases the signal-to-noise ratio (SNR), thereby decreasing the angular error of the device.

Using the simplified equations from the Single Point, End of Line (EOL) Calibration Procedure for the section, the only two factors that must be calculated are the offsets of the sine and cosine channels.

VSIN = A × sin(2 × α) + OS

VCOS = A × cos(2 × α) + OC

During the first full rotation of the device, the offsets of the sine and cosine channels are unknown; therefore, use either a single point EOL calibration scheme or let OS = OC = 0. Setting OS = OC = 0 results in a start-up accuracy that is specified by the uncorrected error section and uncorrected error typical performance characteristics found in the ADA4571 data sheet until it is adjusted for offset in future mechanical rotations.

The external controller must save the maximum and the minimum values for both the sine and cosine channels during the first full revolution. Use these values to determine the offset of each channel independently. It is important that the sensor go through an entire mechanical revolution, not only a single electrical revolution for the purpose of offset correction. For a single dipole magnet in the end of shaft mounting configuration, one mechanical revolution produces two sinusoidal cycles for both the VSIN and VCOS outputs. Each cycle has a slightly different offset; therefore, capturing the minimum and maximum values over two cycles results in the average offset for each channel, resulting in the most accurate value to use in dynamic calibration.

Figure 12 shows the difference between the AMR electrical angle and the mechanical angle for the end of shaft magnet configuration.

Figure 12. Magnetic vs. Mechanical Angle for End of Shaft Magnet Configuration.
Figure 12. Magnetic vs. Mechanical Angle for End of Shaft Magnet Configuration.

Equation 07

The accuracy of a dynamic calibration depends on how accurately the offset of each channel was calculated. When a motor is spinning quickly, at 1000 rpm or more, it is best to use dynamic calibration. At 1000 rpm, the electrical cycles are orders of magnitude faster than the temperature change in environment. In this case, the minimum and maximum values used to calculate the offset were taken from multiple mechanical cycles to ensure that an accurate offset was calculated.

In calculating the final electrical angle calculation, complete the same procedure as used for the single point calibration; however, OS and OC update continuously as follows:

Equation 08

Author

Generic_Author_image

Robert Guyol