AN-111: Single-Supply Wien Bridge Oscillator
Wien bridge oscillators have the advantage of requiring only one op amp, and this advantage is particularly important for battery-oriented applications. The oscillator circuit operates from a single 9V battery.
The conditions for Wien bridge oscillation are:
where β is the ratio of output voltage feedback to the inverting input. If R1 = R2 and C1 = C2, then ωO is 1/RC and β is 1/3.
This oscillator should be set to just diverse in amplitude. Diodes are used to obtain a nonlinear feedback characteristic which will limit the divergence without causing too much distortion. The condition for oscillation is:
As a design example, consider:
C1 = C2 = 0.01μF
R1 = 15.8kΩ
2R2 = 31.8
R3 = 50kΩ
R4 = 10kΩ
R5 = 40kΩ nominally
Diodes = 1N914 or 1N4148
RS = 1MΩ
Using these component values, fO will be 1004Hz. Resistor R5 must be adjusted for best amplitude stability. If R5 is too low, the oscillation might converge; if too large, then the oscillation will diverge until the output clips. An oscillation output of 6V peak-to-peak when operating from a 9V battery is recommended. Resistor R5 needs to be a nominal 40kΩ with a ±2.5kΩ adjustment range.
The OP-22 is operated with a 1MΩset resistor for a set current of 7.8μA which corresponds to a supply current of approximately 100μA. Gain-bandwidth product and slew-rate vary directly with the set current, so RS should be optimized for the specific oscillation frequency. Supply drain can be reduced for lower frequencies. The OP-22 works well for frequencies in the range of 100Hz to 1kHz; the OP-27 is recommended for higher frequencies.
Figure1.