ADALM2000 Activity: The CMOS Analog Switch

Objective

The objective of this exercise is to explore the use of complementary MOS transistors as an analog voltage switch.

Concept

The ideal analog switch has no on-resistance, infinite off-impedance, and zero-time delay, and can handle large signal and common-mode voltages. Real analog switches made with MOS transistors meet none of these criteria, but if we understand the limitations of analog switches, most of these limitations can be overcome. The on-resistance is one of these limitations, and this lab activity will attempt to characterize this switch specification.

Materials

  • ADALM2000 Active Learning Module
  • Solderless breadboard
  • Jumper wires
  • One CD4007 CMOS transistor array
  • Two NPN transistors (2N3904 or equivalent)
  • One 4.7 kΩ resistor
Figure 1. CD4007 CMOS transistor array pinout.
Figure 1. CD4007 CMOS transistor array pinout.

NMOS Directions

Construct the test circuit shown in Figure 2. The blue boxes indicate connections to the connector on the ADALM2000. NMOS and PMOS devices M1 and M2 are contained in the CD4007 package. All unused pins can be left floating. To measure the on-resistance (RON) of the MOS transistors we first need to force a known current through the resistance and then measure the voltage across the resistance. The two NPN devices Q1 and Q2 along with resistor R1 form a current source with an output current of approximately 1 mA. The exact magnitude of this current is not important in that we are mainly interested in the change in the RON of the MOS devices as the voltage at their source/drain varies over the range of between the plus and minus power supplies.

In this first test, only NMOS device M1 is turned on and PMOS device M2 is turned off.

Figure 2. NMOS R<sub>ON</sub> test circuit.
Figure 2. NMOS RON test circuit.

Hardware Setup

Connect the circuit shown in Figure 2 to a breadboard.

Figure 3. NMOS R<sub>ON</sub> test circuit breadboard connections.
Figure 3. NMOS RON test circuit breadboard connections.

Procedure

Configure waveform generator 1 as a 100 Hz triangle wave with an amplitude of 9 V peak-to-peak and an offset of 500 mV. This will swing the voltage on the NMOS switch transistor from +5 V to –4 V. We cannot swing the voltage all the way to –5 V because of the NPN current source Q2. Be sure to turn on the external user power supplies (Vp and Vn) before running the waveform generator. Configure the scope screen in XY mode with Channel 1 on the x-axis, and Channel 2 (the voltage across the switch) on the y-axis. Use the math function to calculate the resistance (C2 / 1 mA). Note: You can get a more precise estimate of the current source by measuring the voltage across R1 and its actual resistance.

Configure the oscilloscope instrument to capture several periods of the two signals being measured. An XY plot example using Scopy is presented in Figure 4.

Figure 4. NMOS R<sub>ON</sub> XY trace.
Figure 4. NMOS RON XY trace.

PMOS Directions

Now modify your circuit to look like Figure 5 by connecting the gates of both M1 and M2 to the negative power supply Vn. In this second test, only PMOS device M2 is turned on and NMOS device M1 is turned off.

Figure 5. PMOS R<sub>ON</sub> test circuit.
Figure 5. PMOS RON test circuit.

Hardware Setup

Connect the circuit shown in Figure 5 to a breadboard.

Figure 6. PMOS R<sub>ON</sub> test circuit breadboard connections.
Figure 6. PMOS RON test circuit breadboard connections.

Procedure

Repeat the sweep of the voltage from the previous section and plot the on-resistance of just the PMOS transistor.

Configure the oscilloscope instrument to capture several periods of the two signals being measured. An XY plot example using Scopy is presented in Figure 7.

Figure 7. PMOS R<sub>ON</sub> XY trace.
Figure 7. PMOS RON XY trace.

CMOS Directions

Now modify your circuit to look like Figure 8 by connecting the gate of M1 to the positive power supply Vp and the gate of M2 to the negative power supply Vn. In this last test, both NMOS device M1 and PMOS device M2 are turned on.

Figure 8. CMOS R R<sub>ON</sub> test circuit.
Figure 8. CMOS RON test circuit.

Hardware Setup

Connect the circuit shown in Figure 8 to a breadboard.

Figure 9. CMOS R<sub>ON</sub> test circuit breadboard connections.
Figure 9. CMOS RON test circuit breadboard connections.

Procedure

Repeat the sweep of the voltage from the previous section and plot the on-resistance of the combined NMOS and PMOS transistors.

Configure the oscilloscope instrument to capture several periods of the two signals being measured. An XY plot example using Scopy is presented in Figure 10.

Figure 10. CMOS R<sub>ON</sub> XY trace.
Figure 10. CMOS RON XY trace.

Questions:

  • For the circuit in Figure 2, at what voltage does the NMOS device turn off?
  • For the circuit in Figure 2, what happens to the drain-to-source voltage as the NMOS transistor turns off?
  • For the circuit in Figure 5, at what voltage does the PMOS device turn off?
  • For the circuit in Figure 5, what happens to the source-to-drain voltage as the PMOS transistor turns off?

You can find the answers at the StudentZone blog.

Authors

Antoniu Miclaus

Antoniu Miclaus

Antoniu Miclaus is a software engineer at Analog Devices, where he works on embedded software for Linux and no-OS drivers, as well as ADI academic programs, QA automation, and process management. He started working at ADI in February 2017 in Cluj-Napoca, Romania. He holds an M.Sc. degree in software engineering from the Babes-Bolyai University and a B.Eng. degree in electronics and telecommunications from the Technical University of Cluj-Napoca.

Doug Mercer

Doug Mercer

Doug Mercer received his B.S.E.E. degree from Rensselaer Polytechnic Institute (RPI) in 1977. Since joining Analog Devices in 1977, he has contributed directly or indirectly to more than 30 data converter products and holds 13 patents. He was appointed to the position of ADI Fellow in 1995. In 2009, he transitioned from full-time work and has continued consulting at ADI as a fellow emeritus contributing to the Active Learning Program. In 2016, he was named engineer in residence within the ECSE department at RPI.