Energy harvesting has been around for a very long time. I still remember my 1980s pocket calculator with a solar cell powering the computing unit as well as the LCD display. But even much before that, usable energy was harvested in the early days of the electrical revolution by putting generators on river mills that were powered by running water to generate electricity. Today, when we talk about energy harvesting, we usually use the term for a power source to replace battery cells in electric equipment. So the example of the pocket calculator from the 1980s fits quite well into what we try to achieve today with “energy harvesting.”
Setup of an Energy Harvesting System
The most important item in energy harvesting systems is obviously a harvester, and the most common one is a solar cell. The electricity generated by the harvester needs to be converted into a useful voltage or current to power the system or charge intermediate energy storage devices such as super capacitors and batteries. When the system is powered, the correct voltage for the electronics needs to be generated. Figure 1 shows the power management unit fulfilling many different tasks. Matching the input impedance to allow for maximum harvested energy, charging an intermediate energy storage, routing power from a conventional primary cell battery, generating the correct output voltage for the system, and monitoring current flows and voltages to generate a reliable system. All these tasks need to be fulfilled at extremely little supply power so that the system can work with a small harvester or sensor. High integration of these functions in the dc-to-dc converter can help to reduce the power needed for such tasks.
The system in Figure 1 shows a typical energy harvesting system for a wireless environmental sensor. These sensors are typically used to sense temperature, humidity, or different gases such as CO2. There are many other applications for energy harvesting. Industrial applications can be found in security and surveillance in wireless occupancy sensors or in industrial monitoring such as asset tracking and machine monitoring.
Energy harvesting is also used in consumer electronics such as in portable and in wearable devices. In home healthcare applications, wireless patient monitoring has a need to run without, or extend, battery life.
Today energy harvesting is a very popular topic. Many engineers must evaluate whether or not an energy harvesting solution can replace or complement an existing power solution. The reason why such systems are so popular today is that we are finally reaching a point of equilibrium, where power being harvested from relatively low cost and small size harvesters is enough to power very low energy consumption microcontrollers and RF circuitry. Advances have been made with both electricity generation and in energy consumption in the last few years, so that today many applications that were unrealistic five to 10 years ago are now possible and economically feasible.

Different Sources of Energy
There are different sources of energy and the most common ones are photovoltaic (PV), thermoelectric (TEG), electromagnetic, piezoelectric, and RF. Photovoltaic and thermoelectric harvesters generate dc voltages, while electromagnetic, piezoelectric, and RF harvesters generate changing or ac voltages. This makes the requirement for a power conversion technology slightly different.
Figure 2 shows different harvesting types and the amount of energy that can roughly be generated with a harvester size of 10 square centimeters. It shows energy generation on the left side and energy consumption for different tasks on the right side. Notice that the power scale in the center is logarithmic. This graph is very important to get a realistic idea of the feasibility of an idea. Often times, designers put work and effort into evaluating an energy harvesting solution only to find out that the harvested energy is not enough to power a given system.

The Importance of the DC-to-DC Converter Unit
Power conversion and management is generally the core of modern energy harvesting systems. While some applications do not use sophisticated power devices, many do. Examples of systems without intelligent power management are a stack of daisy-chained solar cells generating a relatively high dc voltage to either directly power a system or with a simple linear regulator in between. Such systems usually do not have the optimum energy efficiency or do not have a supply voltage that is well regulated. While some loads might work with a widely varying supply voltage, others will not. Future, more advanced systems are more likely to require some form of voltage converter and management block.

Figure 3 shows the block diagram of a modern power management device for energy harvesting applications. It contains start-up circuitry with a charge pump to allow a start-up voltage of 380 mV on the input. Once the system is running, the internal circuitry of the ADP5090 is powered from the output voltage of the ADP5090. This is the node that powers the load of the energy harvesting system. Once this node is above 1.9 V, the input voltage may go down as low as 80 mV while still being able to harvest energy. This is very helpful in systems that spend a lot of time in suboptimal situations. For example, a solar cell powered indoor sensor. In the morning hours and evening hours, there might be very little light on the solar cell, which generates very little electrical power. Using this time to harvest some energy can help the total power budget in a given time period. One other aspect that helps in such situations is the low quiescent current of the ADP5090. While alert, the current consumption is only 260 nA. Figure 4 shows a typical real-world application. This plot shows different places in a residential building and the typical times a sensor with a solar cell spends in darkness. Certainly this is just a typical case. The amount of light a sensor will see depends on the architecture of the house, including the amount of windows, the amount of electric light that is being used, and the exact location of the sensors. Also the time of year and the location of the house will influence such a chart. The point is, in such varying light conditions, the low power consumption of the ADP5090 helps the total power budget immensely, especially in places that spend most of their time in darkness.

The dc-to-dc converter stage in the ADP5090 is quite interesting. It has a regulation loop just like most dc-to-dc converters. However, it does not regulate the output voltage, nor the output current. The regulation loop is primarily set up in a way to regulate the input impedance.
Solar cells have a current and voltage behavior as shown in Figure 5. In an open-loop condition, with no current flow, the provided voltage is at its maximum. Then as current starts to flow, the voltage goes down. At very high currents, the voltage collapses sharply. In the middle of the curve, there is a knee that is the point of peak power. This is the point where the voltage is still relatively high but also where quite a lot of current is drawn. To operate close to the maximum peak power point, we need to track this point. Just setting a fixed current value we draw will not work because the curve of a given solar cell in Figure 5 will shift depending on different light conditions. To track the MPP (maximum peak power point), the ADP5090 stops conducting current on the input, checks the solar cell voltage without it being loaded, and then sets the MPP for the next 16 seconds. After this time period, an open-loop check is performed again. Sixteen seconds turns out to be a good compromise between drifting away from the MPP and interrupting the harvesting action too often.

MPP tracking ensures that the most energy is harvested from a power source, such as a photovoltaic cell or a thermoelectric generator. Still the power management unit has additional tasks. For instance, it needs to control the output voltage in a certain voltage window. The ADP5090 acts like a current source to charge a super cap or a battery. This element is important to decouple energy harvesting with energy consumption. This enables many systems that do not have a constant source of available energy to harvest and perform certain system tasks in set intervals. For example, a sensor in a wireless sensor network that needs to send temperature values every five minutes. If the sensor is powered by a solar cell, it can still operate during dark times due to the intermediate energy storage.
A quite popular architecture today involves attaching energy harvesting to systems that are powered by a primary cell battery. Successful products using a nonrechargeable battery could extend the lifetime of the system by having energy harvesting added. This brings extended operating time without compromising system reliability. For such hybrid systems, the ADP5090 offers the capability to control a primary cell battery. Once there is not enough harvested energy available, the power path from the primary cell battery is routed to power the load directly.

Figure 6 shows a complete energy harvesting power stage with not only the main ADP5090 MPPT energy harvesting IC, but also one second IC, the ADP5310. It is a dc-to-dc converter very efficiently generating two output voltages. The efficiency is close to 90% at 100 µA output current. Additionally, the ADP5310 also has one load switch integrated. This load switch can be used to turn off loads that otherwise would constantly consume power, even when they are not in use.
The ADP5310 step-down converter can accept input voltages all the way up to 15 V. This enables the device to be used directly in ac voltage generators, such as piezoelectric or electromagnetic types. All that is needed is a bridge rectifier and the output voltage can be fed directly into the ADP5310.
Today many power management integrated circuits are available that were specifically designed for use in energy harvesting applications. They enable systems to run with smaller harvesters or make energy harvesting solutions possible that could not have been designed a few years ago. System designers have great ideas that are being implemented right now and which we will be able to see and marvel at in the very near future.