USB Type-C is a relatively new, high power USB peripheral standard used in computer and portable electronic devices. The USB Type-C standard has driven changes in the USB power delivery specification, allowing for increased bus voltages (up to 20 V) and current delivery capability (up to 5 A) from the long-standing 5 V USB standard. Connected USB-C devices can recognize each other and negotiate a bus voltage—from the default 5 V USB output to several higher preset voltage steps—for faster battery charging and higher power delivery where needed, up to 100 W.
The simple, compact buck regulators and linear regulators used in battery chargers that require only USB 5 V at 500 mA to 2 A do not sufficiently cover the full range of Type-C USB power. The increased voltage range, 5 V to 20 V, of Type-C USB power delivery requires more than just step-down voltage conversion from 9 V to 36 V (or 60 V) automotive batteries, or other charging sources. An adjustable buck-boost converter is needed with the ability to both step-up and step-down the input-to-output voltage.
Additionally, for high power automotive USB chargers, a buck-boost converter should support a 10 A or higher peak switch current rating and offer low EMI performance. The ability to set the switching frequency outside the AM radio band and maintain a small solution size are sought-after features. High voltage monolithic converters (with onboard switches) are not capable of sustaining such high peak switch currents without burning up.
The LT8390A is a unique 2 MHz, synchronous 4-switch buck-boost controller. At 2 MHz switching frequency, it can deliver output voltages between 5 V and 15 V (up to 45 W at 3 A) to provide power to a connected USB-C device from a car battery. This high controller switching frequency keeps the solution size small, the bandwidth high, and the EMI outside of the AM radio band. Both spread spectrum frequency modulation and low EMI current-sense architecture help LT8390A applications pass the rigors of the CISPR 25 Class 5 automotive EMI standard.
High Power Density Conversion: Size (and Power), Efficiency, Heat
The design of a voltage regulator system operating in an automotive or portable electronics environment is constrained by the space required for the circuit, as well as the heat it generates during operation. These two factors impose an upper bound of achievable power levels while operating within the given design constraints.
Increasing the switching frequency of a design allows for the use of smaller inductors, which is often the largest footprint component in wide input voltage 4-switch buck-boost voltage regulator designs. The LT8390A’s 2 MHz switching frequency capability enables the use of a much smaller inductor size than a 150 kHz or 400 kHz design. A complete design is shown in Figure 1. Along with a smaller inductor, this solution uses only ceramic output capacitors, eliminating the need for bulky electrolytic capacitors. All the components necessary for this design, including the IC, are contained within a small, 1" square footprint, as shown in Figure 1.

Figure 2 shows a 45 W LT8390A solution using AEC qualified components. This design experiences a maximum temperature increase of 65°C from the ambient temperature, as shown in Figure 3. Even with the small solution size, the LT8390A system boasts a peak efficiency of 94% while delivering a 45 W output, and deviates in efficiency by less than 10% over the input range for each output voltage created, shown in the graphs in Figure 4.



Low EMI for Automotive Applications
The LT8390A has several unique EMI mitigating features that enable high power conversion with low noise performance, which simplifies its implementation in automotive systems. A notable difference between LT8390A and alternative 4-switch controllers is the placement of the inductor current sensing resistor. Most 4-switch buck-boost controllers tend to use a ground-referred current sensing scheme to obtain switch current information, whereas the LT8390A places its current sense resistor in-line with the inductor. By placing the sensing resistor in-line with the inductor, it is effectively removed from both the buck and boost hot loops, shrinking the loops in size and improving the EMI performance.
Along with the architectural advantage of the inductor sensing resistor placement, the LT8390A has built-in spread spectrum frequency modulation to further reduce EMI generated by the controller. Furthermore, the switching edge rate is controlled on both the buck and boost power switches using only a few discrete components to slow the turn-on of the MOSFETs, ensuring the proper balance of high frequency EMI reduction and temperature rise in the power switches. With these EMI-reducing features, the only filtering needed to meet CISPR 25 compliance is taken care of by small ferrite filters on the input and output rather than large ferrite cases and bulky LC filters. The solution shown in Figure 1 was designed using only AEC-Q100 components.
Seamless Output Voltage Transitions
The LT8390A’s output voltage can be adjusted without shutting down the converter by using logic-level signals to drive MOSFETs that adjust the resistor divider off the output to change the set voltage. A USB PD source controller device with GPIO pins can be used in conjunction with the LT8390A system to facilitate the negotiation process between host and USB-connected device and to set the desired bus voltage.
Figure 5 demonstrates how smoothly the output of the LT8390A system transitions from one output voltage to another. When powered from a 12 V input source, each transition to an increased output voltage takes at most 150 µs to settle, as measured from the rising edge of the digital control signal. During these changes in the output voltage, the buck-boost controller goes through mode transitions—between buck, boost, and buck-boost operation—depending on the relation of input to output voltages. These mode transitions are performed in a controlled manner, preventing excessive overshoot or sagging of the output voltage.

Expanding Beyond 45 W
To push the output power level beyond 45 W requires operating at a lower switching frequency to reduce switching losses, which might otherwise thermally stress the MOSFETs at this power level. As an alternative to the LT8390A, the LT8390 operates between 150 kHz and 600 kHz with the same feature set as LT8390A—allowing low EMI, high power buck-boost designs. A 400 kHz LT8390 system, utilizing a larger inductor and output capacitor, easily achieves 100 W of output power from an automotive battery input with acceptable temperature rise. Figure 6 illustrates the power capabilities of the LT8390A and LT8390 product line from various battery-powered inputs.

Conclusion
The new USB standard for voltage regulators powering connected devices permits higher power transfer by increasing the output voltage range and current delivery that regulators can provide. Portable and automotive battery-powered USB-C charger devices require a wide VIN/VOUT buck-boost regulator to deliver a bus voltage above or below the input voltage. The LT8390A provides up to 45 W of output power in a small footprint, made possible by its 2 MHz switching frequency. For power levels exceeding 45 W, the LT8390 can be used with a slightly larger solution size and lower switching frequency.