Linear Multipliers & Dividers
A linear multiplier/divider is a device that produces an output voltage or current that is proportional to the product of two or more independent input voltages or currents. In addition to multiplying
Go to Product Selection Table
Viewing:
Products in Category
AD534S
PRODUCTION
Aerospace Internally Trimmed Precision IC Multiplier
ADL5391
PRODUCTION
DC to 2.0 GHz Multiplier
AD633
PRODUCTION
Low Cost Analog Multiplier
AD835
PRODUCTION
250 MHz, Voltage Output 4-Quadrant Multiplier
AD534
PRODUCTION
Internally Trimmed Precision IC Multiplier
AD834
PRODUCTION
500 MHz Four-Quadrant Multiplier
AD734
PRODUCTION
10 MHz, 4-Quadrant Multiplier/Divider
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}