The rapid rise of AI has ushered in a new era of high-density compute demands, where traditional power architecture simply cannot keep pace. To further support this demand, Analog Devices, Inc. (ADI) announces innovative solutions to support next-generation 800 VDC architectures in data centers. The company’s robust hot swap and first-stage power solutions are designed to enable safe, efficient, and intelligent power distribution—meeting the demands of modern AI factory systems.
Why 800 V Architecture?
Data centers are transitioning from conventional 12V or 48V systems to 800 V architecture for one major reason: efficiency at scale. With the power demands of AI clusters, stepping up the voltage to 800 V allows for higher-density compute clusters with rack power densities of 1 MW or more.
“We are proud to advance technology for 800 V high-voltage data center architectures,” said Todd Sherman, General Manager ADI’s High Voltage & Protection Business. “ADI is a leader in hot swap controllers, which we believe have become essential for protecting these new AI systems.”
ADI's Hot Swap Controllers: Safeguarding High-Power Systems
Hot swap controllers are integrated circuits that protect systems from the dangers of sudden power changes while ensuring the system remains operational. In AI factories, they are essential for managing inrush current and protecting these high-voltage power delivery systems during startup, faults or maintenance.
ADI, with its proven silicon technology and extensive expertise in high-voltage analog design, is a leader that provides critical protection mechanisms.
ADI’s portfolio of 800 V solutions helps to ensure:
- Controlled power-up of AI racks: Preventing current spikes and damage to downstream converters during rack insertion.
- Real-time fault detection: Supporting precise telemetry, system diagnostics and fail-safe operation.
- 99.99% redundancy and resilience: Essential for uptime in AI factories operating 24 hours a day, seven days a week.
800 V in Action
Once the 800 V power is delivered seamlessly into the rack, it must be down converted to intermediate voltages (typically 48V or lower) for localized regulation to processors, GPUs and accelerators.
ADI’s first-stage data center-to-data center conversion solutions are expected to deliver:
- High-efficiency voltage regulation with >98% conversion at high loads
- Digital power control and telemetry interfaces for NVIDIA’s intelligent platform management
- Scalable modules that are designed to support rapidly evolving rack-level architecture and power densities.
The result is a efficient and tightly monitored power path from utility feed to GPU socket, which is critical in data center environments where every watt and millisecond count.
Accelerating the AI Era, Together
AI infrastructure is the integrated hardware and software that accelerates the deployment and efficiency of advanced AI systems, combining optimized computing, networking, power, and cooling with specialized software from cloud to edge. It enables organizations to build secure “AI factories” that turn data into valuable results by managing the entire AI lifecycle—from data ingestion and training to large-scale inference. NVIDIA’s 800 VDC data center power architecture isn’t just about today’s racks—it’s about future-proofing AI infrastructure for AI factories. This shift to high power architectures requires a reimagined approach to power delivery, and ADI is playing a key role in this transformation.
ADI’s solutions, ranging from rack-level hot swap protection to intelligent high-voltage conversion, are helping enable the shift to 800 VDC architecture. These solutions require robustness and efficiency for demanding AI workloads.
As NVIDIA expands its platforms across major cloud providers, ADI is supporting the development of the underlying infrastructure that powers this AI advancement.
Learn more about NVIDIA’s 800 VDC architecture on the NVIDIA Technical Blog
Explore ADI’s hot swap solutions on the ADI website