Modex 2024 Modex 2024
March 11 – 14, 2024
Georgia World Congress Center
Atlanta, GA
Booth #B1429 (B Hall)
Interpret, Connect, Control: Integrated Circuits that Enable OEM Solutions
Visit ADI at booth #B1429 in B hall and explore sensing, motion control, and power solutions that can accelerate time-to-market and deliver best-in-class performance for your robotics, scanning, or point-of-sale applications.
Preview Our Demos
Battery-Powered Technologies for Handheld Devices
Handheld battery-powered systems need accurate state of health and state of charge to maximize how long they can be used during a workers shift and when they are really coming to EOL. With battery counterfeiting on the rise, secure battery authentication is needed more and more to protect the OEM battery makers. Witness how ADI's highest performance secure fuel gauge technology provides the highest performance SOA/SOC together with an integrated security authenticator block to allow battery packs to be fully authenticated using cyber security algorithms.
EV Charging Solutions
Electric vehicle supply equipment on the grid is quickly and continuously expanding but needs to accelerate even more. ADI is making it faster and easier for our customers to build their own charging system utilizing 2 open reference designs: (1) a 22kW AC Wallbox (Level 2) platform with authentication, metrology and charge controller (2) a 3.6kW AC Cordset (Level 1) reference design. The solution allows for bidirectional energy flow across the EV and the grid. It delivers an accurate, secure, and real-time payment processing mechanism together with auditable cloud analytics that can facilitate results like ESG reporting for enterprises and EV fleets .
Logistics Asset Tracking
Real-time asset tracking is a key need to enable end-to-end supply chain tracking, traceability, improve product loss, and enhance inventory restocking. The cost of RFID readers are expensive and the industry needs higher performance RFID readers that can detect RFID tags at a longer range. Learn how ADI's high performance SOC RF transceiver and chip set components enable improved RF performance and system level sensitivity. They increase the useable range of expensive readers meaning fewer readers need to be deployed in the same coverage area.
Modular Mobile Robotics Solutions
Robotics solutions are at the forefront of automation technology, combining cutting-edge semiconductor innovations with advanced sensing, motion control, and machine learning capabilities. These solutions empower industries to create modular mobile robotics systems that are safer, more efficient, and adaptable to a wide range of applications, revolutionizing the way tasks are performed in industrial and commercial settings. ADI solutions enable perception, localization, motion control and battery management.
Warehouse Conveyor and Machine Vision
Conveyor systems today use motor drives that control conveyor speed at constant power and torque regardless of load. Most conveyors operate under light load most of the time burning power unnecessarily. See how ADI Trinamic™ motor drive chips unique functionality monitors the load in real time and modifies the torque applied utilizing the minimum energy needed to drive the conveyor system, thereby saving as much as 30% energy efficiency.
Today in logistics, parcel dimensioning on conveyors is typically done using LIDAR systems which are very costly, large, and power hungry. ADI’s depth sensing technology uses a high-performance depth measurement system with accuracies of 3mm at high frame rates allowing parcel dimensioning at the highest accuracy in the smallest form factor comparing to current systems used today.
Zero Power Robot Positioning
Robots need precision motor control and position feedback to enable the advanced motion control required to operate accurately and efficiently. ADI’s new multiturn technology is a game changer in the industrial rotary and linear position market, eliminating bulky gearing, back up batteries while delivering cost optimized solutions and increasing productivity. ADI Trinamic PanDrive modules provide optimized motion control solutions out of the box offering faster time to market with advanced motion control features.