ATC India 2025 banner
A home hero mobile in
ATC India 2025 ATC India 2025

Join us at ATC India 2025 as we dive into the latest advancements, industry trends and breakthrough solutions that are powering a more intelligent and sustainable future!

Register Now

Asia is a key market for Analog Devices, representing over 40% of the company's total revenue in fiscal year 2024. With a presence spanning over 50 years, ADI has established a strong foothold in these regions. ADI operates a network of facilities to support customer engagement in Asia and has a network of manufacturing sites across these regions, including Chonburi, Thailand, Penang, Malaysia and Cavite, Philippines. To better support customers through cutting-edge technologies and solutions, ADI has 8 design centers across Asia. ADI's strong regional presence is further supported by an extensive network of authorized sales and distribution channels across these regions.

Featured technology

Integrated SoC shrinks the size of the 4-20 mA smart transmitter

The 4-20 mA current loop offers a common technique for transmitting sensor information such as temperature and pressure in industrial process-monitoring applications.

Download Now


High fidelity PCB design for multichannel beamformers

Part 1 discusses designing PCBs with highly accurate 50 Ω trans-mission lines.Part 2 will discuss isolation between transmission lines,how isolation affects beamformer IC performance.

Download Now



How to convert voltages using a high voltage buck controller without a transformer

Switch-mode power supplies without transformers are typically used at lower voltage levels. new devices such as high voltage buck controllers can be used instead.

Download Now


ADI in social media

Analog Devices International, LLC Singapore Branch

Address: Solaris@Kallang 164
164 Kallang Way
#07-09 Singapore 349248
Phone: +65 6427 8430

Analog Devices India Private Limited

Address: Salarpuria Nova
No. 1, Varthur Road
Nagavarpalya, Bengaluru 560093
Email: cic.asia@analog.com

welcome-in-feedback   welcome-in-ezchina-1