LTspice: Models of ISO 7637-2 & ISO 16750-2 Transients

2017-04-05

Introduction

Simulating the ISO 7637-2 and ISO 16750-2 transients early in the design phase of an automotive product can pinpoint issues that would otherwise come to light during electromagnetic compatibility (EMC) testing. If a product fails EMC testing, hardware modifications are required, project schedules suffer, and extra costs result from repeated testing on the new hardware. Spending a few minutes, or hours, simulating the protection circuitry in LTspice helps to avoid expensive hardware respins due to EMC failures.

ISO 7637-2 and ISO 16750-2 are the most common specifications encountered by engineers who design automotive electronics. These two specifications describe potentially destructive transients and the recommended test procedures to ensure that the electronics are suitably protected. More information about these specifications can be found in the following article:

Low Quiescent Current Surge Stopper: Robust Automotive Supply Protection for ISO 7637-2 and ISO 16750-2 Compliance.

In addition to reviewing the above article, it is recommended that anyone dealing with these specifications purchase copies from the International Organization for Standardization (ISO) or American National Standards Institute (ANSI):

ISO 7637-2:2011 Road vehicles — Electrical disturbances from conduction and coupling — Part 2: Electrical transient conduction along supply lines only

ISO 16750-2:2012 Road vehicles — Environmental conditions and testing for electrical and electronic equipment — Part 2: Electrical loads.

For each transient condition in the ISO 16750-2 and ISO 7637-2 specifications, a “Class” of operation is suggested with “Class A” the most stringent requirement and “Class E” the least stringent. The definitions of Class A through Class E are provided in the ISO 16750-1:2006 specification, and they are also included at end of this document for easy reference. Appendix: ISO 16750-1:2006 §6 Functional Status Classification.

Simulating Transients

Simulating the ISO 7637-2 and ISO 16750-2 transients early in the design stage can highlight potential issues before they result in costly failures during ISO 7637-2 and ISO 16750-2 testing. The ISO16750-2 and ISO7637-2 symbols in LTspice simplify this task by providing a nearly complete set of ISO 7637-2 and ISO 16750-2 transients.

When using these symbols in an LTspice schematic, the test condition can be selected by right-clicking on the symbol and then double-clicking on the “SpiceModel” field to open a drop-down menu like the one shown below.

Component Attribute Editor Model Select

Because the requirements are different for devices that operate from 12V supplies and 24V supplies, separate models are provided for each. The models that correspond to 12V supplies have a “_12V” in their name, and those that correspond to 24V supplies have “_24V” in the name. .

Since many automotive manufacturers maintain their own specifications independent from the International Organization for Standardization, these symbols have been created with parameters that allow customization through the “Value” field, as shown below. The parameters for each waveform are described in the sections that follow.

Component Attribute Editor Modify Value

For all of the following conditions, there is a t0 parameter that defines when the condition will be applied. It is not part of the ISO 7637-2 or ISO 16750-2 specifications; it is only used for the LTspice model.

ISO 7637-2:2011 Pulse 1

Pulse 1 describes the negative transient observed by electronics connected in parallel with an inductive load when the connection to the power supply is interrupted.

Parameter

ISO 7637-2: 2011

Nominal 12V

ISO7637-2: Pulse1 12V

(LTspice Default)

ISO 7637-2: 2011

Nominal 24V

ISO7637-2: Pulse1 24V

(LTspice Default)

Ua (V) 13.5±0.5 13.5 27±0.5 27
Us (V) –75 to –150 –150 –300 to –600 –600
Ri (Ω) 10 10 50 50
td (s) 2m 2m 1m 1m
tr (s) 0.5u to 1u 1u 1.5u to 3u 3u
t1 (s) >0.5 0.5 >0.5 0.5
t2 (s) 200m 200m 200m 200m
t3 (s) <100u 50u <100u 50u
t0 (s) 1m 1m
ISO 7637-2 Pulse 1

Requirement: Pulse 1 must be repeated a minimum of 500 times. Class A through Class E operation is negotiated between the vehicle manufacturer and the equipment supplier. Since the power is effectively removed during the test, it is usually defined as Class A if the equipment returns to normal operation without user intervention after power is reapplied.

ISO 7637-2 Pulse 1 Example Circuit

ISO 7637-2:2011 Pulse 2a

Pulse 2a describes the positive voltage spike that may occur when current is interrupted to a circuit in parallel with the electronics being tested. If current is built up in the wiring harness, when a device suddenly stops sinking current, the energy stored in the wiring harness inductance may cause a voltage spike. The energy of this positive spike is limited by the series resistance.

Parameter

ISO 7637-2: 2011

Nominal 12V

ISO7637-2: Pulse2a 12V

(LTspice Default)

ISO 7637-2: 2011

Nominal 24V

ISO7637-2: Pulse2a 24V

(LTspice Default)

Ua (V) 13.5±0.5 13.5 27±0.5 27
Us (V) +37 to +112 112 +37 to +112 112
Ri (Ω) 2 2 2 2
td (s) 0.05m 0.05m 0.05m 0.05m
tr (s) 0.5u to 1u 1u 0.5u to 1u 1u
t1 (s) 0.2 to 5 0.2 0.2 to 5 0.2
t0 (s) 1m 1m
ISO 7637-2 Pulse 2a

Requirement: Pulse 2a must be repeated a minimum of 500 times. Class A through Class E operation is negotiated between the vehicle manufacturer and the equipment supplier, typically Class A.

ISO 7637-2: Pulse 2a Example Circuit

ISO 7637-2:2011 Pulse 2b

Pulse 2b defines a situation that occurs when the ignition is switched off and DC motors act as generators. For example, if the heater is running when the driver turns off the car, for a short time the blower motor can supply DC power to the system while it spins down.

Parameter

ISO 7637-2: 2011

Nominal 12V

ISO7637-2: Pulse2b 12V

(LTspice Default)

ISO 7637-2: 2011

Nominal 24V

ISO7637-2: Pulse2b 24V

(LTspice Default)

Ua (V) 13.5±0.5 13.5 27±0.5 27
Us (V) 10 10 20 20
Ri (Ω) 0 to 0.05 0.05 0 to 0.05 0.05
td (s) 0.2 to 2 0.2 0.2 to 2 0.2
t12 (s) 1m±0.5m 1m 1m±0.5m 1m
tr (s) 1m±0.5m 1m 1m±0.5m 1m
t6 (s) 1m±0.5m 1m 1m±0.5m 1m
trep (s) 0.5 to 5 5 0.5 to 5 5
ton (s) 1 1
t0 (s) 1m 1m
ISO 7637-2 Pulse 2b

Requirement: Pulse 2b must be repeated a minimum of 10 times. Class A through Class E operation is negotiated between the vehicle manufacturer and the equipment supplier. Since the power is effectively removed during the test, it is usually defined as Class A if the equipment returns to normal operation without user intervention after power is reapplied.

ISO 7637-2: Pulse 2b Example Circuit

ISO 7637-2:2011 Pulse 3a

Pulse 3a defines the negative spikes that may occur as a result of switching processes including arcing across switches and relays. For this specification, the energy is limited by a 50Ω series resistance.

Parameter

ISO 7637-2: 2011

Nominal 12V

ISO7637-2: Pulse3a 12V

(LTspice Default)

ISO 7637-2: 2011

Nominal 24V

ISO7637-2: Pulse3a 24V

(LTspice Default)

Ua (V) 13.5±0.5 13.5 27±0.5 27
Us (V) –150 to –300 –300 –112 to –220 –220
Ri (Ω) 50 50 50 50
td (s) 150n±45n 150n 150n±45n 150n
tr (s) 5n±1.5n 5n 5n±1.5n 5n
t1 (s) 100u 100u 100u 100u
t4 (s) 10m 10m 10m 10m
t5 (s) 90m 90m 90m 90m
t0 (s) 1m 1m
ISO 7637-2 Pulse 3a

Requirement: Pulse 3a should be applied repetitively for one hour. Class A through Class E operation is negotiated between the vehicle manufacturer and the equipment supplier, typically Class A.

ISO 7637-2:Pulse 3a Example Circuit

ISO 7637-2:2011 Pulse 3b

Pulse 3b defines the positive spikes that may occur as a result of switching processes including arcing across switches and relays. For this specification, the energy is limited by a 50Ω series resistance.

Parameter

ISO 7637-2: 2011

Nominal 12V

ISO7637-2: Pulse3b 12V

(LTspice Default)

ISO 7637-2: 2011

Nominal 24V

ISO7637-2: Pulse3b 24V

(LTspice Default)

Ua (V) 13.5±0.5 13.5 27±0.5 27
Us (V) +75 to +150 150 +150 to +300 300
Ri (Ω) 50 50 50 50
td (s) 150n±45n 150n 150n±45n 150n
tr (s) 5n±1.5n 5n 5n±1.5n 5n
t1 (s) 100u 100u 100u 100u
t4 (s) 10m 10m 10m 10m
t5 (s) 90m 90m 90m 90m
t0 (s) 1m 1m
ISO 7637-2 Pulse 3b

Requirement: Pulse 3b should be applied repetitively for one hour. Class A through Class E operation is negotiated between the vehicle manufacturer and the equipment supplier, typically Class A.

ISO 7637-2: Pulse 3b Example Circuit

ISO 16750-2:2012 §4.2 Direct Current Supply Voltage

Section 4.2 of ISO 16750-2 defines the minimum and maximum supply voltages. The specification defines multiple “codes” for the minimum supply voltage, and the appropriate code for the supply voltage is negotiated between the vehicle manufacturer and equipment supplier. No LTspice model is provided for this model because it is simply a constant voltage, but the conditions are listed below for easy reference.

Bandwidth

ISO 16750-2: 2012

Nominal 12V

ISO 16750-2: 2012

Nominal 24V

Usmax(V)

Code A: 6V

Code B: 8V

Code C: 9V

Code D: 10.5V

Code E: 10V

Code F: 16V

Code G: 22V

Code H: 18V

Usmax (V) 16 32

Requirement: Class A (continuous operation).

ISO 16750-2:2012 §4.3 Overvoltage

Section 4.3 of ISO 16750-2 describes “Overvoltage” requirements. The first requirement lasts for 60 minutes and simulates the condition where the voltage regulator has failed. For 12V systems, 18V is applied; for 24V systems, 36V is applied. Depending on the application, it might not be necessary for the equipment to operate normally while the test is performed, but it must return to normal operation after the test condition is removed. The second test condition only applies to 12V systems and simulates a jump-start with 24V applied for 60 seconds. Once again, it may not be necessary for the equipment to operate normally during the test.

No LTspice model is provided for this condition since it is simply a voltage source.

Requirement: See ISO 16750-2:2012 specification.

ISO 16750-2:2012 §4.4 Superimposed Alternating Voltage

Section 4.4 provides test conditions to “simulate a residual alternating current on the direct current supply.” During this test, an AC voltage with series impedance between 50mΩ and 100mΩ is swept from 50Hz to 25kHz multiple times. The upper peaks of the voltage are 16V for a 12V system and 32V for a 24V system. The peak to peak voltage is defined by the “severity level” as listed below, and the frequency is swept five times logarithmically, triangular, over 10 minutes.

Parameter

ISO 16750-2: 2012

Nominal 12V

ISO16750-2: 4-4 12V
Superimposed
Alternating Voltage

(LTspice Default)

ISO 16750-2: 2012

Nominal 24V

ISO16750-2: 4-4 24V
Superimposed
Alternating Voltage

(LTspice Default)

Umax (V) 16 16 32 32
Upp (V)

Severity 1: 1V

Severity 2: 4V

Severity 3: N/A

Severity 4: 2V

4

Severity 1: 1V

Severity 2: 4V

Severity 3: 10V

Severity 4: N/A

10
Ri (Ω) 50m to 100m 50m 50m to 100m 50m

Requirement: Class A

ISO16750-2: 4-4 Superimposed Alternating Voltage Example Circuit

ISO 16750-2:2012 §4.5 Slow Decrease and Increase of Supply Voltage

Section 4.5 “Slow decrease and increase of supply voltage” simulates a battery being slowly discharged and then recharged. The test begins with the supply voltage at Usmin, the minimum supply voltage, before it is discharged to 0V at a rate of 0.5V/minute. After reaching 0V, the supply is brought back up to Usmin at the same rate.

In ISO 16750-2, Usmin, the minimum supply voltage, is identified by Code A through Code E in Section 4.2 of the specification. These codes are reproduced below for easy reference.

Obviously, it is not necessary to operate continuously, but this test verifies that the hardware does not fail.

Parameter

ISO 16750-2:2012

Nominal 12V

ISO16750-2: 4-5 12V
Slow Decrease
and Increase of
Supply Voltage

(LTspice Default)

ISO 16750-2:2012

Nominal 24V

ISO16750-2: 4-5 24V
Slow Decrease
and Increase of
Supply Voltage

(LTspice Default)

Usmin (V)

Code A: 6V

Code B: 8V

Code C: 9V

Code D: 10.5V

6

Code E: 10V

Code F: 16V

Code G: 22V

Code H: 18V

10
t0 (s) 1m 1m

Requirement: See ISO 16750-2:2012 specification.

ISO16750-2: 4-5 Slow Decrease and Increase of Supply Voltage Example Circuit

ISO 16750-2:2012 §4.6.1 Discontinuities in Supply Voltage

Section 4.6.1 “Discontinuities in supply voltage” attempts to simulate a failure in another circuit that causes the supply to dip until the other circuit’s fuse blows open. In this test, the supply starts at Usmin, the minimum supply voltage, then dips for 100ms, and finally recovers to Usmin. The rise time and fall time of the dip and recovery are faster than 10ms. For 12V systems, the supply dips to 4.5V, and for 24V systems it dips to 9V.

In ISO 16750-2, Usmin, the minimum supply voltage, is identified by Code A through Code E in Section 4.2 of the specification. These codes are reproduced below for easy reference.

In the simulation, the supply dips at the 10 second timepoint of the simulation.

Parameter

ISO 16750-2:2012

Nominal 12V

ISO16750-2: 4-6-1 12V
Momentary Drop In
Supply Voltage

(LTspice Default)

ISO 16750-2:2012

Nominal 24V

ISO16750-2: 4-6-1 24V
Momentary Drop In
Supply Voltage

(LTspice Default)

Usmin (V)

Code A: 6V

Code B: 8V

Code C: 9V

Code D: 10.5V

6

Code E: 10V

Code F: 16V

Code G: 22V

Code H: 18V

10

Requirement: Class B. The vehicle manufacturer and the equipment supplier may agree that a reset is allowed.

ISO16750-2: 4-6-1 12V Momentary Drop In Supply Voltage Example Circuit

ISO 16750-2:2012 §4.6.2 Reset Behavior at Voltage Drop

Section 4.6.2 “Reset behavior at voltage drop” specifies a series of 5-second supply dips, with each pulse at a lower voltage than the previous one. The purpose is to verify that the device resets properly following a supply dip. During the test, each 5-second dip is 5% lower than the previous one, and it recovers to Usmin for at least 10 seconds between each dip.

In ISO 16750-2, Usmin, the minimum supply voltage, is identified by Code A through Code E in Section 4.2 of the specification. These codes are reproduced below for easy reference.

Parameter

ISO 16750-2:2012

Nominal 12V

ISO16750-2: 4-6-2 12V
Reset Behaviour At
Voltage Drop

(LTspice Default)

ISO 16750-2:2012

Nominal 24V

ISO16750-2: 4-6-2 24V
Reset Behaviour At
Voltage Drop

(LTspice Default)

Usmin (V)

Code A: 6V

Code B: 8V

Code C: 9V

Code D: 10.5V

6

Code E: 10V

Code F: 16V

Code G: 22V

Code H: 18V

10

Requirement: Class C.

ISO 16750-2:2012 §4.6.3 Starting Profile

Section 4.6.3 specifies a waveform representative of a vehicle’s starting profile. It is applied to the device being tested 10 times. The exact voltages and durations required depend on the desired Level I, II, III or IV, which is determined by the application.

Parameter

ISO 16750-2:2012

Nominal 12V

ISO16750-2: 4-6-3 12V
Starting Profile

(LTspice Default)

ISO 16750-2:2012

Nominal 24V

ISO16750-2: 4-6-3 24V
tarting Profile

(LTspice Default)

Ub (V)

12±0.2

12

24±0.2

24
Us6 (V)

Level I: 8V

Level II: 4.5V

Level III: 3V

Level IV: 6V

6

Level I: 10V

Level II: 8V

Level III: 6V

6
Us (V)

Level I: 9.5V

Level II: 6.5V

Level III: 5V

Level IV: 6.5V

6.5

Level I: 20V

Level II: 15V

Level III: 10V

10
tf (s) 5m±0.5m 5m 10m±1m 10m
t6 (s) 15m±1.5m 15m 50m±5m 50m
t7 (s) 50m±5m 50m 50m±5m 50m
t8 (s)

Level I: 1000m±100m

Level II: 10000m±1000m

Level III: 1000m±100m

Level IV: 10000m±1000m

10000m

Level I: 1000m±100m

Level II: 10000m±1000m

Level III: 1000m±100m

1000m
tr (s)

Level I: 40m±4m

Level II: 100m±10m

Level III: 100m±10m

Level IV: 100m±10m

100m

Level I: 40m±4m

Level II: 100m±10m

Level III: 40m±10m

40m
Ri (Ω) 10m 10m
t0 (s) 1 1m
ISO 16750-2 4-6-3 Startup Profile

Requirement: See ISO 16750-2:2012 specification.

ISO 16750-2:2012 §4.6.4 Load Dump Without Centralized Load Dump Suppression – Test A

Section 4.6.4.2.2 “Test A – without centralized load dump suppression” specifies a transient that occurs when the alternator is charging a battery, and the battery connection is lost. “Without centralized load dump suppression” signifies that the alternator does not contain clamp diodes. For an alternator with clamp diodes, use Test B instead. If you are unfamiliar with this distinction, see a more detailed description in the article:

Low Quiescent Current Surge Stopper: Robust Automotive Supply Protection for ISO 7637-2 and ISO 16750-2 Compliance

Parameter

ISO 16750-2:2012

Nominal 12V

ISO16750-2: 4-6-4 12V
Load Dump Without
Suppression

TestA (LTspice Default)

ISO 16750-2:2012

Nominal 24V

ISO16750-2: 4-6-4 24V
Load Dump Without
Suppression

TestA (LTspice Default)

Ua (V) 14±0.2 14 28±0.2 28
Us (V) 79 to 101 101 151 to 202 202
Ri (Ω) 0.5 to 4 0.5 1 to 8 1
td (s) 40m to 400m 100m to 350m
tr (s) 5m to 10m 5m to 10m
t0 (s)
1
1
ISO 16750-2 4-6-4 Test A

Requirement: Ten pulses at 1 minute intervals. Class C.

16750-2:2012 §4.6.4 Load Dump With Centralized Load Dump Suppression – Test B

Section 4.6.4.2.2 “Test B – with centralized load dump suppression” specifies a transient that occurs when the alternator is charging a battery, and the battery connection is lost. “With centralized load dump suppression” signifies that the alternator contains clamp diodes. For an alternator without clamp diodes, use Test A instead. If you are unfamiliar with this distinction, see a more detailed description in the article:

Low Quiescent Current Surge Stopper: Robust Automotive Supply Protection for ISO 7637-2 and ISO 16750-2 Compliance

Parameter

ISO 16750-2:2012

Nominal 12V

ISO16750-2: 4-6-4 12V
Load Dump With Suppression

Test B (LTspice Default)

ISO 16750-2:2012

Nominal 24V

ISO16750-2: 4-6-4 24V
Load Dump With Suppression

Test B (LTspice Default)

Ua (V) 14±0.2 14 28±0.2 28
Us (V) 79 to 101 101 151 to 202 202
UsClamp (V) 35 35 (58 typical) 58
Ri (Ω) 0.5 to 4 0.5 1 to 8 1
td (s) 40m to 400m 100m to 350m
tr (s) 5m to 10m 5m to 10m
t0 (s) 1 1
ISO16750-2 4-6-4 Test B

Requirement: Five pulses at 1 minute intervals. Class C.

ISO 16750-2:2012 §4.7 Reversed Voltage

Section 4.7 of ISO 16750-2 describes “Reversed voltage” or what most automotive engineers simply refer to as “Reverse Battery.” As you would expect, this covers the human error scenario where someone connects a battery with the polarity reversed. “Case 2” is simulated here, which requires that a reverse test voltage be applied at all inputs for 60 seconds to ensure that the system survives without damage.

An alternative test condition, “Case 1”, is also allowed by ISO 16750-2 for 12V systems if no fuse is present in series with the alternator and the alternator’s rectifier diodes limit the voltage by conducting the substantial current delivered by the reverse connected battery. When Case 1 is used, a 4V reverse voltage is applied for 60 seconds.

Parameter

ISO 16750-2:2012

Nominal 12V

ISO16750-2: 4-7 12V
Reversed Voltage Case2

(LTspice Default)

ISO 16750-2:2012

Nominal 24V

ISO16750-2: 4-7 24V
Reversed Voltage Case2

(LTspice Default)

Ua (V) 14 14 28 28

Requirement: Class A after replacing blown fuse-links.

ISO 16750-2:2012 §4.9 Open Circuit Tests

Section 4.9 covers “line interruption” tests and describes procedures to ensure that a device resumes normal operation after a connection is removed and then restored. During this test, the circuit is opened for 10 seconds and then restored. Section 4.9 also includes “multiple line interruption” requirements which is not covered here.

Parameter

ISO 16750-2:2012

Nominal 12V

ISO16750-2: 4-9-1 12V
Single Line Interruption

(LTspice Default)

ISO 16750-2:2012

Nominal 24V

ISO16750-2: 4-9-1 24V
Single Line Interruption

(LTspice Default)

Ua (V) 14 14 28 28
t0 (s) 1 1

Requirement: Class C.

ISO 16750-2:2012 §4.8, §4.10, §4.11, §4.12, and §4.13 Tests

These sections are not incorporated into the LTspice simulation models since the nature of the tests is beyond the scope of a single predefined model. Of special note is §4.10 Short-Circuit Protection tests, which require connecting each input and output to the maximum supply voltage and ground for 60 seconds. These can be especially challenging, and it is suggested to simulate and test the conditions extensively.

  • ISO 16750-2:2012 §4.8 Ground Reference and Supply Offset
  • ISO 16750-2:2012 §4.10 Short Circuit Protection
  • ISO 16750-2:2012 §4.11 Withstand Voltage
  • ISO 16750-2:2012 §4.12 Insulation Resistance
  • ISO 16750-2:2012 §4.13 Electromagnetic Compatibility

Conclusion

The ISO16750-2 and ISO7637-2 symbols in LTspice provide simulation models of the transients described by the ISO 7637-2 and ISO 16750-2 specifications. Simulating protection circuitry during the design phase of product development helps to avoid failures that would otherwise occur during the EMC testing of hardware. Clearly, the effort spent in simulation upfront is worthwhile when one considers the costs incurred by eventual EMC test failures.

Appendix: ISO 16750-1:2006 §6 Functional Status Classification

Class A through Class E operation is defined in ISO 16750-1:2006 as follows:

Class A All functions of the device/system perform as designed during and after the test.
Class B All functions of the device/system perform as designed during the test. However, one or more may go beyond the specified tolerance. All functions return automatically to within normal limits after the test. Memory functions shall remain Class A.
Class C One or more functions of a device/system do not perform as designed during the test but return automatically to normal operation after the test.
Class D One or more functions of a device/system do not perform as designed during the test and do not return to normal operation after the test until the device/system is reset by simple “operator/use” action.
Class E One or more functions of a device/system do not perform as designed during and after the test and cannot be returned to proper operation without repairing or replacing the device/system

关于作者

Dan Eddleman
Dan Eddleman是一名模拟工程师,在凌力尔特工作超过15年,曾担任过IC设计人员、新加坡IC设计中心经理和应用工程师。

他的职业生涯始于凌力尔特,设计了LTC2923和LTC2925电源跟踪控制器、LTC4355高压双通道理想二极管OR和LTC1546多协议收发器。他还是世界首款以太网供电控制器LTC4255的设计团队成员。他拥有两项与这些产品相关的专利。

随后,他搬到新加坡管理凌...

最新视频 21

Subtitle
了解更多