High Efficiency Synchronous Boost Converter Provides Output Load Disconnect and Soft-Start in ThinSOT Package

2004-02-01

Introduction

In a typical boost converter architecture, the inductor and the Schottky diode or the body-diode of the PMOS rectifier constitute a forward conduction path from input to output whenever the output is lower than the input (e.g., during start-up and shutdown). As a result, the output capacitor usually draws a heavy inrush of current from the input supply during start-up. Likewise, in shutdown, the output capacitor holds the output at a potential equal to the input supply voltage minus a forward diode drop.

Linear Technology’s new LTC3429 solves both of these problems by eliminating any forward conduction through the body diode of the synchronous PMOS switch. This enables the part to achieve output load disconnect by allowing the output voltage to go to zero during shutdown, drawing no current from the input source. It also allows for inrush current limiting at start-up, minimizing surge currents seen by the input supply.

Figure 1. Switch configurations for the LTC3429.

Features

The LTC3429 is a high efficiency (up to 96%), fixed frequency, synchronous step-up DC/DC converter with true output load disconnect, soft-start, and automatic Burst Mode® operation in a low profile 6-lead SOT-23 package. The device has a wide input voltage range, from 0.9V to 4.4V, and the output voltage range is from 2.5V to 5V, making it suitable for applications which require 3.3V or 5V output from a single or dual AA cell or a Li-Ion battery.

Figure 2. 2-cell to 3.3V synchronous boost converter.

Figure 3. Efficiency of the circuit in Figure 2.

At 3.3V output, it is capable of supplying 100mA from a single AA cell or 250mA from a 2-cell AA battery making it ideal for portable electronics. At light load, the LTC3429 automatically switches to Burst Mode operation, which draws only 20μA of quiescent current. In shutdown, the part draws less than 1μA of quiescent current and disconnects the output from the supply. A switching frequency of 500kHz minimizes overall solution footprint by allowing the use of tiny, low profile inductors and ceramic capacitors. Also the internal compensation of the current mode PWM control loop reduces the number of external parts required, thereby saving critical board real estate.

Low Voltage Start-Up and Soft-Start

The LTC3429 includes an independent start-up oscillator designed to start up at input voltages as low as 0.9V. This feature makes it suitable for applications using a single-cell battery. The frequency and duty cycle are internally set to 150kHz and 67%, respectively. Soft-start and inrush current limiting are provided during start-up as well as normal mode operation. An internal soft-start capacitor slowly ramps the peak inductor current from zero to a maximum value of 850mA over a period of 1.5ms. Once the output voltage exceeds 2.3V, the start-up circuitry is disabled and normal fixed-frequency PWM operation is initiated. In this mode, the LTC3429 operates independent of the input, allowing extended operating time as the battery can droop to about half a volt without affecting the output voltage regulation. The only limiting factor in the application is the ability of the battery to supply sufficient energy to the output.

Output Load Disconnect and Inrush Current Limiting

The LTC3429 includes circuitry that switches the n-well body of the internal PMOS rectifier to either the input supply or to the output depending on whichever is higher (see Figure 1). Thus, during start-up and shutdown, when the output voltage is less than the input supply, the n-well is switched to the input making the body diode reverse-biased. As a result, in shutdown, no current can flow to the output, and the output capacitor can be completely discharged to zero. Likewise, during start-up, the reverse-biased body diode prevents the inrush of current typically seen by the input supply.

Burst Mode Operation

Portable devices frequently spend extended time in low power or standby mode, only switching to high power consumption when specific functions are enabled. To improve battery life in these types of products, it is important to maintain a high efficiency over a wide output power range. The LTC3429 provides automatic Burst Mode operation to increase efficiency of the power converter at light loads. Burst Mode operation is initiated if the output load current falls below an internally programmed threshold. In this mode, most of the device is turned off, reducing the quiescent current to only 20μA. When the output voltage droops by about 1% from its nominal value, the part wakes up and commences normal PWM operation. The output capacitor recharges and causes the part to re-enter the idle mode if the output load remains less than the Burst Mode threshold. The frequency of this intermittent PWM or burst operation is proportional to load current; that is, as the load current drops further below the burst threshold, the LTC3429 turns on less frequently. When the load current increases above the burst threshold, the LTC3429 seamlessly resumes continuous PWM operation.

关于作者

Ashish Kirtania
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目

关联至此文章

产品

产品分类

最新视频 21

Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目