搜索 筛查 筛查 产品分类 更多 资源 更多 行业解决方案 更多 工具和模型 技术解决方案 更多 网站部分 结果类型 Blog2Blog Post216Comment342Docs & FAQs3,228Forum Reply46,459Forum Thread17,827Gallery10Groups, Forums & Libraries43更多 群组、论坛和库 ADE电能计量专区1,413ADUC Cortex M3系列162ADUC7xxx系列162ADUC微处理器专区1,472GMSL414MEMS专区3,276Other Products (CN)1,724Power 中文专区4,491更多 ADIApproved5,325ADIForum1,095ADI_Amy562ADI_Eva344ALee687779Admin_ADI1,259Amenda-NanYa289EZAdministrator1,173更多 Precision A/D Converters1,359amplifiers1,109hardware881Integrated/Special Purpose A/D Converters747clock and timing747RF Integrated Transceivers726Sensors and MEMS684Wideband Transceiver IC663更多 Analog.com 0 EngineerZone中文技术论坛 68,153 Analog.com上的搜索结果 0 相关性 相关性 最旧 最新 排序 Technology_solutions.lvl0:Precision Technology Solutions > Isolated Gate Driver Solutions✕ 清除选择 很抱歉,我们没有找到符合搜索条件的结果。请使用其他搜索关键词和/或更改筛选条件后重试。 <<<1>>> EngineerZone中文技术论坛上的搜索结果 68,153 EVAL-ADA4254 power supplyForum ThreadAnswered 放大器专区01 April, 2025I read in the EVAL-ADA4254 data sheet that VDDH and VSSH require a ±28V power supply. However, I currently do not have a ±28V power supply. I only have access to the NI ELVIS II+ experimental platform, which can provide a ±15V power supply. I saw that the ADA4254 … amplifiersADA4254hardwareInstrumentation AmplifiersEVAL-ADA4254AD5940_Ramp休眠唤醒问题Forum ThreadAnswered MEMS专区28 March, 2025使用AD5940_Ramp例程,完成一次检测后,过一会AD5940进入休眠,使用 AD5940_SEQCtrlS(bTRUE); /* Enable sequencer, and wait for trigger */ AppRAMPCtrl(APPCTRL_START, 0); 程序去启动AD5940扫描,AD5940不运行。 需要 … Sensors and MEMSad5940Electrochemical SensorsLVDS隔离电路ADN4650输出异常Forum ThreadAnswered 接口和隔离专区26 March, 2025将一个20ns窄脉冲输入到比较器AD8465的正端,负端为固定电平,将AD8465输出送入LVDS隔离电路ADN4650的输入;当AD8465输入正负端幅度相等 … About IBIAS of LTC6811-1Forum ThreadAnswered 能源存储系统(ESS)和电池管理系统(BMS)23 March, 2025LTC6811的IBIAS接口在isoSPI电路唤醒之后,根据规格书所述,IBIAS引脚电平应当在2V(误差在0.1V内)左右。且关于该引脚电路,数据手册上 … hardwarebattery managementltc6811-1Multicell Battery Stack Monitor96724/96712 同步聚合pipe限制问题Forum ThreadAnswered GMSL18 March, 2025使用96724/96712 做同步聚合Concatenation,发现一个pipe只能在一个aggregator做聚合,否则该pipe会报 overflow。这方面synchronous aggregation是否有什么限制? 请问如下使用三 … MAX96724interface and isolationsynchronous aggregationGSMLSerializer/Deserializer (SerDes) and Selector MuxesGigabit Multimedia Serial Link™ (GMSL)LT3952A芯片测试Forum ThreadAnswered Power 中文专区17 March, 2025原理图如下,选择36V升压至43V,最大电流为3A,电感选择3.3uH和4.7uHBOOST不能升压,ctrl引脚为200mv时电流不能调节,固定只有1A附近 … hardwareLT3952AMultitopology LED DriverLED Driver IC关于ADXRS620三轴陀螺仪的振动信号测量Forum ThreadAnswered MEMS专区06 March, 2025有人使用过仙ADXRS620三轴陀螺仪吗?我想用它来测试振动信号读取数据,想知道配套设备都用了哪些? AD4696驱动问题Forum ThreadAnswered 精密转换器专区05 March, 2025我们使用的stm32来驱动AD4696,在adi官网上有个demo,里面有个ad469x的驱动,我根据驱动里面的一个basic_example.c修改的代码修改的,现在第 … softwareMultiplexed A/D Convertersad4696驱动不正常Precision A/D Convertersad4696AD736 SPICE模型存在问题Forum ThreadAnswered 基准电压源专区05 March, 2025我按照数据手册搭建的外围电路,±5V供电,输入信号为200mV的正弦量,然而运行起来速度极慢,且vout引脚自激振荡,改变输入信 … softwarespiceAnalog Functions芯片ad736RMS to DC Convertersaducm355官方历程 M355_ECSns_EIS 历程。void AD5940ImpedanceStructInit(void)函数,我修改电压出现问题Forum ThreadAnswered 生物/电化学/磁场/温度传感器专区05 March, 2025这个代码里的 pImpedanceCfg->SensorCh0.Vzero = 1100; /* Set Vzero = 1100mV. Voltage on SE0 pin*/我修改为500mv 用示波器测得的电压呈现,下面这种类似于方波的型状,是为何? 用默 … softwareSensors and MEMSaducm355Electrochemical Sensors <<<1234567>>>