搜索 筛查 筛查 产品分类 更多 资源 更多 行业解决方案 更多 工具和模型 技术解决方案 更多 网站部分 结果类型 Blog2Blog Post216Comment342Docs & FAQs3,228Forum Reply46,520Forum Thread17,851Gallery10Groups, Forums & Libraries43更多 群组、论坛和库 ADE电能计量专区1,415ADUC Cortex M3系列162ADUC7xxx系列162ADUC微处理器专区1,472GMSL417MEMS专区3,267Other Products (CN)1,732Power 中文专区4,507更多 ADIApproved5,329ADIForum1,095ADI_Amy562ADI_Eva344ALee687779Admin_ADI1,259Amenda-NanYa289EZAdministrator1,173更多 Precision A/D Converters1,361amplifiers1,109hardware891Integrated/Special Purpose A/D Converters747clock and timing747RF Integrated Transceivers726Sensors and MEMS685Wideband Transceiver IC663更多 Analog.com 0 EngineerZone中文技术论坛 68,238 Analog.com上的搜索结果 0 相关性 相关性 最旧 最新 排序 Product_categories.lvl0:iButton和存储器✕Resource_types.lvl0:Case Study✕ 清除选择 很抱歉,我们没有找到符合搜索条件的结果。请使用其他搜索关键词和/或更改筛选条件后重试。 <<<1>>> EngineerZone中文技术论坛上的搜索结果 68,238 软件Forum ThreadAnswered 嵌入式安全与1-Wire08 April, 2025ibutton数据无法全部读取,这东西不是显示最高能存几万个数据吗,我用它记录了4000多个数据,但读取时只能读取出2048个数据 … softwareibutton数据无法全部读取iButtonAD5940_Ramp休眠唤醒问题Forum ThreadAnswered 生物/电化学/磁场/温度传感器专区07 April, 2025使用AD5940_Ramp例程,完成一次检测后,过一会AD5940进入休眠,使用 AD5940_SEQCtrlS(bTRUE); /* Enable sequencer, and wait for trigger */ AppRAMPCtrl(APPCTRL_START, 0); 程序去启动AD5940扫描,AD5940不运行。 需要 … Sensors and MEMSad5940Electrochemical Sensorsds2484 读取max1888 程序,怎么不能读取温度和IO口状态Forum ThreadAnswered 嵌入式安全与1-Wire07 April, 2025ds2484 读取max1888 程序,怎么不能读取温度和IO口状态 /* Includes ------------------------------------------------------------------*/ #include "DS2484_MAX31888.h"#include "DS2484_DS18B20.h"void DS2484_MAX31888_delay(uint32_t nCount){ for (; nCount != 0; nCount--);} /////DS2482,复位设备状态机逻辑。终 … ds2484 读取max1888 程序,怎么不能读取温度和IO口状态1-Wire Interface Products1-Wire DevicesEVAL-ADA4254 power supplyForum ThreadAnswered 放大器专区01 April, 2025I read in the EVAL-ADA4254 data sheet that VDDH and VSSH require a ±28V power supply. However, I currently do not have a ±28V power supply. I only have access to the NI ELVIS II+ experimental platform, which can provide a ±15V power supply. I saw that the ADA4254 … amplifiersADA4254hardwareInstrumentation AmplifiersEVAL-ADA4254AD7768驱动SPI读取寄存器问题?Forum ThreadAnswered 精密转换器专区31 March, 2025 寄存器读取出来全部是0E,上图为逻辑分析仪抓取时序。 使用软件模拟SPI的方式 LVDS隔离电路ADN4650输出异常Forum ThreadAnswered 接口和隔离专区26 March, 2025将一个20ns窄脉冲输入到比较器AD8465的正端,负端为固定电平,将AD8465输出送入LVDS隔离电路ADN4650的输入;当AD8465输入正负端幅度相等 … About IBIAS of LTC6811-1Forum ThreadAnswered 能源存储系统(ESS)和电池管理系统(BMS)23 March, 2025LTC6811的IBIAS接口在isoSPI电路唤醒之后,根据规格书所述,IBIAS引脚电平应当在2V(误差在0.1V内)左右。且关于该引脚电路,数据手册上 … hardwarebattery managementltc6811-1Multicell Battery Stack Monitor96724/96712 同步聚合pipe限制问题Forum ThreadAnswered GMSL18 March, 2025使用96724/96712 做同步聚合Concatenation,发现一个pipe只能在一个aggregator做聚合,否则该pipe会报 overflow。这方面synchronous aggregation是否有什么限制? 请问如下使用三 … MAX96724interface and isolationsynchronous aggregationGSMLSerializer/Deserializer (SerDes) and Selector MuxesGigabit Multimedia Serial Link™ (GMSL)LT3952A芯片测试Forum ThreadAnswered Power 中文专区17 March, 2025原理图如下,选择36V升压至43V,最大电流为3A,电感选择3.3uH和4.7uHBOOST不能升压,ctrl引脚为200mv时电流不能调节,固定只有1A附近 … hardwareLT3952AMultitopology LED DriverLED Driver IC关于ADXRS620三轴陀螺仪的振动信号测量Forum ThreadAnswered MEMS专区06 March, 2025有人使用过仙ADXRS620三轴陀螺仪吗?我想用它来测试振动信号读取数据,想知道配套设备都用了哪些? <<<1234567>>>