Search

筛查
筛查
网站部分
- 34
Analog.com上的搜索结果
相关性
排序
- Site_section:媒体中心展会新闻咨询资源库资源库
- Product_categories.lvl0:电源管理 > LED 驱动器 IC
- Analog DialogueThe article describes composite amplifier which is an arrangement of two individual amplifiers configured in such a way as to realize the benefits of each individual amplifier while negating or diminishing the drawbacks of each.
- Technical ArticlesOct 1, 2016This article presents a simple way to build and optimize the performance of a low cost in-amp.
- Analog DialogueSeismic geophones are electromechanical conversion devices that convert ground vibration signals into electrical signals. This article describes a very low power data aquisition (DAQ) system.
- Technical ArticlesJan 1, 2016In today’s data acquisition systems (DAQs), performance boundaries are continually being pushed.
- Analog DialogueThe AD4000 ADC family unique combination of high-Z mode, reduced input current and longer acquisition phase enables ease of drive and help designers eliminate dedicated high-speed ADC driver stage, saving PCB area, power and BOM cost and broadens choice of ADC drivers.
- Analog DialogueThis article discusses the common pain-points encountered in designing a precision data acquisition signal chain and how to address them using the next generation of 16-bit/18-bit, 2 MSPS precision SAR ADCs.
- Analog DialogueWhen designing precision signal chains, it can be hard to achieve a clear noise floor without spurs. Spurs can be introduced by components or they can be the result of external interference.This article will introduce approaches for determining the root causes of spur issues in high-resolution, precision ADC applications and present solutions to solve them.
- Technical ArticlesOct 21, 2021This article provides a high level discussion of sensor interfacing data acquisition (DAQ) signal chain design considerations for condition monitoring systems.
- Solutions Bulletin & Brochure
- Analog DialogueThe article described the key problems selecting buffers in sigma delta discrete time converters, and the main benefit of integrating pre-charging amplifiers.