搜索 “tool” 的搜索结果 筛查 筛查 产品分类 更多 资源 更多 行业解决方案 更多 工具和模型 技术解决方案 更多 网站部分 结果类型 Blog Post1Comment2Docs & FAQs28Forum Reply1,750Forum Thread885Webinar1更多 群组、论坛和库 A2B4ADSP-2156x176ADSP-SC59x31ADSP-SC5xx/ADSP-215xx62Audio23Blackfin Processors13CrossCore Embedded Studio and Add-ins124Design Support AD9361/AD9363/AD936410更多 ADIApproved359Adeel15AlClark20Divya.P35EZAdministrator134EZAutoReply93Harshit.Gaharwar69Hfuhrhurr25更多 Audio Signal Processors164SHARC Audio Processors/SoCs161software112Step-Down (Buck) Regulators60ADSP2156x56ADSP-2156x53Internal Power Switch Buck Regulators53sharc50更多 Analog.com 0 EngineerZone中文技术论坛 2,667 Analog.com上的搜索结果 0 相关性 相关性 最旧 最新 排序 Product_categories.lvl0:光通信和光学传感 > 光学传感器✕ 清除选择 很抱歉,我们没有找到符合搜索条件的结果。请使用其他搜索关键词和/或更改筛选条件后重试。 <<<1>>> EngineerZone中文技术论坛上的搜索结果 2,667 ADSP21573Forum ThreadAnswered CrossCore Embedded Studio and Add-ins15 April, 2025I have a 10MB LDR file that needs programming via this command: cldp -proc ADSP-21573 -core 1 -emu 1000 \ -driver "./dev_programmer_Core1.dxe" \ -cmd prog -erase affected -format bin -offset -file ./App_Core2.ldr \ -cmd compare -format bin -offset -file ./App_Core2.ldr The flashing process currently takes … Audio Signal Processorssoftwareadsp-21573How to optimize programming speed for large LDR files using CLDP tool?SHARC Audio Processors/SoCshow can the host MCU get the command response after sending it to ADSP215xx via SPI?Forum ThreadAnswered SigmaStudio for SHARC16 July, 2024We are using CCES and SS4SH to do development based on DemoUC projects. The version of CCES is 2.10.1, the version of SS4SH is v4.7. The target hardware platform is our customized ADSP21565 platform. Now, the DSP can be booted and controlled by MCU via SPI2. And … CCES2.10.1ccessoftwaresigmastudio_for_sharcspisigmaStudio 4.7SigmaStudioForSHARCADSP-2156xA2B TDM8 inputs 8 signals into ADSP21489 and outputs 3 TMD8 signals problemForum ThreadAnswered SigmaStudio for SHARC12 March, 2024 Background of the problem: A2B TDM8 inputs 8 signals into ADSP21489 and outputs 3 TMD8 signals to the power amplifier. ADSP21489 uses the SS4SH framework, version 2.1.0 2.Problem description: Using one TDM8 input and one TDM output, with channels set to 10 in and 10 out … softwareadsp21489Custom Device Programmer for ADSP21363 not allocating AFPBuffer in system heapForum ThreadAnswered CrossCore Embedded Studio and Add-ins06 March, 2024… looking at other posts here, I know that I need to do a custom device programmer and have modified the example device programmer for the ADSP21364 EZ-kit board with m25p20 flash to our needs (ADSP21363 with m25p16 flash). Modifying from ADSP21364 is what we did for our original visual … Audio Signal ProcessorsADSP21363Cross Core Embedded Studio v2.12.0adsp-21363Audio Productssoftwarecustom device programmeradsp-21364SHARC Audio Processors/SoCsDPIA buffer errorHow do I implement LibIntegrationAsDemoUc functionality on the adsp21565Forum ThreadAnswered SigmaStudio for SHARC27 December, 2023Hi, I hope to implement LibIntegrationAsDemoUc function on our ADSP21565. Now the sigmastudio project has been completed and the CCES code has been implemented, as shown in the attachment. But I don't understand the exported sigmastudio data: How to convert SMAP_Data_IC_1, Program_Data_IC_1, Param … Audio Signal ProcessorsAudio ProductssoftwareADSP-21565ADSP21565SHARC Audio Processors/SoCsONLY USE S/PDIF Transmitter IN adsp21565?Forum ThreadAnswered ADSP-2156x20 December, 2023I want ONLY use S/PDIF Transmitte in adsp21565 and i encount some issue . the route: sport3B(tx)---------SPDIF TX0 (tx) ---------DAI0_PIN08(TX) 1 the next picture about my pcg B config and it's right? nDIV=2 ,ADI_PCG_CLK_EXT=24.576MHz(DAI0_PIIN03) 2 the next … ADSP-21569Audio Signal ProcessorsAudio Productsspdif 21565ADSP21565SHARC Audio Processors/SoCs在Sigma Studio 4.6 中,怎么将ADSP21593的程序怎么烧进Flash里,实现脱机运行?Forum ThreadAnswered SigmaStudio for SHARC26 November, 2023在Sigma Studio中,怎么将ADSP21593的程序怎么烧进Flash里,实现脱机运行? SigmaStudio for SharcsoftwareADSP21569Sigma Studio 4.6adsp21593ADSP21569 spi slave mode transfer errorForum ThreadAnswered ADSP-2156x30 October, 2023 I use microcontroller to communicate with 21569. 21569 is in slave mode. I use the function of "adi_spi_DMAWrite" in the file "adi_spi_2156x.c" in CCES to let 21569 transfer data in dma mode and in slave mode I found that 21569 transfer less data that … cceshardwareADSP21569ADSP-2156xCCES2.11.0ADSP21569的FIFO内存问题 - Translation: FIFO memory problem of ADSP21569Forum ThreadAnswered CrossCore Embedded Studio and Add-ins24 October, 2023Translation: Real-time audio processing is performed through ADSP21569, and the calculated data is first stored in the FIFO queue and then output for playback. However, the sound played was stuck, and after pausing, it was found that the FIFO sequence had exceeded the capacity. 通过ADSP21569进行 … ADSP-21569Audio Signal ProcessorsAudio ProductshardwarebufferADSP-2156xCCES2.11.2fifoSHARC Audio Processors/SoCsHow to change ldf file in adsp21569 projectForum ThreadAnswered CrossCore Embedded Studio and Add-ins15 October, 2023How can I create some custom memory and section in ldf In the 21569 cces project, I want to split the block3 to two memory in the ldf file, and then I create the section. and use the "section()" section pragma in .c file to link some data into the … ADSP-21569Audio Signal ProcessorsAudio ProductsCCES 2.11.1softwarecrosscore embedded studioSHARC Audio Processors/SoCs <<<1234567>>>