主页
Search
left arrow 返回 主页
Clear Search Box Icon

“ADSP-BF506” 的搜索结果

筛查

筛查

filter-icon
产品分类
  • A/D Converters (ADC) 3
  • Amplifiers 14
  • Audio Products 4
  • Clock and Timing 2
  • D/A Converters (DAC) 2
filter-icon
资源
  • Evaluation Board 1,135
filter-icon
行业解决方案
  • A2B Audio Bus Technology 4
  • Aerospace and Defense Systems 1,135
  • Automotive Solutions 188
  • Consumer Technology Solutions 52
  • Data Center Solutions 32
filter-icon
工具和模型
filter-icon
技术解决方案
  • A2B Audio Bus Technology 6
  • Gallium Nitride (GaN) Technology 2
  • Gigabit Multimedia Serial Link (GMSL) Technology 1
  • Industrial Automation 1
  • Precision Technology Solutions 1
filter-icon
网站部分
  • 1,135
filter-icon
结果类型
filter-icon
群组、论坛和库
filter-icon
filter-icon
Analog Devices Inc. logo Analog.com
1,135
engineer-zone-play-icon EngineerZone中文技术论坛
10,360

Analog.com上的搜索结果

1,135
相关性
相关性
最旧
最新

排序

    Clear All Filters Icon
    External Link Icon arrow External Link Icon External Link Icon Tag pst-icon
    1. EVAL-ADRF5046
      Evaluation Board & Kit
      ADRF5046-EVALZ is a fully populated, connectorized evaluation board using 4-layer, 62 mil thick, RO4003 PCB material.  For normal operation, two supply voltages +3.3V and -3.3V should be applied to the VDD and VSS test points respectively, while their ground voltages are connected to the GND test point. Two control input voltages, 0/+3.3V, should be applied to V1 and V2 test points to select the switch states; RFC to RF1 …
      EVAL-ADRF5046

      文件

    2. EVAL-ADRF5160
      Evaluation Board & Kit
      Generate the evaluation PCB with proper RF circuit design techniques. Signal lines at the RF port must have a 50 Ω impedance, and the package ground leads and backside ground slug must connect directly to the ground plane. The evaluation board available from Analog Devices, Inc. upon request.
      EVAL-ADRF5160

      文件

    3. EVAL-ADRF5042
      Evaluation Board & Kit
      The ADRF5042-EVALZ (see Figure 1) is designed to evaluate the features and performance of the ADRF5042 100 MHz to 44 GHz, nonreflective, SP4T switch manufactured in the silicon on insulator (SOI) process. For full details on the ADRF5042, see the ADRF5042 data sheet, which must be consulted in conjunction with this user guide when using the ADRF5042-EVALZ.
      EVAL-ADRF5042

      文件

    4. EVAL-ADRF5026
      Evaluation Board & Kit
      ADRF5026-EVALZ is a fully populated, connectorized evaluation board using 4-layer, 62 mil thick, RO4003 PCB material.  For normal operation, two supply voltages +3.3V and -3.3V should be applied to the VDD and VSS test points respectively, while their ground voltages are connected to the GND test point. Two control input voltages, 0/+3.3V, should be applied to EN and CTRL test points to select the switch state between RFC-RF1 …
      EVAL-ADRF5026

      文件

    5. EVAL-ADRF5027
      Evaluation Board & Kit
      ADRF5027-EVALZ is a fully populated, connectorized evaluation board using 4-layer, 62 mil thick, RO4003 PCB material.  For normal operation, two supply voltages +3.3V and -3.3V should be applied to the VDD and VSS test points respectively, while their ground voltages are connected to the GND test point. Two control input voltages, 0/+3.3V, should be applied to EN and CTRL test points to select the switch state between RFC-RF1 …
      EVAL-ADRF5027

      文件

    6. ADIS16507-x/PCBZ
      Evaluation Board & Kit
      The ADIS16507-x/PCBZ breakout boards provide a convenient method for establishing a prototype connection between each ADIS16507 IMU model and an embedded processor platform. Each ADIS16507-x/PCBZ breakout board connects to J1 on the EVAL-ADIS2 evaluation system, as well.
      ADIS16507-x/PCBZ

      文件

    7. EVAL-ADISIMU1-RPIZ
      Evaluation Board & Kit
      This adaptor board allows for easy plug and play connection of Analog Devices Inertial Measurement Unit (IMU) devices to the Raspberry Pi platform, providing application and software development. There are two ways in which to connect your IMU to this adaptor board. Direct board mounting using the screws and mounting locations provided. Mount the IMU to a separate ADIS16IMU1/PCBZ or ADIS16IMU4/PCBZ breakout board and use the flexible 16-position ribbon cable to the …
      EVAL-ADISIMU1-RPIZ

      文件

    8. EVAL-ADA4571
      Evaluation Board & Kit
      The EV-ADA4571RSDZ evaluation board features the ADA4571 in an end of shaft magnet configuration. The evaluation kit is composed of an ADA4571 motherboard, a magnetic stimulus on a hand turnable mount, a USB interface, and an SDP-S controller board. The required LabVIEW 2015 graphical user interface (GUI) software for Windows® is available for download from the EV-ADA4571RSDZ product page. The EV-ADA4571RSDZ evaluation board features an on-board 5 V regulator …

      文件

    9. ADRV9009-ZU11EG RF-SOM
      Evaluation Board & Kit
      The ADRV9009-ZU11EG is a highly integrated RF System-On-Module(RF-SOM) based on dual Analog Devices ADRV9009 wideband transceivers. When combined with the ADRV2CRR-FMC carrier board this hardware platform can be used for prototyping and reducing time to market for application specific designs offering 4 Tx and Rx RF channels. An additional RF board can also be fitted to the carrier to further expand the system up to 8 Tx and Rx …
      ADRV9009-ZU11EG RF-SOM

      文件

    10. DC2524A
      Evaluation Board & Kit
      Demonstration circuit 2524A is optimized for evaluation of the LTC5555 programmable gain downconverting mixer. The IC incorporates an active mixer and a digital IF VGA with 15.5dB gain control range. The IF gain is programmed in 0.5dB steps through the SPI or parallel interface. The LTC5555 has single-ended 50Ω RF input, single-ended or differential-drive LO input, and differential IF output. It features an enable pin for fast turn-on and …
      DC2524A

      文件

    • <<
    • <
    • 96
    • 97
    • 98
    • 99
    • 100
    • >
    • >>

    EngineerZone中文技术论坛上的搜索结果

    10,360
      Clear All Filters Icon
      很抱歉,我们没有找到符合搜索条件的结果。请使用其他搜索关键词和/或更改筛选条件后重试。
      • <<
      • <
      • 1
      • >
      • >>
    • 关于我们
    • 职位信息
    • 新闻中心
    • 我们做些什么
    • 投资者关系
    • 销售和分销商
    • Analog.com 上的最新内容
    • 联系我们
    • 支持
    • 中文技术论坛
    • 资源库
    • Wiki
    • 模拟对话
    • 法律与风险
    • 可访问性
    • 隐私设置
    • 隐私与安全
    • Cookie 设置
    • Bilibili
    • Linkedin
    • Weixin Code