搜索 筛查 筛查 产品分类 更多 资源 更多 行业解决方案 更多 工具和模型 技术解决方案 更多 网站部分 结果类型 Blog2Blog Post216Comment342Docs & FAQs3,228Forum Reply46,661Forum Thread17,917Gallery10Groups, Forums & Libraries43更多 群组、论坛和库 ADE电能计量专区1,416ADUC Cortex M3系列162ADUC7xxx系列162ADUC微处理器专区1,472GMSL437MEMS专区3,290Other Products (CN)1,789Power 中文专区4,530更多 ADIApproved5,356ADIForum1,095ADI_Amy562ADI_Eva344ALee687779Admin_ADI1,259Amenda-NanYa289EZAdministrator1,173更多 Precision A/D Converters1,368amplifiers1,110hardware921Integrated/Special Purpose A/D Converters749clock and timing747RF Integrated Transceivers729Sensors and MEMS685Wideband Transceiver IC666更多 Analog.com 0 EngineerZone中文技术论坛 68,445 Analog.com上的搜索结果 0 相关性 相关性 最旧 最新 排序 Site_section:媒体中心✕展会✕新闻咨询✕资源库资源库✕Product_categories.lvl0:Audio Products✕ 清除选择 很抱歉,我们没有找到符合搜索条件的结果。请使用其他搜索关键词和/或更改筛选条件后重试。 <<<1>>> EngineerZone中文技术论坛上的搜索结果 68,445 Do I need separate Op-Amp for REFIO if Driving multiple AD7380 using LTC6655Forum ThreadAnswered 精密转换器专区17 April, 2025Hi, I need to use 3 to 4 AD7380 for data collection and using 1 LTC6655 for Reference Voltage. I do not know whether the sink current of REFIO pin is suffice. Do I need 3 to 4 Op Amp for buffering each AD7380 REFIO pin if I need to … Series Voltage ReferencesSimultaneous Sampling A/D ConvertersAD7380voltage referencesPrecision A/D Convertersltc6655Open Loop Simulation of AD8605Forum ThreadAnswered 放大器专区12 April, 2025Hello I would like to perform a open loop simulation of AD8605 to generate open-loop gain(AOL), 1/beta, AOLbeta curves However, the result is not what I expected. Can you support on that? Thanks in advance! Operational Amplifiers (Op Amps)Datasheet/SpecsPrecision Op Amps (Vos ≤1mV & TCVos ≤2uV/C)ad8605AD7606C-18的硬件串行模式,如何使用三线SPI,即手册中说的CS_N固定为低电平的情况,这里的时序要求是什么样的?Forum ThreadAnswered 精密转换器专区09 April, 2025我在使用EVAL-AD7606C-18的验证板,我使用FPGA去驱动它,我选择的模式是硬件串行模式,当我使用四线SPI去读取数据时,一切正常,我 … AD7606C-18softwareSimultaneous Sampling A/D ConvertersPrecision A/D Convertersfpga软件Forum ThreadAnswered 嵌入式安全与1-Wire08 April, 2025ibutton数据无法全部读取,这东西不是显示最高能存几万个数据吗,我用它记录了4000多个数据,但读取时只能读取出2048个数据 … softwareibutton数据无法全部读取iButtonAD5940_Ramp休眠唤醒问题Forum ThreadAnswered 生物/电化学/磁场/温度传感器专区07 April, 2025使用AD5940_Ramp例程,完成一次检测后,过一会AD5940进入休眠,使用 AD5940_SEQCtrlS(bTRUE); /* Enable sequencer, and wait for trigger */ AppRAMPCtrl(APPCTRL_START, 0); 程序去启动AD5940扫描,AD5940不运行。 需要 … Sensors and MEMSad5940Electrochemical Sensorsds2484 读取max1888 程序,怎么不能读取温度和IO口状态Forum ThreadAnswered 嵌入式安全与1-Wire07 April, 2025ds2484 读取max1888 程序,怎么不能读取温度和IO口状态 /* Includes ------------------------------------------------------------------*/ #include "DS2484_MAX31888.h"#include "DS2484_DS18B20.h"void DS2484_MAX31888_delay(uint32_t nCount){ for (; nCount != 0; nCount--);} /////DS2482,复位设备状态机逻辑。终 … ds2484 读取max1888 程序,怎么不能读取温度和IO口状态1-Wire Interface Products1-Wire DevicesEVAL-ADA4254 power supplyForum ThreadAnswered 放大器专区01 April, 2025I read in the EVAL-ADA4254 data sheet that VDDH and VSSH require a ±28V power supply. However, I currently do not have a ±28V power supply. I only have access to the NI ELVIS II+ experimental platform, which can provide a ±15V power supply. I saw that the ADA4254 … amplifiersADA4254hardwareInstrumentation AmplifiersEVAL-ADA4254AD7768驱动SPI读取寄存器问题?Forum ThreadAnswered 精密转换器专区31 March, 2025 寄存器读取出来全部是0E,上图为逻辑分析仪抓取时序。 使用软件模拟SPI的方式 LVDS隔离电路ADN4650输出异常Forum ThreadAnswered 接口和隔离专区26 March, 2025将一个20ns窄脉冲输入到比较器AD8465的正端,负端为固定电平,将AD8465输出送入LVDS隔离电路ADN4650的输入;当AD8465输入正负端幅度相等 … About IBIAS of LTC6811-1Forum ThreadAnswered 能源存储系统(ESS)和电池管理系统(BMS)23 March, 2025LTC6811的IBIAS接口在isoSPI电路唤醒之后,根据规格书所述,IBIAS引脚电平应当在2V(误差在0.1V内)左右。且关于该引脚电路,数据手册上 … hardwarebattery managementltc6811-1Multicell Battery Stack Monitor <<<1234567>>>