主页
Search
left arrow 返回 主页
Clear Search Box Icon

筛查

筛查

filter-icon
产品分类
filter-icon
资源
  • Evaluation Board 1
filter-icon
行业解决方案
  • Aerospace and Defense Systems 1
  • Automotive Solutions 1
filter-icon
工具和模型
filter-icon
技术解决方案
  • Gigabit Multimedia Serial Link (GMSL) Technology 1
filter-icon
网站部分
  • 1
filter-icon
结果类型
  • 34
  • 6,355
  • 99,528
  • 116,187
  • 539,433
  • 1,353
filter-icon
群组、论坛和库
  • 11,168
  • 10,638
  • 14,952
  • 13,071
  • 9,803
  • 18,534
  • 17,598
  • 12,624
filter-icon
  • 30,783
  • 1,447
  • 1,422
  • 2,044
  • 1,904
  • 1,929
  • 956
  • 1,009
filter-icon
  • 55,394
  • 55,214
  • 52,549
  • 39,571
  • 32,372
  • 27,669
  • 27,328
  • 24,360
Analog Devices Inc. logo Analog.com
1
engineer-zone-play-icon EngineerZone中文技术论坛
762,892

Analog.com上的搜索结果

1
相关性
相关性
最旧
最新

排序

  • Site_section:媒体中心展会新闻咨询资源库资源库
  • Product_categories.lvl0:电源管理 > LED 驱动器 IC
Clear All Filters Icon
External Link Icon arrow External Link Icon External Link Icon Tag pst-icon
  1. MAX9288COAXEVKIT
    Evaluation Board & Kit
    The MAX9288/MAX9290 evaluation kit (EV kit) provides a proven design to evaluate the MAX9288 and MAX9290 high-bandwidth gigabit multimedia serial link (GMSL) deserializers with spread spectrum and full-duplex control channel, with the use of a standard FAKRA coaxial cable. The EV kit also includes Windows Vista®-, and Windows® 7-compatible software that provides a simple graphical user interface (GUI) for exercising features of the device. The EV kit comes with …

    文件

  • <<
  • <
  • 1
  • >
  • >>

EngineerZone中文技术论坛上的搜索结果

762,892
    Clear All Filters Icon
    1. IIO Absolute Time Tagging to GPSDO and PPS for SDR

      Forum Thread
      Answered
      Design Support AD9361/AD9363/AD9364
      20 June, 2025
      I need to have time accurate or time tagged I/Q data. Adding PPS and a GPSDO are straightforward enough to a reference design. Does there exist any concept of absolute time in IIO? Could I easily extended iio to support time tags? Utilities like iio_readdev seem to suggest …
      iioad9361sdrplutoWideband Transceiver ICRF Integrated Transceivers

    2. SIO (Set Output) command in TMCL

      Forum Thread
      Answered
      Other Products (EN)
      19 June, 2025
      I'm using the TMCM-3216-TMCL board with the TCML-IDE 4.7.1 and try to flip the digital IO pins using the SIO command. I can't see any voltage change on the output pin nor any change in the LED indicator on the board. Is there …
      hardwareTMCM-3216-TMCL

    3. phase difference in channels

      Forum Thread
      Answered
      High-Speed ADCs
      18 June, 2025
      Hello there, I used an AD9613 EVAL-BOARD for sampling from two sine signal (two sine signal with 0 phase difference that checked up with oscilloscope too) but when I use Matlab I see that there is 180 degrees phase difference between CH1 and Ch2 of AD9613. why there is …
      Datasheet/SpecsHigh Speed A/D Converters &gt;10 MSPSad9613Standard High Speed A/D Converters

    4. input noise of the EVAL-AD9248

      Forum Thread
      Answered
      High-Speed ADCs
      18 June, 2025
      Hi I want to know what the input noise of the EVAL-AD9248. Thanks
      hardwareEVAL-AD9248ad9248High Speed A/D Converters &gt;10 MSPSStandard High Speed A/D Converters

    5. AD8293G80 Figure 6 and (Figure 9).

      Forum Thread
      Answered
      Instrumentation Amplifiers
      18 June, 2025
      The data sheet indicates that the input common mode range extends to 0V. And the /reference input should be at least 0.8V above 0V and 0.8V below Vs+. But what does the pink area of Figure 6 mean in the datasheet? My input would be roughly -in = 0V …
      amplifiersInstrumentation Amplifiers

    6. CLOCK NOISE IS HIGH

      Forum Thread
      Answered
      Clock and Timing
      18 June, 2025
      Hi;We are building a tranceiver system and block diagram like following: where ADC's sampling rate is 500KHz and both AD9520's configuration are same except remote AD9520's ref divider is 5:Zero Delay: onVCO Divider: 2Phase Detector Frequency: 10MVCO Frequency:1600MCharge Pump Current: 1.8MALoop Bandwidth: 10kHzLoop …
      Clock Generation Devicesad9520-4Clock Generation and Distributionhardware

    7. Issues with serial input ports

      Forum Thread
      Answered
      SigmaDSP Processors & SigmaStudio Dev. Tool
      17 June, 2025
      Hi all,I'm having trouble getting the serial input ports other than the first one to work.This is my setup:Serial input port 0: it's connected to an ADC that acts as an I2S master.Serial input port 1: it's connected to a microcontroller that acts …
      Audio Signal Processorsadau1452adchardwaremcuserial inputi2sSigmaDSP Audio Processors

    8. Not reading data correctly.

      Forum Thread
      Answered
      High-Speed DACs
      17 June, 2025
      The output of the JESD204B interface is not always correct. Below are my settings for the JESD204B interface. CS = 0 Control bits per Sample N' = 16 total number of bits per Sample N = 16 Converter Resolution M = 2 Converters per device S = 1 Samples per Converter per Frame CF = 0 …
      hardwareHigh Speed D/A Converters =30MSPSMAX5871incorrect dataFast Precision D/A Converters

    9. Need help to troubleshoot the simulation.

      Forum Thread
      Answered
      LTspice
      17 June, 2025
      Hi Engineers, I'm in the middle of the preliminary design of a converter that uses a forward converter at the primary side and a full bridge converter at the secondary side. However, the efficiency keeps getting stuck and is not able to reach >80% as expected. Appreciate your help …
      software

    10. AD9576 Eval board SPI configuration support and frequency conversion with dual PLL

      Forum Thread
      Answered
      Clock and Timing
      17 June, 2025
      Hi Team, Here we are trying to configure AD9576 eval board. We need your support in configuring the SPI communication ( Pins in Eval board hardware and the setting to be used in ACE installer). Also can you please assist in, 1. To convert the on-board crystal Ref input 25MHz …
      Clock Generation and DistributionhardwareClock Distribution DevicesAD9576ACE installer

    • <<
    • <
    • 1
    • 2
    • 3
    • 4
    • 5
    • 6
    • 7
    • >
    • >>
  • 关于我们
  • 职位信息
  • 新闻中心
  • 我们做些什么
  • 投资者关系
  • 销售和分销商
  • Analog.com 上的最新内容
  • 联系我们
  • 支持
  • 中文技术论坛
  • 资源库
  • Wiki
  • 模拟对话
  • 法律与风险
  • 可访问性
  • 隐私设置
  • 隐私与安全
  • Cookie 设置
  • Bilibili
  • Linkedin
  • Weixin Code