搜索 筛查 筛查 产品分类 A/D Converters (ADC) 2 Amplifiers 1 Sensors and MEMS 1 更多 资源 Evaluation Board 3 Technical Documentation 1 更多 行业解决方案 Aerospace and Defense Systems 5 Automotive Solutions 7 Consumer Technology Solutions 1 Energy Solutions 5 Healthcare Solutions 5 更多 工具和模型 技术解决方案 ADI OtoSense™ Predictive Maintenance Solutions 1 Precision Technology Solutions 1 Sensor Interface Solutions 1 更多 网站部分 Resource Library4 结果类型 Blog Post7Docs & FAQs39Forum Reply886Forum Thread299Webinar3更多 群组、论坛和库 ADIsimPE Library1ARM7 Core Products2Amplifiers29Audio12Automated Test Equipment (ATE)1Clock and Timing6Design Tools and Calculators1Differential Amplifiers and ADC Drivers86更多 ADIApproved115DanLavry14EZAdministrator35Emman.A10Fdelaram57FormerMember25Gauzz29GenevaCooper18更多 Operational Amplifiers (Op Amps)208amplifiers200High Output Current Op Amps = 100mA87ada487087High Speed Op Amps (Bandwidth = 50MHz)44hardware43Low Input Bias Current Op Amps (≤100 pA)35Precision Op Amps (Vos ≤1mV & TCVos ≤2uV/C)28更多 Analog.com 4 EngineerZone中文技术论坛 1,234 Analog.com上的搜索结果 4 相关性 相关性 最旧 最新 排序 Industry_solutions.lvl0:医疗健康解决方案✕Technology_solutions.lvl0:A2B Audio Bus Technology✕ 清除选择 很抱歉,我们没有找到符合搜索条件的结果。请使用其他搜索关键词和/或更改筛选条件后重试。 <<<1>>> EngineerZone中文技术论坛上的搜索结果 1,234 OPAMP Output oscillating when driving ADC Input, ADA4807-1, AD9236Forum ThreadAnswered Operational Amplifiers24 September, 2024Image is showing an AD4807-1 based driver for ADC input.ADC is AD9236BCPZ-80 running at 12 MHz.At output of OPAMP I'm measuring approx. 200 mVp-p AC ripple looking somewhat as AM-modulated signal.At Pin 4 of OPAMP I'm measuring steady sinewave 1.2Vp … Operational Amplifiers (Op Amps)ADA4807-1hardwareada4807adc inputHigh Speed Op Amps (Bandwidth = 50MHz)AD9236BCPZ-80High Speed A/D Converters >10 MSPSStandard High Speed A/D ConvertersADA4807 max input currentForum ThreadAnswered Other Products (EN)26 January, 2024I cannot find where the Max input current is specified in the datasheet. If the input voltage may exceed the supply voltage for short periods what source resistance will I need to use to protect the device ? Many thanks, Ian Datasheet/Specsada4807ADA4807-4 Spice ModelForum ThreadAnswered Operational Amplifiers04 November, 2022Hi I did a simulation in LTSpice using the ADA4807-4 OpAmp. I want to use it to generate a triangular waveform. But my calculations do not match the simulation. I changed the OpAmp. And it works with all other OpAmps I tried with similar specifications. Is the spice model … Operational Amplifiers (Op Amps)Datasheet/Specsamplifiersada4807triangularLTspiceHigh Speed Op Amps (Bandwidth = 50MHz)ada4807-4ADA4807 Disable ThresholdsForum ThreadAnswered Operational Amplifiers22 July, 2022Table 10 of the datasheet for this part specifies the disable thresholds for +/-5V operation as: Enabled when > 1.6V Disabled when < 1.3V It also provides a graph (Figure 64) for determining the thresholds for any operating voltage. The thresholds provided by this graph are graph are higher (3 … Datasheet/Specsada4807ADA4807-1 had output oscillation on Non-inverting TopologyForum ThreadAnswered Operational Amplifiers15 January, 2021… of ADA4807-1 is 13.26MHz Oscillation waveform. My schematic of PCB is the same as LTspice. I use 100nF X7R & 6.8uF X5R on ADA4807-1 bypass capacitor. Following is the Oscilloscope waveform. CH1 is ADA4807-1 output, CH2 is ADA4807-1 input. Why dose the ADA4807-1 oscillation … Operational Amplifiers (Op Amps)ADA4807-1non_inverting_amplifieramplifiersada4807opampamplifierHigh Speed Op Amps (Bandwidth = 50MHz)Not able to understand ADA4807-2ACP's behaviorForum ThreadAnswered Differential Amplifiers and ADC Drivers19 December, 2020Hi I have set up the ADA4807 in simulation as shown in the picture below and I do not seem to get the gain unlike mentioned in the article A Low Power, Low Cost, Differential Input to a Single-Ended Output Amplifier | Analog Devices What am I doing wrong here … ada4807LTspiceADA4807 Spice Model Slew Rate Modeled Correctly?Forum ThreadAnswered Operational Amplifiers19 December, 2018Hello, I am using the ADA4807 model to model the ADA4807-2 in an active filter application where the output is a 10 MHz sinewave. The output has a peak voltage of 1.79 V. Theoretical calculation shows: Min Req Slew Rate = 2 * pi * 10 * f * Vpeak/(10^6) V … Operational Amplifiers (Op Amps)amplifiersspice modelspiceada4807slew rateopampHigh Speed Op Amps (Bandwidth = 50MHz)ada4807-2ADA4807Forum ThreadAnswered Other Products (EN)01 December, 2015 Dear Analog Devices I am having challenge in understanding the datasheet on the ADA4807 (alternative AD8027), in respect of the output swing. My challenge is that I have an input from a potmeter, providing a voltage input to a “buffer”, using an opamp (ADA4841-1YRJZ) with gain +1. The … ada4807ada8027ada4841ADA4807: FAQDocs & FAQsAmplifiersFAQ ada4807The spec table states the capacitive load drive of the ADA4807-2 is 15pF. Can the ADA4807-2 drive larger capacitor loads? Will this heavy capacitive load make the amplifier unstable?Docs & FAQsAmplifiersQ The spec table states the capacitive load drive of the ADA4807-2 is 15pF. Can the ADA4807-2 drive larger capacitor loads? Will this heavy capacitive load make the amplifier unstable? A Yes, the ADA4807-2 can drive larger capacitor loads. A capacitive load adds an extra pole to … ada4807 <<<1234567>>>