搜索 筛查 筛查 产品分类 更多 资源 更多 行业解决方案 更多 工具和模型 技术解决方案 更多 网站部分 结果类型 Docs & FAQs2Forum Reply50Forum Thread35更多 群组、论坛和库 ARM7 Core Products1Clock and Timing3Data Converters1Differential Amplifiers and ADC Drivers4Direct Digital Synthesis (DDS)22High-Speed ADCs1Instrumentation Amplifiers2Interface and Isolation4更多 ADIApproved9Alon1Ayo1Ben241DLobb3841EZAdministrator1EricC1GHz1更多 Direct Digital Synthesis (DDS)13clock and timing13Capacitive-to-Digital and Touch Screen Controllers9Integrated/Special Purpose A/D Converters9ad77467ad99106Precision A/D Converters5ad98345更多 Analog.com 0 EngineerZone中文技术论坛 87 Analog.com上的搜索结果 0 相关性 相关性 最旧 最新 排序 Industry_solutions.lvl0:医疗健康解决方案✕ 清除选择 很抱歉,我们没有找到符合搜索条件的结果。请使用其他搜索关键词和/或更改筛选条件后重试。 <<<1>>> EngineerZone中文技术论坛上的搜索结果 87 RE: Current stability of ADN2830?Forum ReplyPower Management05 March, 2014… noise performance numbers either bu I think it will be lower as it is not designed for high speed applications. Additional Pulse Oximeter application also require very low noise currnet sources. Here are a couple of examples: http://www.analog.com/en/circuits-from-the-lab/cn0125/vc.html LucaV Queries on CN-0105: drive ckt for AD7626Forum ThreadAnswered Differential Amplifiers and ADC Drivers25 July, 2024… factor of 10 & 100 accordingly. How is the idea? In addition, I want to use the ADA4932 for driving the AD7626 rather than ADA4899. In CN-0105, it is mentioned that ADA4899 is the recommended driver at lower frequencies. I want to know what are the issues with ADA4932 at … Operational Amplifiers (Op Amps)Single Channel A/D Convertersamplifiersada4899-1Differential Amplifiers and ADC Driversada4932-1ad7626Precision A/D ConvertersSingle-Ended to Differential AmplifiersHigh Voltage Op Amps =12VCN-0156 ,Similar to it needed Amplitude Control of Sine wave from 0.5VAC to 6VACForum ThreadAnswered Reference Designs28 December, 2018Dear Sir/Madam, I am looking for Amplitude Control of Sine wave from( 0.5VAC to 5.5VAC) with Frequency of 400Hz, Amplitude Control thought microcontroller or thought SPI interface, https://www.analog.com/media/en/reference-design-documentation/reference-designs/CN0156.pdf The about link is Somewhat okay but … clock and timingad9833ad9850ad9834Direct Digital Synthesis (DDS)cn-0156Amplitude Control of Sine wavead9833_designSome questions about the synchronization of AD9910 in the CN-0121Forum ThreadAnswered Direct Digital Synthesis (DDS)15 November, 2018 Hi I am synchronizing two AD9910 according to CN-0121, and have some questions. In the CN-0121,it uses the AD9520 to provide the clock signal.Is the purpose of AD9520 frequency multiplication?Does AD9520 have other purposes? I want to use one crystal oscillator to provide the … clock and timingDirect Digital Synthesis (DDS)ad9910ADC Selection, Circuit Note CN-0254 opamp selectionForum ThreadAnswered Precision ADCs13 June, 2017… Could you suggest any ADC that supports these specifications? Alternatively, could you provide solution to this design. Also, I am referring to the circuit note CN-0254. The opamp AD8608 has a slew rate of 5V/us. However, the maximum signal frequency is 1.5MHz and output voltage peak is … Operational Amplifiers (Op Amps)amplifiersad8608cn-0254Low Input Bias Current Op Amps (≤100 pA)ADuM5000 questions (CN-0159)Forum ThreadAnswered Reference Designs14 October, 2011I am looking at Analog Devices Circuit Note CN-0159, the schematic on page 2 uses a ADuM5000 at location U2_C2. The schematic ties pin 11 ( no connect) to Viso and has the note. "DNP R10_C2 if U2_C2 is an AduM5000". The device in this location is … isopowerDigital Isolation Technologydnpadum5000cn-0159about CN-0257 .20-bit, linear, low noise, precision, unipolar +10 V DC voltage sourceForum ThreadAnswered Precision DACs09 April, 2019https://www.analog.com/media/cn/reference-design-documentation/reference-designs/CN0191.pdf 20-bit, linear, low noise, precision, bipolar ±10V is described in your solution DC voltage source. Now we want to adjust the output voltage to +-50V. How should I modify it? Whether to adjust the output op … RE: CN-0156 ,Similar to it needed Amplitude Control of Sine wave from 0.5VAC to 6VACForum ReplyReference Designs06 May, 2019Hi pavankumarsn27, The datasheet for the AD9834 is indeed a bit light on signal conditioning for the output signal, but fundamentally, the outputs are two complementary current sources, with a compliance voltage of +0.6V. That is, if the output load resistance is too high such that the output voltage … RE: CN-0156 ,Similar to it needed Amplitude Control of Sine wave from 0.5VAC to 6VACForum ReplyReference Designs05 May, 2019Hi, I moved your thread to the Reference Circuits Community. They could give some insights regarding your application. Best regards, Mark RE: about CN-0257 .20-bit, linear, low noise, precision, unipolar +10 V DC voltage sourceForum ReplyPrecision DACs10 April, 2019You can post your question about ADCs, input driver, signal conditioning on this link. Someone should be able to help you on your ADC requirements. Best regards, Rainier <<<1234567>>>