LTspice: Parametric Plots

2013-08-06

Plotting results in LTspice is as easy as clicking on a node to show voltage, or a component to show current—the trace is then displayed in the waveform viewer. In transient analysis, the horizontal axis defaults to showing time, but you can always change the horizontal axis to show other quantities (such as current) to validate model parameters.

To change the default settings of the X-axis:

  1. Click on a node/component to plot its voltage/current in the waveform viewer.
  2. Move the cursor to the horizontal axis of the waveform viewer (the cursor will turn into a ruler) and right-click.
  3. In the Horizontal Axis dialog, enter an expression for the “Quantity Plotted.
  4. Click OK.

关于作者

Gabino Alonso
Gabino Alonso目前是Power by Linear™部门的战略营销总监。加入ADI公司之前,Gabino在凌力尔特、德州仪器、加州理工州立大学担任过市场营销、工程、运营和讲师等多个职位。他拥有加州大学圣巴巴拉分校电子和计算机工程硕士学位。

关联至此文章

产品

资源

最新视频 21

Subtitle
了解更多