How to Use the MAX17501 and MAX17502 for Negative Output Voltage Applications

2014-04-30
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目

摘要

This article shows how to produce negative output voltages from positive input voltages using the MAX17501 and MAX17502 synchronous step-down converters.

Introduction

Industrial control equipment such as programmable logic controllers, I/O modules, mass flow controllers, and various other sensors and supporting systems use analog components like amplifiers and multiplexers that operate on negative supply voltage. Typically operating at ±12V, ±18V or other variations, these voltages are generated from a 24V DC bus. Maxim’s portfolio of high-voltage synchronous buck regulators offer 50% lower power loss allowing customers to operate their equipment 50% cooler. In this application note, we discuss techniques to use these synchronous buck regulators to generate negative voltages.

Design Considerations

Synchronous buck converters can be configured to work in a buck-boost topology to produce negative output voltage from positive input voltage. This application note explains how the MAX17501 and MAX17502 synchronous step-down converters can be used to generate negative output voltage from positive input voltage. A -15V output voltage application is used to demonstrate the principle.

Table 1. Negative Output Voltage Power-Supply Requirements

VIN Operating input voltage 24V ±6V
VOUT Output voltage -15V
IOUT Maximum output current 500mA
VIN_ripple Steady-state input ripple voltage 1% of nominal VIN
VOUT_ripple Steady-state output ripple voltage 1% of nominal VOUT

Operating Input Voltage Range

The sum of the maximum operating input voltage for the negative output application and the absolute value of the output voltage should not exceed the maximum operating voltage (60V) of the MAX17501 and MAX17502, as expressed by the following equation:

VIN_MAX + |VOUT| < 60V

Therefore, for -15V output voltage, maximum operating input voltage can be as high as 45V. The minimum operating input voltage for the negative output voltage application should be greater than 4.5V.

Calculating Duty Ratio

The expression for the duty ratio of the negative output power supply is shown below; ignoring the losses associated with the power switches and the inductor DC resistance:

Equation 1.

For the specifications listed above, the duty cycle varies between 0.45 at 18V input voltage to 0.33 at 30V input voltage. At the nominal input voltage of 24V, duty cycle is 0.38. Note that the highest duty ratio (DMAX) occurs at the minimum operating input voltage and the lowest duty ratio (DMIN) occurs at the maximum operating input voltage (VIN_MAX).

Load Current Capability and Part Number Selection

The negative output voltage design requirements are not compatible with the versions of the MAX17501 and MAX17502 that have internal compensation—so, consider only the G and H versions of the MAX17501 and MAX17502 for building negative output voltage applications.

To estimate whether the MAX17501 and MAX17502 are capable of delivering the required output current, the value of the maximum inductor average current should be calculated first, based on the following equation:

Equation 2.

Assume IL_MAX to be 550mA and 1.2A for the MAX17501 and MAX17502, respectively, to allow some room for the output capacitor charging current. Assuming the value of the maximum inductor ripple (ΔIL) is 250mA for the MAX17501 and 500mA for the MAX17502, we arrive at the following maximum values of IL_AVG for both parts:

IL_AVG = 425mA for the MAX17501
IL_AVG = 950mA for the MAX17502

The maximum load current that can be supported by the MAX17501 and the MAX17502 is expressed by the following equation:

IOUT_MAX = IL_AVG × (1 - DMAX)

Since DMAX is 0.45 for the specifications being targeted here, IOUT_MAX is calculated as 234mA for the MAX17501 and 522mA for the MAX17502. Therefore, the MAX17502G is selected for this application. It is recommended to design with the MAX17501 whenever the targeted IOUT is less than the maximum load current allowed by the MAX17501.

Start Voltage

When used as a buck converter, the voltage at which the MAX17501 and MAX17502 turns on/off can be adjusted by using the resistive divider connected from the VIN pin to GND. When used as a negative output voltage power supply, only the start voltage can be programmed by the resistive divider. When the part turns on, the effective input voltage experienced by the part increases as the output voltage builds up to full regulation voltage. The input voltage must drop by the absolute value of the output voltage to shut down the part.

Applications Information

Inductor Selection
Based on ripple current requirements, the minimum value of the inductance is calculated by the following equation:

Equation 3.

The switching frequency (fSW) is 600kHz for the MAX17501G and MAX17502G parts and 300kHz for the MAX17501H and MAX17502H. Assuming maximum inductor ripple (ΔIL) to be 500mA for the MAX17502, LMIN turns out to be 27µH for the specifications mentioned in Table 1.

Slope compensation requirements impose the following constraint on the inductor value:

Equation 4.

where x = 4 for the MAX17502G, x = 8 for the MAX17501G and MAX17502H, and x = 16 for the MAX17501H.

The constraint shown above is valid only if the maximum duty ratio is greater than 0.25. Since MAX17502G has been selected for this application, the inductor value should be between 27µH and 160µH for the specifications mentioned in Table 1. A 33µH inductor has been used for this application.

Ensure that the saturation current of the selected inductor is greater than the peak current limits of the MAX17501 and MAX17502.

Input Capacitor Selection
The minimum value of the input capacitor is expressed as follows:

Equation 5.

Inductor ripple (ΔIL) in the above equation should be calculated based on the actual inductance value chosen for the application:

Equation 6.

where LSEL is the selected inductance. For the specifications mentioned in Table 1, the CIN_MIN turns out to be 0.36µF. A 2.2µF capacitor in 1206 package has been used for this design. The capacitance derates to approximately 1.3µF at 24V input voltage.

Output Capacitor Selection
The minimum required value of the output capacitor is calculated by the following equation:

Equation 7.

For the specifications mentioned in Table 1, the COUT_MIN turns out to be 2.5µF. A 4.7µF capacitor in 1206 package has been used for this design. The capacitance derates to approximately 2.5µF at 15V output voltage.

Adjusting Output Voltage
Set the output voltage with a resistive voltage-divider connected from the ground terminal of the inductor to VOUT. Connect the center node of the divider to the FB/VO pin. Select the values of resistors R4 and R5 as follows:

Equation 8.

where R4 and R5 are in kΩ. The values of R4 and R5 selected for this application are 243kΩ and 15.4kΩ, respectively.

Setting the Input Turn-On Voltage
Set the input voltage at which the MAX17501 and MAX17502 turn on with a resistive voltage-divider connected from VIN to VOUT (see Figure 1). Connect the center node of the divider to the EN/UVLO pin. Choose R1 to be 3.3MΩ, and then calculate R2 as:

Equation 9.

where VINU is the input voltage at which the MAX17501 and MAX17502 are required to turn on. Selecting a value of 261kΩ for R2 results in the part turning on at 16.6V input voltage.

External Loop Compensation
Compensation components R3 and C5 should be calculated as follows:

Equation 10.

where k = 1 for the MAX17502 and k = 2 for the MAX17501.

The value of C5 should be calculated as follows:

Equation 11.

Use the DC voltage derated value of the output capacitor (COUT) while calculating the values of R3 and C5. DC voltage derating curves are available from all major capacitor vendors. Using the derated value of output capacitance (2.5µF), the value of R3 turns out to be 7.8kΩ. Choosing R3 of 7.5kΩ results in the value of C5 being 6800pF.

Soft-Start Capacitor Selection
The MAX17501 and MAX17502 implement adjustable soft-start operation to reduce inrush current. A capacitor connected from the SS pin to VOUT programs the soft-start period. The soft-start time (tSS) is related to the capacitor connected at SS (CSS) by the following equation:

CSS = 5.55 × tSS

where tSS is in milliseconds and CSS is in nanofarads. For example, to program a 1.2ms soft-start time, a 6800pF capacitor should be connected from the SS pin to VOUT.

Schematic for the Design
Schematic for the design.
Figure 1. Schematic for the design.

Bill of Materials

Table 2. Bill of Materials

Designator Value Description Part Number Manufacturer Package Qty
C1 2.2µF/X7R/50V Input bypass capacitor GRM31CR71H225KA88L Murata 1206 1
C2 1µF/X7R/6.3V VCC bypass capacitor GRM188R70J105KA01 Murata 0603 1
C3 6800pF/X7R/25V Soft-start capacitor GRM155R71E682KA01D Murata 0402 1
C4 4.7µF/X7R/25V Output capacitor GRM31CR71E475KA88L Murata 1206 1
C5 6800pF/X7R/25V Compensation capacitor GRM155R71E682KA01D Murata 0402 1
C9 Not installed       0402 0
L1 33µH Inductor MSS1048-333ML Coilcraft 10.2mm x 10mm 1
R1 3.32MΩ ±1% EN/UVLO resistor-divider     0402 1
R2 261kΩ ±1% EN/UVLO resistor-divider     0402 1
R3 7.5kΩ ±1% Compensation resistor     0402 1
R4 243kΩ ±1% FB resistor-divider     0402 1
R5 15.4kΩ ±1% FB resistor-divider     0402 1
U1   Internal switch buck converter MAX17502GATB+ Maxim 10 TDFN 3 x 2 1

Experimental Results
  • Efficiency of the Negative Output Power Supply
  • Efficiency vs. load current.
    Figure 2. Efficiency vs. load current.

  • Load and Line Regulation of Output Voltage
  • Load and line regulation of output voltage.
    Figure 3. Load and line regulation of output voltage.

  • Soft-Start/Turn-Off of Output Voltage
  • Soft-start with 500mA load on output.
    Figure 4. Soft-start with 500mA load on output.

    Shutdown with 500mA load on output.
    Figure 5. Shutdown with 500mA load on output.

    Soft-start with no load on output.
    Figure 6. Soft-start with no load on output.

    Shutdown with no load on output.
    Figure 7. Shutdown with no load on output.

  • Switching Waveforms
  • Switching waveforms at no load.
    Figure 8. Switching waveforms at no load.

    Switching waveforms at 500mA load.
    Figure 9. Switching waveforms at 500mA load.

  • Load Transient Waveforms
  • Load-transient response from no load to 250mA.
    Figure 10. Load-transient response from no load to 250mA.

    Load transient response from 250mA to 500mA.
    Figure 11. Load transient response from 250mA to 500mA.

  • Bode Plot
  • Bode plot at full load.
    Figure 12. Bode plot at full load.

Layout of the Evaluation Board

Component-side PCB layout.
Figure 13. Component-side PCB layout.

Solder-side PCB layout.
Figure 14. Solder-side PCB layout.

Component placement guide.
Figure 15. Component placement guide.

Top solder mask.
Figure 16. Top solder mask.

Bottom solder mask.
Figure 17. Bottom solder mask.

Appendix: Additional Reference Designs

The schematic shown in Figure 1 corresponds to all the following reference designs.

  • Reference Design 2: VIN = 22V to 30V, VOUT = -24V, IOUT = 150mA
  • Table 3. Bill of Materials for Reference Design 2

    Designator Value Description Part Number Manufacturer Package Qty
    C1 0.47µF/X7R/50V Input bypass capacitor GRM31MR71H474KA01 Murata 1206 1
    C2 1µF/X7R/6.3V VCC bypass capacitor GRM188R70J105KA01 Murata 0603 1
    C3 6800pF/X7R/25V Soft-start capacitor GRM155R71E682KA01D Murata 0402 1
    C4 2.2µF/X7R/50V Output capacitor GRM31CR71H225KA88 Murata 1206 1
    C5 12000pF/X7R/25V Compensation capacitor GRM155R71E123KA61D Murata 0402 1
    C9 Not installed       0402 0
    L1 150µH Inductor VLP8040T-151M TDK 8mm x 7.7mm 1
    R1 3.32MΩ ±1% EN/UVLO resistor-divider     0402 1
    R2 215kΩ ±1% EN/UVLO resistor-divider     0402 1
    R3 10.7kΩ ±1% Compensation resistor     0402 1
    R4 392kΩ ±1% FB resistor-divider     0402 1
    R5 15.4kΩ ±1% FB resistor-divider     0402 1
    U1   Internal switch buck converter MAX17501GATB+ Maxim 10 TDFN 3 x 2 1

  • Reference Design 3: VIN = 4.5V to 5.5V, VOUT = -12V, IOUT = 100mA
  • Table 4. Bill of Materials for Reference Design 3

    Designator Value Description Part Number Manufacturer Package Qty
    C1 0.47µF/X7R/50V Input bypass capacitor GRM31MR71H474KA01 Murata 1206 1
    C2 1µF/X7R/6.3V VCC bypass capacitor GRM188R70J105KA01 Murata 0603 1
    C3 6800pF/X7R/25V Soft-start capacitor GRM155R71E682KA01D Murata 0402 1
    C4 2.2µF/X7R/16V Output capacitor GRM31MR71C225KA35 Murata 1206 1
    C5 33000pF/X7R/25V Compensation capacitor GRM155R71E333KA88J Murata 0402 1
    C9 Not installed       0402 0
    L1 100µH Inductor VLC6045T-101M TDK 6mm x 6mm 1
    R1 3.32MΩ ±1% EN/UVLO resistor-divider     0402 1
    R2 1.5MΩ ±1% EN/UVLO resistor-divider     0402 1
    R3 3.24kΩ ±1% Compensation resistor     0402 1
    R4 200kΩ ±1% FB resistor-divider     0402 1
    R5 16.2kΩ ±1% FB resistor-divider     0402 1
    U1   Internal switch buck converter MAX17501GATB+ Maxim 10 TDFN 3 x 2 1

  • Reference Design 4: VIN = 18V to 30V, VOUT = -5V, IOUT = 150mA
  • Table 5. Bill of Materials for Reference Design 4

    Designator Value Description Part Number Manufacturer Package Qty
    C1 0.47µF/X7R/50V Input bypass capacitor GRM31MR71H474KA01 Murata 1206 1
    C2 1µF/X7R/6.3V VCC bypass capacitor GRM188R70J105KA01 Murata 0603 1
    C3 6800pF/X7R/25V Soft-start capacitor GRM155R71E682KA01D Murata 0402 1
    C4 2.2µF/X7R/10V Output capacitor GRM31MR71A225KA01 Murata 1206 1
    C5 3900pF/X7R/25V Compensation capacitor GRM155R71b92KA01D Murata 0402 1
    C9 Not Installed       0402 0
    L1 33µH Inductor LPS6235-333ML Coilcraft 6mm x 6mm 1
    R1 3.32MΩ ±1% EN/UVLO resistor-divider     0402 1
    R2 261kΩ ±1% EN/UVLO resistor-divider     0402 1
    R3 12.1kΩ ±1% Compensation resistor     0402 1
    R4 84.5kΩ ±1% FB resistor-divider     0402 1
    R5 18.7kΩ ±1% FB resistor-divider     0402 1
    U1   Internal switch buck converter MAX17501GATB+ Maxim 10 TDFN 3 x 2 1

    关于作者

    Dipankar Mitra

最新视频 21

Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目