Detailed Description of Hardware
The Oceanside subsystem reference design operates from a 3.3V to 15V DC power source. The MAX668 high-efficiency step-up controller boosts the input voltage to 16V and connects to the input of the H-bridge transformer driver. The MAX13256 H-bridge transformer driver switches at 425kHz and drives the primary side of the 1:1 turns ratio, with the use of TGMR-501V6LF transformers from Halo® Electronics. The full-wave bridge rectifiers convert the AC outputs of the Halo transformers’ secondary coils into DC outputs. The LDOs regulate the voltages to ±15V. The Zener diodes (D3 and D4) protect the LDOs by keeping their input voltages below 16.5V.
The output current of the H-bridge transformer driver is limited to 300mA by the R5 2.2kΩ resistor, which protects the LDO from overcurrent. The following equation sets the current limit for the H-bridge transformer driver.
R5 (kΩ) = 650/ILIM (mA)
Having a step-up controller before the H-bridge transformer driver gives users the advantage of not needing to change the transformers to get a different turns ratio when a different input supply voltage is applied.
The input power is selectable by JU1. Place the shunt on the 1-2 position to power the board by an external power supply connected to the VIN and GND1 connectors. Place the shunt on the 2-3 position to power the board by the J1 Pmod-compatible connector.
To change the output voltage of this subsystem reference design, simply change the feedback resistors (R7–R10) of the LDOs (U3 and U4), and also change the feedback resistors (R3 and R4) of the step-up controller (U1). The output voltage of the MAX668 step-up controller is set by the following equation:
- VOUT = VSET × (1 + R7/R9) for U3
- VOUT = VSET × (1 + R8/R10) for U4 Where
- VSET = 1.21V The output voltage of the MAX668 step-up controller is set by the following equation:
- VOUT = VSET × (1 + R3/R4) Where VSET = 1.25
For example, for the ±12V output application, change R7 and R8 to 90.9kΩ, and change R9 and R10 to 10.2kΩ. The output of the LDOs becomes ±12V when their inputs (outputs of the transformers and the full-wave bridge rectifiers) are higher than 12V plus the dropout voltage. Next, change R3 to 100kΩ and R4 to 10.5kΩ to set the output of the step-up controller to 13.15V (slightly higher than 12V plus the dropout voltage and two diode voltage drops from the full-wave bridge rectifier). It is important to not set this voltage too much higher than the output of LDOs, because the extra power would be lost in the LDOs and thus efficiency would be lower. In applications that are sensitive to output voltage ripple, a lowpass LC pi filter can be added in front of the LDO input.
The isolation transformer in this design has an isolation voltage of 5000VRMS. It is recognized by UL 60950 and EN 60950 and falls into the "functional" insulation class.