AN-2548: Ultra-Fast Settling PLL with RF to 13 GHz

Circuit Function and Benefits

The phase-locked loop (PLL) circuit shown in Figure 1 uses a 13 GHz fractional-N synthesizer, wideband active loop filter and VCO, and has a phase settling time of less than 5 µs to within 5° for a 200 MHz frequency jump.

The performance is achieved using an active loop filter with 2.4 MHz bandwidth. This wide bandwidth loop filter is achievable because of the ADF4159 phase-frequency detector (PFD) maximum frequency of 110 MHz; and the AD8065 op amp high gain-bandwidth product of 145 MHz.

The AD8065 op amp used in the active filter can operate on a 24 V supply voltage that allows control of most wideband VCOs having tuning voltages from 0 V to 18 V.

Figure 1. Block Diagram of ADF4159, AD8065 Active Loop Filter, and 11.4 GHz to 12.8 GHz VCO. (Simplified Schematic: All Connections and Decoupling Not Shown)
Figure 1. Block diagram of ADF4159, AD8065 active loop filter, and 11.4 ghz to 12.8 ghz vco. (simplified schematic: all connections and decoupling not shown)

Circuit Description

In a PLL and VCO frequency synthesis system, achieving less than 5 µs frequency and phase settling time requires a very wide loop bandwidth. The loop bandwidth (LBW) defines the speed of the control loop. A wider LBW allows faster settling time, at the expense of less attenuation of phase noise and spurious signals.

The circuit in Figure 1 operates by locking the ADF4159 to the RFOUT/2 signal (~6 GHz) of the 12 GHz VCO (MACOM MAOC-009269). VCOs with divide by 2 outputs can be used to generate output frequencies of up to 26 GHz. For example, if the primary output of the VCO is at 26 GHz, the divide by 2 signal (at 13 GHz) can be fed back to the ADF4159.

ADF4159 Fractional-N Synthesizer

 
In a fractional-N architecture PLL, the noise from the sigma-delta modulator (SDM) peaks at half the PFD frequency (fPFD). For example, if a fractional-N PLL has a PFD frequency of 32 MHz, then the unfiltered SDM noise peaks at 16 MHz. The SDM noise makes the loop unstable, and the PLL does not lock. Figure 2 shows a simulated phase noise plot of this condition.

Figure 2. Phase Noise Plot at 12 GHz Output with fPFD = 32 MHz and LBW = 2.4 MHz
Figure 2. Phase noise plot at 12 GHz output with fPFD = 32 MHz and LBW = 2.4 MHz

The ADF4159 has a maximum PFD frequency of 110 MHz. This means that the unfiltered SDM noise peaks at 55 MHz. Figure 3 shows a phase noise plot with a PFD frequency of 110 MHz. The SDM noise occurs at a large offset from the carrier and is therefore filtered by the loop filter.

Figure 3. Phase Noise Plot at 12 GHz Output with fPFD = 110 MHz and LBW = 2.4 MHz
Figure 3. Phase noise plot at 12 GHz output with fPFD = 110 MHz and LBW = 2.4 MHz

The ADF4159 high maximum PFD frequency is also important because it is recommended to keep the LBW less than 1/10 of the PFD frequency to ensure stability.

The ADF4159 has a maximum RF input frequency of 13 GHz. In the configuration of this circuit, the ADF4159 is actually being driven with the VCO RFOUT/2 signal. This means that when the VCO primary output is 12 GHz, the ADF4159 is actually locking to 6 GHz.

This configuration means a 24 GHz VCO can be used so that the RFOUT/2 signal of 12 GHz, is fed back to the ADF4159. The evaluation board has a footprint capable of supporting a variety of 32-lead 5 mm × 5 mm LFCSP VCOs.

The supply voltage for the ADF4159 internal charge pump is 3.3 V. However, many wideband VCOs require a tuning voltage of up to 18 V. To handle this, an active loop filter is required. The active filter multiplies the output tuning range of the ADF4159 by the gain of the op amp. For more detail, see the AD8065 section of this circuit note.

The ADF4159 supports a programmable charge pump current feature. This feature allows the user to easily modify the loop filter dynamic without changing the physical components. In this circuit, the LBW was designed for 2.4 MHz at a charge pump current of 2.5 mA. The charge pump current can be reduced in order to reduce the LBW without physically changing the loop filter components.

Active Filter Using the AD8065

 
The AD8065 op amp has a 24 V supply voltage range, a gain bandwidth product (GBP) of approximately 145 MHz, and low noise (7 nV/√Hz). These features make it ideal for an active filter.

For most PLL applications, a phase margin of 45° to 55° is recommended to maintain a stable loop and to minimize settling time. In an active loop filter, that is, when there is an op amp in a loop filter, an additional pole occurs at the unity gain frequency (or gain bandwidth product) of the op amp. This additional pole adds extra phase lag; therefore, depending on the frequency of the pole, it can render the loop unstable.

Table 1. Phase Lag as a Function of GBP:LBW Ratio
GBP/LBW Ratio Extra Phase Lag (°)
5 (for example, GBW = 1 MHz, LBW = 200 kHz) 11.3
10 5.7
20 2.9

The higher the ratio of GBP to LBW, the less phase lag. For example, Table 1 shows that a GBP/LBW ratio of 10 reduces the phase margin by 5.7°. If the GBP/LBW ratio is too low, the phase margin also becomes too low and results in an unstable loop.

This circuit uses a 2.4 MHz LBW, so the AD8065 145 MHz GBP results in negligible phase lag (GBP/LBW = 60).

Comparison with OP184 Active Filter

 
The OP184 is a frequently used op amp in active filter PLL applications. However, the OP184 is not suitable for very wide LBW applications due to its 4 MHz GBP. Some optimization of the phase margin allows the use of the OP184 at wide LBWs, but ultimately, the OP184 limits the maximum LBW.

The op amp in the active filter is configured in the inverting mode, therefore the ADF4159 is programmed with a negative phase-detector polarity. The inverting configuration is easier to implement because the op amp positive input can be biased at a fixed voltage that does not change with the op amp output (as it does in the noninverting configuration).

The AD8065 also acts as a buffer to mitigate the input capacitance of the VCO. For a 2.4 MHz LBW passive filter, the combined capacitance of the VCO input and the last capacitor in the filter must be approximately 1.5 pF. However, the VCO measured input capacitance alone is 52 pF.

Ceramic C0G/NP0 capacitors (which discharge quicker than standard capacitors) are recommended for the loop filter capacitors to minimize phase settling time.

Excellent layout, grounding, and decoupling techniques are required for the circuit as described in the MT-031 and MT-101 tutorials.

Test Results

 
The measured phase noise of the circuit is shown in Figure 4. Frequency and phase settling time for a 200 MHz jump in frequency are shown in Figure 5 and Figure 6, respectively.

Figure 4. Phase Noise at 12.002 GHz; LBW = 2.4 MHz
Figure 4. Phase noise at 12.002 GHz; LBW = 2.4 MHz
Figure 5. Frequency Settling for a 200 MHz Jump from 12.2 GHz to 12.0 GHz
Figure 5. Frequency settling for a 200 MHz jump from 12.2 GHz to 12.0 GHz
Figure 6. Phase Settling for a 200 MHz Jump from 12.2 GHz to 12.0 GHz
Figure 6. Phase settling for a 200 MHz jump from 12.2 GHz to 12.0 GHz