MAXREFDES281 Introduction and Demonstration
This video will introduce the MAXREFDES281, and provide a demonstration on setting up and using the board. The flashed firmware allows the MAXREFDES281 to be used as an IO-Link interface for the MAX22007PMB industrial analog output board.
Video Player is loading.
Current Time 0:00
Duration 7:45
Loaded: 0.00%
Stream Type LIVE
Remaining Time 7:45
 
1x
  • Chapters
  • descriptions off, selected
  • subtitles off, selected
  • en (Main), selected

MAXREFDES281 Introduction and Demonstration

2025-04-03

This video will introduce the MAXREFDES281, and provide a demonstration on setting up and using the board. The demonstration will be evaluating the MAXREFDES281 using the firmware already flashed to the board. This firmware allows the MAXREFDES281 to be used as an IO-Link interface for the MAX22007PMB industrial analog output board.

MAXREFDES281 Introduction and Demonstration
This video will introduce the MAXREFDES281, and provide a demonstration on setting up and using the board. The flashed firmware allows the MAXREFDES281 to be used as an IO-Link interface for the MAX22007PMB industrial analog output board.
Video Player is loading.
Current Time 0:00
Duration 7:45
Loaded: 0.00%
Stream Type LIVE
Remaining Time 7:45
 
1x
  • Chapters
  • descriptions off, selected
  • subtitles off, selected
  • en (Main), selected

MAXREFDES281 Introduction and Demonstration

2025-04-03

This video will introduce the MAXREFDES281, and provide a demonstration on setting up and using the board. The demonstration will be evaluating the MAXREFDES281 using the firmware already flashed to the board. This firmware allows the MAXREFDES281 to be used as an IO-Link interface for the MAX22007PMB industrial analog output board.